Main functions for USB Device vendor example.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
int | main (void) |
Main function. Execution starts here. More... | |
void | main_resume_action (void) |
Turn on a led to notify active mode Called when the USB line is resumed from the suspend state. More... | |
bool | main_setup_in_received (void) |
Manage the reception of setup request IN. More... | |
bool | main_setup_out_received (void) |
Manage the reception of setup request OUT. More... | |
void | main_sof_action (void) |
Manages the leds behaviors Called when a start of frame is received on USB line each 1ms. More... | |
void | main_suspend_action (void) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More... | |
void | main_vendor_bulk_in_received (udd_ep_status_t status, iram_size_t nb_transfered, udd_ep_id_t ep) |
void | main_vendor_bulk_out_received (udd_ep_status_t status, iram_size_t nb_transfered, udd_ep_id_t ep) |
void | main_vendor_disable (void) |
Notify via user interface that enumeration is disabled This is called by vendor interface when USB Host disable it. More... | |
bool | main_vendor_enable (void) |
Notify via user interface that enumeration is ok This is called by vendor interface when USB Host enable it. More... | |
void | main_vendor_int_in_received (udd_ep_status_t status, iram_size_t nb_transfered, udd_ep_id_t ep) |
void | main_vendor_int_out_received (udd_ep_status_t status, iram_size_t nb_transfered, udd_ep_id_t ep) |
void | main_vendor_iso_in_received (udd_ep_status_t status, iram_size_t nb_transfered, udd_ep_id_t ep) |
void | main_vendor_iso_out_received (udd_ep_status_t status, iram_size_t nb_transfered, udd_ep_id_t ep) |
Variables | |
static volatile bool | main_b_vendor_enable = false |
Buffer for loopback | |
#define | MAIN_LOOPBACK_SIZE 1024 |
Size of buffer used for the loopback. More... | |
static COMPILER_WORD_ALIGNED uint8_t | main_buf_loopback [MAIN_LOOPBACK_SIZE] |
static uint8_t | main_buf_iso_sel |
#define MAIN_LOOPBACK_SIZE 1024 |
Size of buffer used for the loopback.
int main | ( | void | ) |
Main function. Execution starts here.
References board_init(), cpu_irq_enable(), irq_initialize_vectors, sleepmgr_enter_sleep(), sleepmgr_init(), sysclk_init(), udc_start(), and ui_init().
void main_resume_action | ( | void | ) |
Turn on a led to notify active mode Called when the USB line is resumed from the suspend state.
Called by UDD when the USB line exit of suspend state.
bool main_setup_in_received | ( | void | ) |
Manage the reception of setup request IN.
true | if request accepted |
References main_buf_loopback, min, udd_ctrl_request_t::payload, udd_ctrl_request_t::payload_size, udd_ctrl_request_t::req, udd_g_ctrlreq, ui_loop_back_state(), and usb_setup_req_t::wLength.
bool main_setup_out_received | ( | void | ) |
Manage the reception of setup request OUT.
true | if request accepted |
References main_buf_loopback, min, udd_ctrl_request_t::payload, udd_ctrl_request_t::payload_size, udd_ctrl_request_t::req, udd_g_ctrlreq, ui_loop_back_state(), and usb_setup_req_t::wLength.
void main_sof_action | ( | void | ) |
Manages the leds behaviors Called when a start of frame is received on USB line each 1ms.
Called when a start of frame is received on USB line.
void main_suspend_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state.
Turn off all leds Callback running when USB Host set USB line in suspend state.
Called by UDD when a suspend is received Callback running when USB Host set USB line in suspend state.
void main_vendor_bulk_in_received | ( | udd_ep_status_t | status, |
iram_size_t | nb_transfered, | ||
udd_ep_id_t | ep | ||
) |
References main_buf_loopback, main_vendor_bulk_out_received(), UDD_EP_TRANSFER_OK, udi_vendor_bulk_out_run(), ui_loop_back_state(), and UNUSED.
Referenced by main_vendor_bulk_out_received(), and main_vendor_enable().
void main_vendor_bulk_out_received | ( | udd_ep_status_t | status, |
iram_size_t | nb_transfered, | ||
udd_ep_id_t | ep | ||
) |
References main_buf_loopback, main_vendor_bulk_in_received(), UDD_EP_TRANSFER_OK, udi_vendor_bulk_in_run(), ui_loop_back_state(), and UNUSED.
Referenced by main_vendor_bulk_in_received().
void main_vendor_disable | ( | void | ) |
Notify via user interface that enumeration is disabled This is called by vendor interface when USB Host disable it.
References main_b_vendor_enable.
bool main_vendor_enable | ( | void | ) |
Notify via user interface that enumeration is ok This is called by vendor interface when USB Host enable it.
true | if vendor startup is successfully done |
References main_b_vendor_enable, main_buf_iso_sel, main_vendor_bulk_in_received(), main_vendor_int_in_received(), main_vendor_iso_out_received(), and UDD_EP_TRANSFER_OK.
void main_vendor_int_in_received | ( | udd_ep_status_t | status, |
iram_size_t | nb_transfered, | ||
udd_ep_id_t | ep | ||
) |
References main_buf_loopback, main_vendor_int_out_received(), UDD_EP_TRANSFER_OK, udi_vendor_interrupt_out_run(), ui_loop_back_state(), and UNUSED.
Referenced by main_vendor_enable(), and main_vendor_int_out_received().
void main_vendor_int_out_received | ( | udd_ep_status_t | status, |
iram_size_t | nb_transfered, | ||
udd_ep_id_t | ep | ||
) |
References main_buf_loopback, main_vendor_int_in_received(), UDD_EP_TRANSFER_OK, udi_vendor_interrupt_in_run(), ui_loop_back_state(), and UNUSED.
Referenced by main_vendor_int_in_received().
void main_vendor_iso_in_received | ( | udd_ep_status_t | status, |
iram_size_t | nb_transfered, | ||
udd_ep_id_t | ep | ||
) |
References ui_loop_back_state(), and UNUSED.
Referenced by main_vendor_iso_out_received().
void main_vendor_iso_out_received | ( | udd_ep_status_t | status, |
iram_size_t | nb_transfered, | ||
udd_ep_id_t | ep | ||
) |
Referenced by main_sof_action(), main_vendor_disable(), and main_vendor_enable().
|
static |
Referenced by main_vendor_enable(), and main_vendor_iso_out_received().
|
static |