License | Copyright (c) 2017-2018 Microchip Technology Inc |
Extra Information for Peripheral DMA Controller | |
Examples for Peripheral DMA Controller | This is a list of the available Quick Start guides (QSGs) and example applications for SAM3A/3N/3S/3U/3X/4E/4N/4S/G Peripheral DMA Controller (PDC) Driver |
 Quick Start Guide for PDC - Basic | This is the quickstart guide for SAM3A/3N/3S/3U/3X/4E/4N/4S/G Peripheral DMA Controller (PDC) Driver with step-by-step instructions on how to configure and use the driver |
 Peripheral DMA Controller Example | |
Document Revision History | |
Quick start guide for the common IOPORT service | This is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases |
 Advanced use case doing port access | In this case we will read out the pins from one whole port and write the read value to another port |
Quickstart guide for Common service TWI | This is the quickstart guide for the Common service TWI, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick start guide for USB device Mass Storage module (UDI MSC) | This is the quick start guide for the USB device interface MSC module (UDI MSC) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 MSC in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
 Change USB speed | In this use case, the USB device is used with different USB speeds |
 Use USB strings | In this use case, the usual USB strings is added in the USB device |
 Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
 Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
 USB dynamic serial number | In this use case, the USB serial strings is dynamic |
Quick start guide for USB device mouse module (UDI mouse) | This is the quick start guide for the USB device mouse module (UDI mouse) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 HID mouse in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
 Change USB speed | In this use case, the USB device is used with different USB speeds |
 Use USB strings | In this use case, the usual USB strings is added in the USB device |
 Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
 Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
 USB dynamic serial number | In this use case, the USB serial strings is dynamic |
Quickstart guide for SAM SPI driver | This is the quickstart guide for the SAM SPI driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick Start Guide for the SAM PIO driver | This is the quick start guide for the PIO Driver, with step-by-step instructions on how to configure and use the driver for specific use cases |
Advanced use case - Interrupt driven edge detection | |
Quick start guide for First-In-First-Out Buffer (FIFO) | This is the quick start guide for the First-In-First-Out Buffer (FIFO), with step-by-step instructions on how to configure and use the driver in a selection of use cases |
 Push and flush | In this use case, two elements will be pushed to the FIFO, and the FIFO will be flushed |
Quick Start Guide for the SPI Master Driver | This is the quick start guide for the SPI Driver, with step-by-step instructions on how to configure and use the driver for a specific use case |
 Basic setup for SPI master on XMEGA devices | |
Quick start guide for the SAM PMC module | This is the quick start guide for the PMC module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
conf_clock.h examples with USB support | Content of XMEGA conf_clock.h: |
Quick start guide for USB Device Vendor module (UDI Vendor) | This is the quick start guide for the USB device interface Vendor module (UDI Vendor) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 Vendor in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
 Change USB speed | In this use case, the USB device is used with different USB speeds |
 Use USB strings | In this use case, the usual USB strings is added in the USB device |
 Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
 Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
 USB dynamic serial number | In this use case, the USB serial strings is dynamic |
Quick start guide for Serial Interface service | This is the quick start guide for the Serial Interface module, with step-by-step instructions on how to configure and use the serial in a selection of use cases |
 Advanced use case - Send a packet of serial data | In this use case, the USART module is configured for: |
Quick start guide for USB host mass-storage module (UHI MSC) | This is the quick start guide for the USB host mass-storage module (UHI MSC) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 Enable USB high speed support | In this use case, the USB host is used to support USB high speed |
 Multiple classes support | In this use case, the USB host is used to support several USB classes |
 Dual roles support | In this use case, the USB host and USB device are enabled, it is the dual role |
Quick start guide for the SAM WM8731 module | This is the quick start guide for the WM8731 Audio Codec, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick start guide for USB device generic module (UDI generic) | This is the quick start guide for the USB device generic module (UDI generic) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 HID generic in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
 Change USB speed | In this use case, the USB device is used with different USB speeds |
 Use USB strings | In this use case, the usual USB strings is added in the USB device |
 Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
 Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
 USB dynamic serial number | In this use case, the USB serial strings is dynamic |
Quickstart guide for SDRAMC driver. | This is the quickstart guide for the SDRAM Controller, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Extra Information for Direct Memory Access Controller Driver | |
Examples for Direct Memory Access Controller Driver | This is a list of the available Quick Start Guides (QSGs) and example applications for SAM3A/3U/3X/4E DMA Controller (DMAC) Driver |
 Quick Start Guide for the DMAC driver | This is the quick start guide for the SAM3A/3U/3X/4E DMA Controller (DMAC) Driver, with step-by-step instructions on how to configure and use the driver for a specific use case |
 SAM Direct Memory Access Controller - Example Memory to Memory Transfer | |
Document Revision History | |
Quick start guide for the SAM USART module | This is the quick start guide for the USART module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
 USART receive character and echo back | In this use case, the USART module is configured for: |
 USART receive character and echo back via interrupts | In this use case, the USART module is configured for: |
Quickstart guide for SAM CAN module. | This is the quickstart guide for the SAM CAN module",with step-by-step instructions on how to configure and use the drivers in a selection of use cases |
 Use case #1 | In this use case, CAN0 mailbox 0 works in PRODUCER mode, and CAN1 mailbox 0 works in CONSUMER mode |
Quick start guide for USB host Communication Device Class module (UHI CDC) | This is the quick start guide for the USB host Communication Device Class module (UHI CDC) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 Enable USB high speed support | In this use case, the USB host is used to support USB high speed |
 Multiple classes support | In this use case, the USB host is used to support several USB classes |
 Dual roles support | In this use case, the USB host and USB device are enabled, it is the dual role |
Quickstart guide for MCP980X module | This is the quickstart guide for the MCP980X module, with step-by-step instructions on how to configure and use the drivers in a selection of use cases |
Extra Information for Reset Controller Driver | |
Examples for Reset Controller Driver | This is a list of the available Quick Start Guides (QSGs) and example applications for SAM3/4C/4CM/4CP/4E/4N/4S/G/V71/V70/S70/E70 Reset Controller (RSTC) Driver |
 Quick Start guide for SAM RSTC driver | This is the quick start guide for the SAM3/4C/4CM/4CP/4E/4N/4S/G/V71/V70/S70/E70 Reset Controller (RSTC) Driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
 Reset Controller (RSTC) Example | |
Document Revision History | |
Quick start guide for USB host mouse module (UHI mouse) | This is the quick start guide for the USB host mouse module (UHI mouse) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 Enable USB high speed support | In this use case, the USB host is used to support USB high speed |
 Multiple classes support | In this use case, the USB host is used to support several USB classes |
 Dual roles support | In this use case, the USB host and USB device are enabled, it is the dual role |
Quick start guide for USB device keyboard module (UDI keyboard) | This is the quick start guide for the USB device keyboard module (UDI keyboard) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 HID keyboard in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
 Change USB speed | In this use case, the USB device is used with different USB speeds |
 Use USB strings | In this use case, the usual USB strings is added in the USB device |
 Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
 Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
 USB dynamic serial number | In this use case, the USB serial strings is dynamic |
uxQueueMessagesWaiting | Queue |
vQueueDelete | Queue |
vSemaphoreDelete | Semphr |
xTaskHandle | Task |
taskYIELD | Task |
taskENTER_CRITICAL | Task |
taskEXIT_CRITICAL | Task |
taskDISABLE_INTERRUPTS | Task |
taskENABLE_INTERRUPTS | Task |
xTaskGetTickCount | Task |
uxTaskGetNumberOfTasks | Task |
pcTaskGetTaskName | Task |
vTaskList | Task |
vTaskGetRunTimeStats | Task |
vTaskStartTrace | Task |
usTaskEndTrace | Task |
Quickstart guide for SAM ADC driver | This is the quickstart guide for the SAM ADC driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
 Advanced use cases | In this use case the ADC module and one channel are configured for: |
Quickstart guide for AT25DFx component. | This is the quickstart guide for the AT25DFx SerialFlash component, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Extra Information for Timer Counter Driver | |
Examples for Timer Counter | This is a list of the available Quick Start Guides (QSGs) and example applications for SAM3/4S/4L/4E/4N/4CM/4C/G Timer Counter (TC) Driver |
 Quick Start Guide for the TC driver | This is the quick start guide for the SAM3/4S/4L/4E/4N/4CM/4C/G Timer Counter (TC) Driver, with step-by-step instructions on how to configure and use the driver for a specific use case |
 Timer Counter Capture Waveform Example | |
Document Revision History | |
Quick start guide for USB device Communication Class Device module (UDI CDC) | This is the quick start guide for the USB device interface CDC module (UDI CDC) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 CDC in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
 Change USB speed | In this use case, the USB device is used with different USB speeds |
 Use USB strings | In this use case, the usual USB strings is added in the USB device |
 Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
 Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
 USB dynamic serial number | In this use case, the USB serial strings is dynamic |
Quick start guide for the maXTouch component | This is the quick start guide for the maXTouch component The guide will give you a step-by-step introduction on how to setup and use the component to be able to read touch responses from the maXTouch Xplained kit |
Quick Start Guide for the ILI9341 Display Controller Component Driver | This is the quick start guide for the ILI9341 Display Controller Component Driver, with step-by-step instructions on how to configure and use the component driver for specific use cases |
Quick Start Guide for the System Clock Management service (SAM3A) | This is the quick start guide for the System Clock Management service, with step-by-step instructions on how to configure and use the service for specific use cases |
death.c | Create a single persistent task which periodically dynamically creates another two tasks |
Quick Start Guide for the ILI93XX | LCD Glass component |
Quick start guide for the | NAND Flash module |
Quick start guide for | FreeRTOS UART peripheral control functions |
 Initializing the FreeRTOS UART | Driver for standard operation |
 Transmitting using the FreeRTOS UART driver in | Standard mode |
 Initializing the FreeRTOS UART | Driver for asynchronous operation |
 Transmitting using the FreeRTOS UART driver in | Fully asynchronous mode |
 Receiving using the FreeRTOS UART driver | This example demonstrates using the FreeRTOS UART API to receive data |
Quick Start Guide for the graphics service | This is the quick start guide for the Graphics (GFX) service", with step-by-step instructions on how to configure and use it for a specific use case |
Quick start guide for USB host vendor module (UHI vendor) | This is the quick start guide for the USB host vendor module (UHI vendor) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 Enable USB high speed support | In this use case, the USB host is used to support USB high speed |
 Multiple classes support | In this use case, the USB host is used to support several USB classes |
 Dual roles support | In this use case, the USB host and USB device are enabled, it is the dual role |
Quick start guide for QTouch component | This is the quick start guide for the QTouch device driver for I2C interface, with step-by-step instructions on how to configure and use the driver for a specific use case |
Quick start guide for USB device multi-touch module (UDI Multi-touch) | |
Quick start guide for the SAM LIN module | This is the quick start guide for the LIN module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
conf_clock.h examples with USB support | Content of conf_clock.h for AT32UC3A0, AT32UC3A1, AT32UC3B devices (USBB): |
Quickstart guide for SAM PWM module | This is the quickstart guide for the PWM module, with step-by-step instructions on how to configure and use the drivers in a selection of use cases |
 Use case #1 | In this use case, the PWM module is configured to: |
Quick start guide for | FreeRTOS TWI peripheral control functions |
 Initializing the FreeRTOS TWI driver | For standard operation |
 Transmitting using the FreeRTOS TWI driver in | Standard mode |
 Receiving using the FreeRTOS TWI driver in | Standard mode |
 Initializing the FreeRTOS TWI driver | For asynchronous operation |
 Transmitting using the FreeRTOS TWI driver in | Fully asynchronous mode |
 Receiving using the FreeRTOS TWI driver in fully | Asynchronous mode |
Quick start guide for | FreeRTOS USART peripheral control functions |
 Initializing the FreeRTOS USART | Driver for standard operation |
 Transmitting using the FreeRTOS USART driver in | Standard mode |
 Initializing the FreeRTOS USART | Driver for asynchronous operation |
 Transmitting using the FreeRTOS USART driver in | Fully asynchronous mode |
 Receiving using the FreeRTOS USART driver | This example demonstrates using the FreeRTOS USART API to receive data |
Quick Start quide for common NVM driver | This is the quick start quide for the Common NVM driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quickstart guide for SAM RTC driver | This is the quickstart guide for the SAM RTC driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quickstart guide for EMAC driver. | This is the quickstart guide for the Ethernet MAC, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Todo List | |
Deprecated List | |