See Quickstart guide for SDRAMC driver..
Driver for the SDRAMC (SDRAM Controller). This driver provides access to the main features of the SDRAM controller.
This driver does not depend on other modules.
Modules | |
Related Project(s) | |
In this section you can find all the projects related to the SDRAMC - SDRAM Controller. | |
Quick Start Guide(s) | |
In this section you can find a list of all Quick Start guides related to the SDRAMC - SDRAM Controller. | |
Functions | |
void | sdramc_deinit (void) |
De-initialize the SDRAM controller. More... | |
void | sdramc_init (sdramc_memory_dev_t *p_sdram, uint32_t ul_clk) |
Initialize the SDRAM controller. More... | |
void sdramc_deinit | ( | void | ) |
De-initialize the SDRAM controller.
References SLEEPMGR_ACTIVE, and sleepmgr_unlock_mode().
void sdramc_init | ( | sdramc_memory_dev_t * | p_sdram, |
uint32_t | ul_clk | ||
) |
Initialize the SDRAM controller.
p_sdram | Pointer to the sdram memory structure. |
ul_clk | SDRAM clock frequency. |
References sdramc_memory_dev::cr, SLEEPMGR_ACTIVE, sleepmgr_lock_mode(), sdramc_memory_dev::ul_bk1, sdramc_memory_dev::sdramc_cr::ul_cfg, and sdramc_memory_dev::ul_mode.
Referenced by main(), memories_initialization(), and run_sdramc_test().