Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
FTM280C34D display using ILI9325 display controller

This is hardware specific configuration that configures the graphical service for use with the ILI9325 display controller and the ET024006DHU display.

All the drawing functionality in this configuration is provided by the Generic Implementation of Graphics Primitives driver. This configuration includes information about the panel size, data type used for coordinates and color and functionality to convert RGB color to the color format native to the display.

Macros

#define GFX_COLOR(r, g, b)   ILI9325_COLOR(r, g, b)
 
#define gfx_color(r, g, b)   gfx_ili9325_color(r, g, b)
 ILI9325 display driver specific function, see gfx_ili9325_color. More...
 
#define GFX_COLOR_INVALID   GFX_COLOR(1, 2, 3)
 It is not possible to define a color that is outside the color spectrum for the ILI9325 driver, hence use a dark color as invalid color. More...
 
#define GFX_COLOR_TRANSPARENT   GFX_COLOR(254, 0, 0)
 
#define gfx_copy_pixels_from_screen(pixels, count)   ili9325_copy_pixels_from_screen(pixels, count)
 ILI9325 display driver specific function, see ili9325_copy_pixels_from_screen. More...
 
#define gfx_copy_pixels_to_screen(pixels, count)   ili9325_copy_pixels_to_screen(pixels, count)
 ILI9325 display driver specific function, see ili9325_copy_pixels_to_screen. More...
 
#define gfx_copy_progmem_pixels_to_screen(pixels, count)   ili9325_copy_raw_pixel_24bits_to_screen(pixels, count)
 ILI9325 display driver specific function available for ATmega and ATXmega devices, see ili9325_copy_progmem_pixels_to_screen. More...
 
#define gfx_draw_bitmap(bmp, x, y)   gfx_generic_draw_bitmap(bmp, x, y)
 ILI9325 display driver uses generic gfx implementation for this function. More...
 
#define gfx_draw_bitmap_tiled(bmp, x1, y1, x2, y2, tile_origin_x, tile_origin_y)
 ILI9325 display driver uses generic gfx implementation for this function. More...
 
#define gfx_draw_circle(x, y, radius, color, octant_mask)   gfx_generic_draw_circle(x, y, radius, color, octant_mask)
 ILI9325 display driver uses generic gfx implementation for this function. More...
 
#define gfx_draw_filled_circle(x, y, radius, color, quadrant_mask)
 ILI9325 display driver uses generic gfx implementation for this function. More...
 
#define gfx_draw_filled_rect(x, y, width, height, color)   gfx_generic_draw_filled_rect(x, y, width, height, color)
 ILI9325 display driver uses generic gfx implementation for this function. More...
 
#define gfx_draw_horizontal_line(x, y, length, color)   gfx_generic_draw_horizontal_line(x, y, length, color)
 ILI9325 display driver uses generic gfx implementation for this function. More...
 
#define gfx_draw_line(x1, y1, x2, y2, color)   gfx_generic_draw_line(x1, y1, x2, y2, color)
 ILI9325 display driver uses generic gfx implementation for this function. More...
 
#define gfx_draw_line_pixel(x, y, color)
 ILI9325 display driver specific function, see gfx_ili9325_draw_line_pixel. More...
 
#define gfx_draw_pixel(x, y, color)   gfx_ili9325_draw_pixel(x, y, color)
 ILI9325 display driver specific function, see gfx_ili9325_draw_pixel. More...
 
#define gfx_draw_rect(x, y, width, height, color)   gfx_generic_draw_rect(x, y, width, height, color)
 ILI9325 display driver uses generic gfx implementation for this function. More...
 
#define gfx_draw_vertical_line(x, y, length, color)   gfx_generic_draw_vertical_line(x, y, length, color)
 ILI9325 display driver uses generic gfx implementation for this function. More...
 
#define gfx_duplicate_pixel(color, count)   ili9325_duplicate_pixel(color, count)
 ILI9325 display driver specific function, see ili9325_duplicate_pixel. More...
 
#define gfx_get_pixel(x, y)   gfx_ili9325_get_pixel(x, y)
 ILI9325 display driver specific function, see gfx_ili9325_get_pixel. More...
 
#define gfx_get_pixmap(pixmap, map_width, map_x, map_y, x, y, width, height)
 ILI9325 display driver uses generic gfx implementation for this function. More...
 
#define gfx_init()   gfx_ili9325_init()
 ILI9325 display driver specific function, see gfx_ili9325_init. More...
 
#define gfx_put_bitmap(bmp, map_x, map_y, x, y, width, height)   gfx_generic_put_bitmap(bmp, map_x, map_y, x, y, width, height)
 ILI9325 display driver uses generic gfx implementation for this function. More...
 
#define gfx_put_pixmap(pixmap, map_width, map_x, map_y, x, y, width, height)
 ILI9325 display driver uses generic gfx implementation for this function. More...
 
#define gfx_set_bottom_right_limit(x, y)   ili9325_set_bottom_right_limit(x, y)
 ILI9325 display driver specific function, see ili9325_set_bottom_right_limit. More...
 
#define gfx_set_ext_handler(ext_draw_handler)   gfx_generic_set_ext_handler(ext_draw_handler)
 ILI9325 display driver uses generic gfx implementation for this function. More...
 
#define gfx_set_limits(x1, y1, x2, y2)   ili9325_set_limits(x1, y1, x2, y2)
 ILI9325 display driver specific function, see ili9325_set_limits. More...
 
#define gfx_set_orientation(flags)   gfx_ili9325_set_orientation(flags)
 ILI9325 display driver specific function, see gfx_ili9325_set_orientation. More...
 
#define gfx_set_top_left_limit(x, y)   ili9325_set_top_left_limit(x, y)
 ILI9325 display driver specific function, see ili9325_set_top_left_limit. More...
 
#define gfx_sync()   gfx_generic_sync()
 ILI9325 display driver uses generic gfx implementation for this function. More...
 

Functions

gfx_color_t gfx_ili9325_color (uint8_t r, uint8_t g, uint8_t b)
 Generate native color value from R/G/B values. More...
 
void gfx_ili9325_draw_line_pixel (gfx_coord_t x, gfx_coord_t y, gfx_color_t color)
 Draw a single pixel on the screen. More...
 
void gfx_ili9325_draw_pixel (gfx_coord_t x, gfx_coord_t y, gfx_color_t color)
 Draw a single pixel on the screen. More...
 
gfx_color_t gfx_ili9325_get_pixel (gfx_coord_t x, gfx_coord_t y)
 Get the color of a pixel on the display. More...
 
void gfx_ili9325_init (void)
 Initialize the ili9325 display controller. More...
 
void gfx_ili9325_set_orientation (uint8_t flags)
 Set display orientation. More...
 
#define ILI9325_LCD_CS   1
 
gfx_coord_t gfx_height
 Current height of screen. More...
 
gfx_coord_t gfx_width
 Current width of screen. More...
 
gfx_coord_t gfx_min_x
 Minimum X of current clipping region. More...
 
gfx_coord_t gfx_min_y
 Maximum Y of current clipping region. More...
 
gfx_coord_t gfx_max_x
 Minimum X of current clipping region. More...
 
gfx_coord_t gfx_max_y
 Maximum Y of current clipping region. More...
 

#define GFX_COLOR (   r,
  g,
 
)    ILI9325_COLOR(r, g, b)
#define gfx_color (   r,
  g,
 
)    gfx_ili9325_color(r, g, b)

ILI9325 display driver specific function, see gfx_ili9325_color.

#define GFX_COLOR_INVALID   GFX_COLOR(1, 2, 3)

It is not possible to define a color that is outside the color spectrum for the ILI9325 driver, hence use a dark color as invalid color.

#define GFX_COLOR_TRANSPARENT   GFX_COLOR(254, 0, 0)
#define gfx_copy_pixels_from_screen (   pixels,
  count 
)    ili9325_copy_pixels_from_screen(pixels, count)

ILI9325 display driver specific function, see ili9325_copy_pixels_from_screen.

#define gfx_copy_pixels_to_screen (   pixels,
  count 
)    ili9325_copy_pixels_to_screen(pixels, count)

ILI9325 display driver specific function, see ili9325_copy_pixels_to_screen.

#define gfx_copy_progmem_pixels_to_screen (   pixels,
  count 
)    ili9325_copy_raw_pixel_24bits_to_screen(pixels, count)

ILI9325 display driver specific function available for ATmega and ATXmega devices, see ili9325_copy_progmem_pixels_to_screen.

#define gfx_draw_bitmap (   bmp,
  x,
 
)    gfx_generic_draw_bitmap(bmp, x, y)

ILI9325 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_bitmap

#define gfx_draw_bitmap_tiled (   bmp,
  x1,
  y1,
  x2,
  y2,
  tile_origin_x,
  tile_origin_y 
)
Value:
gfx_generic_draw_bitmap_tiled(bmp, x1, y1, x2, y2,\
tile_origin_x, tile_origin_y)
void gfx_generic_draw_bitmap_tiled(const struct gfx_bitmap *bmp, gfx_coord_t x1, gfx_coord_t y1, gfx_coord_t x2, gfx_coord_t y2, gfx_coord_t tile_origin_x, gfx_coord_t tile_origin_y)
Definition: gfx_generic.c:546

ILI9325 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_bitmap_tiled

#define gfx_draw_circle (   x,
  y,
  radius,
  color,
  octant_mask 
)    gfx_generic_draw_circle(x, y, radius, color, octant_mask)

ILI9325 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_circle

#define gfx_draw_filled_circle (   x,
  y,
  radius,
  color,
  quadrant_mask 
)
Value:
gfx_generic_draw_filled_circle(x, y, radius, color,\
quadrant_mask)
void gfx_generic_draw_filled_circle(gfx_coord_t x, gfx_coord_t y, gfx_coord_t radius, gfx_color_t color, uint8_t quadrant_mask)
Definition: gfx_generic.c:296

ILI9325 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_filled_circle

#define gfx_draw_filled_rect (   x,
  y,
  width,
  height,
  color 
)    gfx_generic_draw_filled_rect(x, y, width, height, color)

ILI9325 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_filled_rect

#define gfx_draw_horizontal_line (   x,
  y,
  length,
  color 
)    gfx_generic_draw_horizontal_line(x, y, length, color)

ILI9325 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_horizontal_line

#define gfx_draw_line (   x1,
  y1,
  x2,
  y2,
  color 
)    gfx_generic_draw_line(x1, y1, x2, y2, color)

ILI9325 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_line

#define gfx_draw_line_pixel (   x,
  y,
  color 
)
Value:
color)
void gfx_ili9325_draw_line_pixel(gfx_coord_t x, gfx_coord_t y, gfx_color_t color)
Draw a single pixel on the screen.
Definition: gfx_ili9325_ftm280c34d.c:115

ILI9325 display driver specific function, see gfx_ili9325_draw_line_pixel.

#define gfx_draw_pixel (   x,
  y,
  color 
)    gfx_ili9325_draw_pixel(x, y, color)

ILI9325 display driver specific function, see gfx_ili9325_draw_pixel.

#define gfx_draw_rect (   x,
  y,
  width,
  height,
  color 
)    gfx_generic_draw_rect(x, y, width, height, color)

ILI9325 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_rect

#define gfx_draw_vertical_line (   x,
  y,
  length,
  color 
)    gfx_generic_draw_vertical_line(x, y, length, color)

ILI9325 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_vertical_line

#define gfx_duplicate_pixel (   color,
  count 
)    ili9325_duplicate_pixel(color, count)

ILI9325 display driver specific function, see ili9325_duplicate_pixel.

#define gfx_get_pixel (   x,
 
)    gfx_ili9325_get_pixel(x, y)

ILI9325 display driver specific function, see gfx_ili9325_get_pixel.

#define gfx_get_pixmap (   pixmap,
  map_width,
  map_x,
  map_y,
  x,
  y,
  width,
  height 
)
Value:
gfx_generic_get_pixmap(pixmap, map_width, map_x, map_y, x, y,\
width, height)
void gfx_generic_get_pixmap(gfx_color_t *pixmap, gfx_coord_t map_width, gfx_coord_t map_x, gfx_coord_t map_y, gfx_coord_t x, gfx_coord_t y, gfx_coord_t width, gfx_coord_t height)
Definition: gfx_generic.c:358

ILI9325 display driver uses generic gfx implementation for this function.

See gfx_generic_get_pixmap

#define gfx_init ( )    gfx_ili9325_init()

ILI9325 display driver specific function, see gfx_ili9325_init.

#define gfx_put_bitmap (   bmp,
  map_x,
  map_y,
  x,
  y,
  width,
  height 
)    gfx_generic_put_bitmap(bmp, map_x, map_y, x, y, width, height)

ILI9325 display driver uses generic gfx implementation for this function.

See gfx_generic_put_bitmap

#define gfx_put_pixmap (   pixmap,
  map_width,
  map_x,
  map_y,
  x,
  y,
  width,
  height 
)
Value:
gfx_generic_put_pixmap(pixmap, map_width, map_x, map_y, x, y,\
width, height)
void gfx_generic_put_pixmap(const gfx_color_t *pixmap, gfx_coord_t map_width, gfx_coord_t map_x, gfx_coord_t map_y, gfx_coord_t x, gfx_coord_t y, gfx_coord_t width, gfx_coord_t height)
Definition: gfx_generic.c:452

ILI9325 display driver uses generic gfx implementation for this function.

See gfx_generic_put_pixmap

#define gfx_set_bottom_right_limit (   x,
 
)    ili9325_set_bottom_right_limit(x, y)

ILI9325 display driver specific function, see ili9325_set_bottom_right_limit.

#define gfx_set_ext_handler (   ext_draw_handler)    gfx_generic_set_ext_handler(ext_draw_handler)

ILI9325 display driver uses generic gfx implementation for this function.

See gfx_generic_set_ext_handler

#define gfx_set_limits (   x1,
  y1,
  x2,
  y2 
)    ili9325_set_limits(x1, y1, x2, y2)

ILI9325 display driver specific function, see ili9325_set_limits.

#define gfx_set_orientation (   flags)    gfx_ili9325_set_orientation(flags)

ILI9325 display driver specific function, see gfx_ili9325_set_orientation.

#define gfx_set_top_left_limit (   x,
 
)    ili9325_set_top_left_limit(x, y)

ILI9325 display driver specific function, see ili9325_set_top_left_limit.

#define gfx_sync (   void)    gfx_generic_sync()

ILI9325 display driver uses generic gfx implementation for this function.

See gfx_generic_sync

#define ILI9325_LCD_CS   1

Referenced by gfx_ili9325_init().

gfx_color_t gfx_ili9325_color ( uint8_t  r,
uint8_t  g,
uint8_t  b 
)

Generate native color value from R/G/B values.

Converts 8-bit R/G/B values to a color value native to the display.

The macro GFX_COLOR does the same, only allows the preprocessor to handle the calculations.

Parameters
r8-bit red value.
g8-bit green value.
b8-bit blue value.
Returns
Color value in display native format.

References GFX_COLOR.

void gfx_ili9325_draw_line_pixel ( gfx_coord_t  x,
gfx_coord_t  y,
gfx_color_t  color 
)

Draw a single pixel on the screen.

This function draws a single pixel on screen only setting top limit which makes it more suitable for line drawing. If outside the clipping region, nothing is drawn.

Parameters
xX coordinate of the pixel to be drawn.
yY coordinate of the pixel to be drawn.
colorColor value of the pixel in display native format.

References gfx_max_x, gfx_max_y, gfx_min_x, gfx_min_y, gfx_set_top_left_limit(), and ili9325_write_gram().

void gfx_ili9325_draw_pixel ( gfx_coord_t  x,
gfx_coord_t  y,
gfx_color_t  color 
)

Draw a single pixel on the screen.

Draw a single pixel on screen setting top and bottom limits. If outside the clipping region, nothing is drawn.

Parameters
xX coordinate of the pixel to be drawn.
yY coordinate of the pixel to be drawn.
colorColor value of the pixel in display native format.

References gfx_max_x, gfx_max_y, gfx_min_x, gfx_min_y, gfx_set_limits(), and ili9325_write_gram().

gfx_color_t gfx_ili9325_get_pixel ( gfx_coord_t  x,
gfx_coord_t  y 
)

Get the color of a pixel on the display.

Parameters
xX coordinate of the pixel to be sampled.
yY coordinate of the pixel to be sampled.
Returns
Color value of the pixel at (x, y) in display native format, or GFX_COLOR_INVALID if outside the clipping region.

References gfx_bitmap::color, GFX_COLOR_INVALID, gfx_max_x, gfx_max_y, gfx_min_x, gfx_min_y, gfx_set_limits(), and ili9325_read_gram().

void gfx_ili9325_set_orientation ( uint8_t  flags)

gfx_coord_t gfx_height

Current height of screen.

gfx_coord_t gfx_max_x

Minimum X of current clipping region.

gfx_coord_t gfx_max_y

Maximum Y of current clipping region.

gfx_coord_t gfx_min_x

Minimum X of current clipping region.

gfx_coord_t gfx_min_y

Maximum Y of current clipping region.

gfx_coord_t gfx_width

Current width of screen.