Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Frame widget

Frame widget provides a frame with border and a title bar.

It can be configured to be resizable and movable.

Typedefs

typedef bool(* wtk_frame_handler_t )(struct wtk_frame *frame, win_command_t command_data)
 Frame command event handler callback. More...
 

Functions

struct win_windowwtk_frame_as_child (struct wtk_frame *frame)
 This function returns a reference to the window that should be used when managing the widget, such as move, resize, destroy and reparenting. More...
 
struct win_windowwtk_frame_as_parent (struct wtk_frame *frame)
 This function returns a reference to the window that should be used as a parent for child widgets and windows. More...
 
struct wtk_framewtk_frame_create (struct win_window *parent, struct win_area const *area, char const *caption, bool allow_resize, wtk_frame_handler_t frame_handler, void *custom_data)
 This function creates a new frame widget. More...
 
void * wtk_frame_get_custom_data (struct wtk_frame const *frame)
 This function returns the custom data from the frame's attributes. More...
 
static bool wtk_frame_handler (struct win_window *win, enum win_event_type type, void const *data)
 This function is the window event handler for frame widgets. More...
 

typedef bool(* wtk_frame_handler_t)(struct wtk_frame *frame, win_command_t command_data)

Frame command event handler callback.

struct win_window* wtk_frame_as_child ( struct wtk_frame frame)

This function returns a reference to the window that should be used when managing the widget, such as move, resize, destroy and reparenting.

Parameters
frameFrame widget to manage.
Returns
Window to be used for managing the frame.

References Assert, and wtk_frame::container.

struct win_window* wtk_frame_as_parent ( struct wtk_frame frame)

This function returns a reference to the window that should be used as a parent for child widgets and windows.

This corresponds to the internal area inside borders and title bar.

Parameters
frameFrame widget to be a parent.
Returns
Window to be used as parent for child contents.

References Assert, and wtk_frame::contents.

struct wtk_frame* wtk_frame_create ( struct win_window parent,
struct win_area const *  area,
char const *  caption,
bool  allow_resize,
wtk_frame_handler_t  frame_handler,
void *  custom_data 
)

This function creates a new frame widget.

It allocates required memory and intializes necessary windows to create the widget. If there is not enough memory, the function returns NULL.

To destroy the widget and all its contents, and free its memory, call win_destroy() on the frame's child reference, given by wtk_frame_as_child(), like this: "win_destroy(wtk_frame_as_child(my_frame_ptr));". The frame's internal area will equal the area parameter, but the total extents will be slightly larger, to accommodate for titlebar, borders etc.

Parameters
parentParent window.
areaArea of the internal contents.
captionPointer to caption string. Will be copied into widget.
allow_resizeTrue if resize handle should be included on the frame.
frame_handlerOptional command event handler, for applications.
custom_dataOptional custom data link, for applications.
Returns
Pointer to frame, or NULL if failed.

References win_attributes::area, Assert, win_attributes::background, win_attributes::behavior, wtk_frame::caption, wtk_frame::container, wtk_frame::contents, win_attributes::custom, wtk_frame::custom_data, win_attributes::event_handler, wtk_frame::frame_handler, membag_alloc(), membag_free(), NULL, win_area::pos, wtk_frame::resize, win_area::size, wtk_frame::state, WIN_BEHAVIOR_RAISE_ON_PRESS, win_create(), win_destroy(), win_show(), wtk_copy_string(), wtk_frame_background, wtk_frame_handler(), WTK_FRAME_NORMAL, wtk_resize_frame(), win_point::x, and win_point::y.

void* wtk_frame_get_custom_data ( struct wtk_frame const *  frame)

This function returns the custom data from the frame's attributes.

The custom data can be used for e.g. linking to associated applications.

Parameters
framePointer to frame.
Returns
Copy of the custom data.

References Assert, and wtk_frame::custom_data.

static bool wtk_frame_handler ( struct win_window win,
enum win_event_type  type,
void const *  data 
)
static