Microchip® Advanced Software Framework

lwip-1.4.1/src/include/lwip/def.h File Reference
#include "lwip/arch.h"
#include "lwip/opt.h"

Macros

#define htonl(x)   lwip_htonl(x)
 
#define htons(x)   lwip_htons(x)
 
#define lwip_htonl(x)   (x)
 
#define lwip_htons(x)   (x)
 
#define LWIP_MAKE_U16(a, b)   ((a << 8) | b)
 
#define LWIP_MAX(x, y)   (((x) > (y)) ? (x) : (y))
 
#define LWIP_MIN(x, y)   (((x) < (y)) ? (x) : (y))
 
#define lwip_ntohl(x)   (x)
 
#define lwip_ntohs(x)   (x)
 
#define LWIP_PLATFORM_BYTESWAP   0
 
#define ntohl(x)   lwip_ntohl(x)
 
#define ntohs(x)   lwip_ntohs(x)
 
#define NULL   ((void *)0)
 
#define PP_HTONL(x)   (x)
 
#define PP_HTONS(x)   (x)
 
#define PP_NTOHL(x)   (x)
 
#define PP_NTOHS(x)   (x)
 

#define htonl (   x)    lwip_htonl(x)

Referenced by ipaddr_aton().

#define htons (   x)    lwip_htons(x)
#define lwip_htonl (   x)    (x)
#define lwip_htons (   x)    (x)

Referenced by lwip_ntohs().

#define LWIP_MAKE_U16 (   a,
 
)    ((a << 8) | b)
#define LWIP_MAX (   x,
 
)    (((x) > (y)) ? (x) : (y))
#define LWIP_MIN (   x,
 
)    (((x) < (y)) ? (x) : (y))

Referenced by pbuf_alloc(), and pbuf_take_at().

#define lwip_ntohl (   x)    (x)
#define lwip_ntohs (   x)    (x)
#define LWIP_PLATFORM_BYTESWAP   0
#define ntohl (   x)    lwip_ntohl(x)
#define ntohs (   x)    lwip_ntohs(x)

Referenced by ip_input().

#define NULL   ((void *)0)

Referenced by at25dfx_enable_write(), at25dfx_erase_block(), at25dfx_erase_chip(), at25dfx_protect_sector(), at45dbx_usb_read_10(), at45dbx_usb_write_10(), chipid_read(), compute_address(), configure_console(), configure_rx_dma(), configure_usart(), create_peripheral_control_semaphores(), create_task_command(), create_twi_task(), create_usart_tasks(), delete_task_command(), efc_perform_read_sequence(), emac_dev_read(), emac_dev_set_rx_callback(), emac_dev_set_tx_wakeup_callback(), emac_init_mem(), emac_process_arp_packet(), emac_process_ip_packet(), ethernet_configure_interface(), ethernetif_init(), ethernetif_input(), flash_erase_all(), flash_get_descriptor(), flash_get_wait_state(), flash_lock(), flash_set_wait_state(), flash_set_wait_state_adaptively(), flash_unlock(), FreeRTOS_CLIGetParameter(), FreeRTOS_CLIProcessCommand(), FreeRTOS_CLIRegisterCommand(), freertos_obtain_peripheral_access_semphore(), freertos_optionally_wait_transfer_completion(), freertos_start_pdc_transfer(), freertos_twi_master_init(), freertos_uart_serial_init(), freertos_uart_serial_read_packet(), freertos_usart_serial_init(), freertos_usart_serial_read_packet(), fs_open(), get_usart(), gfx_draw_char_hugemem(), gfx_draw_char_progmem(), gfx_draw_progmem_string_aligned(), gfx_draw_string_aligned(), gfx_generic_put_bitmap(), gfx_get_progmem_string_bounding_box(), gfx_get_string_bounding_box(), http_accept(), http_close_conn(), http_poll(), http_recv(), if(), ili9341_copy_pixels_to_screen(), ili9341_duplicate_pixel(), ili93xx_disable_scroll(), ili93xx_display_off(), ili93xx_display_on(), inet_chksum_pbuf(), inet_cksum_pseudo_base(), inet_cksum_pseudo_partial_base(), ip_input(), ip_output(), ip_output_if(), ip_output_if_src(), ip_route(), ipaddr_ntoa_r(), lin_rx_response(), lin_tx_header_and_response(), lin_tx_response(), local_twi_handler(), local_uart_handler(), local_usart_handler(), low_level_init(), low_level_input(), low_level_output(), main(), main_test11(), main_test12(), main_test13(), main_test14(), main_test15(), main_test16(), main_test18(), main_test20(), main_test6(), main_usb_enum_step11(), main_usb_enum_step12(), main_usb_enum_step13(), main_usb_enum_step14(), main_usb_enum_step5(), main_usb_enum_step9(), mem_free(), mem_malloc(), mem_name(), mem_realloc(), mem_trim(), membag_alloc(), membag_get_largest_free_block_size(), membag_get_smallest_free_block_size(), memp_free(), memp_init(), multi_parameter_echo_command(), mxt_init_device(), mxt_process_messages(), nand_flash_usb_read_10(), nand_flash_usb_write_10(), netif_add(), netif_find(), netif_init(), netif_remove(), netif_set_default(), netif_set_ipaddr(), nfc_copy_data_from_internal_sram(), nfc_copy_data_to_internal_sram(), pbuf_alloc(), pbuf_cat(), pbuf_clen(), pbuf_coalesce(), pbuf_copy(), pbuf_copy_partial(), pbuf_dechain(), pbuf_free(), pbuf_get_at(), pbuf_header(), pbuf_header_impl(), pbuf_memcmp(), pbuf_put_at(), pbuf_realloc(), pbuf_ref(), pbuf_skip(), pbuf_strstr(), pbuf_take(), pbuf_take_at(), portTASK_FUNCTION(), prvAddNewTaskToReadyList(), prvAllocateTCBAndStack(), prvCopyDataToQueue(), prvHeapInit(), prvHelpCommand(), prvHighestPriorityPeekTask(), prvHighPriorityMutexTask(), prvHighPriorityPeekTask(), prvInitialiseNewQueue(), prvInitialiseTaskLists(), prvInitialiseTCBVariables(), prvLowPriorityMutexTask(), prvMediumPriorityMutexTask(), prvMediumPriorityPeekTask(), prvRecursiveMutexBlockingTask(), prvRecursiveMutexControllingTask(), prvUnlockQueue(), pvPortMalloc(), run_emac_read_write_test(), run_gpbr_test(), sd_mmc_usb_read_10(), sd_mmc_usb_write_10(), ssc_dma(), ssc_set_receiver(), ssc_set_transmitter(), stdio_serial_init(), stdio_usb_init(), sys_arch_mbox_fetch(), sys_arch_mbox_tryfetch(), sys_arch_sem_wait(), sys_init(), sys_mbox_fetch(), sys_mbox_free(), sys_mbox_new(), sys_mbox_post(), sys_mbox_set_invalid(), sys_mbox_trypost(), sys_mutex_set_invalid(), sys_sem_free(), sys_sem_new(), sys_sem_set_invalid(), sys_sem_signal(), sys_sem_wait(), sys_thread_new(), sys_timeout(), sys_untimeout(), tcpip_callback_with_block(), tcpip_callbackmsg_new(), tcpip_init(), tcpip_input(), tcpip_thread(), tcpip_timeout(), tcpip_untimeout(), test_case_run(), twi_eeprom_task(), twi_get_pdc_base(), twi_master_pdc_read(), twi_master_pdc_write(), udc_iface_disable(), udc_iface_enable(), udc_process_setup(), udc_req_std_dev_get_descriptor(), udc_sof_notify(), udd_ctrl_init(), udd_ctrl_out_received(), udi_msc_trans_block(), uhc_connection_tree(), uhc_dev_get_power(), uhc_dev_get_string(), uhc_dev_get_string_manufacturer(), uhc_dev_get_string_product(), uhc_dev_get_string_serial(), uhc_dev_is_high_speed_support(), uhc_dev_reset(), uhc_enumeration_error(), uhc_enumeration_step11(), uhc_enumeration_step12(), uhc_enumeration_step13(), uhc_enumeration_step14(), uhc_enumeration_step15(), uhc_enumeration_step5(), uhc_enumeration_step9(), uhc_get_device_number(), uhc_notify_sof(), uhc_remotewakeup(), uhd_ctrl_phase_data_in(), uhd_ctrl_phase_data_out(), uhd_ctrl_request_end(), uhd_enable(), uhd_interrupt(), uhd_pipe_finish_job(), uhd_setup_request(), uhi_aoa_install(), uhi_aoa_mode_enable_step1(), uhi_aoa_mode_enable_step2(), uhi_aoa_mode_enable_step3(), uhi_aoa_register_hid(), uhi_aoa_send_hid_event(), uhi_aoa_send_info_string(), uhi_aoa_uninstall(), uhi_aoa_unregister_hid(), uhi_cdc_free_device(), uhi_cdc_get_nb_received(), uhi_cdc_get_port(), uhi_cdc_getc(), uhi_cdc_install(), uhi_cdc_is_tx_ready(), uhi_cdc_putc(), uhi_cdc_read_buf(), uhi_cdc_rx_received(), uhi_cdc_set_conf(), uhi_cdc_set_ctrl_line(), uhi_cdc_sof(), uhi_cdc_tx_send(), uhi_cdc_uninstall(), uhi_cdc_write_buf(), uhi_hid_mouse_install(), uhi_hid_mouse_uninstall(), uhi_msc_enable(), uhi_msc_enable_step1(), uhi_msc_enable_step2(), uhi_msc_get_lun(), uhi_msc_get_lun_desc(), uhi_msc_mem_read_10_ram(), uhi_msc_mem_read_capacity(), uhi_msc_mem_read_sector_size(), uhi_msc_mem_wr_protect(), uhi_msc_mem_write_10_ram(), uhi_msc_reset_endpoint(), uhi_msc_scsi_test_unit_ready(), uhi_msc_uninstall(), uhi_vendor_bulk_is_available(), uhi_vendor_control_in_run(), uhi_vendor_control_out_run(), uhi_vendor_enable(), uhi_vendor_install(), uhi_vendor_int_is_available(), uhi_vendor_iso_is_available(), uhi_vendor_uninstall(), usart_echo_tx_task(), usart_get_pdc_base(), usart_lin_handler(), usart_task(), uxListRemove(), vAltStartComTestTasks(), vCreateAltBlockTimeTasks(), vCreateBlockTimeTasks(), vCreateSuicidalTasks(), virtual_usb_trans(), vListInitialiseItem(), vListRemove(), vPortDefineHeapRegions(), vPortFree(), vSecondaryBlockTimeTestTask(), vStartAltBlockingQueueTasks(), vStartAltGenericQueueTasks(), vStartAltPolledQueueTasks(), vStartBlockingQueueTasks(), vStartCountingSemaphoreTasks(), vStartDynamicPriorityTasks(), vStartEthernetTaskLauncher(), vStartGenericQueueTasks(), vStartIntegerMathTasks(), vStartLEDFlashTasks(), vStartMathTasks(), vStartPolledQueueTasks(), vStartQueuePeekTasks(), vStartRecursiveMutexTasks(), vStartSemaphoreTasks(), vTaskStartScheduler(), win_add_top_child(), win_create(), win_destroy(), win_destroy_children(), win_draw_contents(), win_get_area(), win_get_attributes(), win_handle_pointer_event(), win_hide(), win_is_visible(), win_lower(), win_process_command_event(), win_process_keyboard_event(), win_process_pointer_event(), win_raise(), win_reparent(), win_set_area(), win_set_attributes(), win_set_keyboard_focus(), win_show(), win_unlink(), wtk_basic_frame_create(), wtk_button_create(), wtk_button_handler(), wtk_check_box_create(), wtk_check_box_handler(), wtk_frame_create(), wtk_handle_frame_release(), wtk_handle_resize_release(), wtk_icon_button_create(), wtk_icon_button_handler(), wtk_icon_group_create(), wtk_label_create(), wtk_plot_create(), wtk_plot_handler(), wtk_progress_bar_create(), wtk_radio_button_create(), wtk_radio_button_handler(), wtk_radio_group_create(), wtk_slider_create(), wtk_slider_handler(), wtk_start_drag(), xCoRoutineCreate(), xEventGroupCreate(), xQueueGenericCreate(), xQueueGenericReceive(), xQueueGenericSend(), xQueueGenericSendFromISR(), xQueueGiveFromISR(), xQueuePeek(), xQueuePeekFromISR(), xQueueReceive(), xQueueReceiveFromISR(), xStreamBufferReceive(), xStreamBufferReceiveCompletedFromISR(), xStreamBufferReset(), xStreamBufferSend(), xStreamBufferSendCompletedFromISR(), xTaskIncrementTick(), and xTaskResumeAll().

#define PP_HTONL (   x)    (x)

Referenced by netif_init().

#define PP_HTONS (   x)    (x)

Referenced by ip_input().

#define PP_NTOHL (   x)    (x)
#define PP_NTOHS (   x)    (x)