Information concerning the data transmission.
#include <twi.h>
Data Fields | |
uint8_t | addr [3] |
TWI address/commands to issue to the other chip (node). More... | |
uint32_t | addr_length |
Length of the TWI data address segment (1-3 bytes). More... | |
void * | buffer |
Where to find the data to be transferred. More... | |
uint8_t | chip |
TWI chip address to communicate with. More... | |
uint32_t | length |
How many bytes do we want to transfer. More... | |
uint8_t twi_packet::addr[3] |
TWI address/commands to issue to the other chip (node).
Referenced by at24cxx_acknowledge_polling(), at24cxx_read_byte(), at24cxx_read_continuous(), at24cxx_read_page(), at24cxx_write_byte(), at24cxx_write_continuous(), at24cxx_write_page(), freertos_twi_read_packet_async(), freertos_twi_write_packet_async(), main(), mxt_get_crc_value(), mxt_get_message_count(), mxt_probe_device(), mxt_read_config_object(), mxt_read_config_reg(), mxt_read_id_block(), mxt_read_message(), mxt_read_object_table(), mxt_write_config_object(), mxt_write_config_reg(), qt_write_regs(), read_page_from_eeprom(), twi_master_pdc_read(), twi_master_pdc_write(), twi_master_read(), twi_master_write(), twi_probe(), and write_page_to_eeprom().
uint32_t twi_packet::addr_length |
Length of the TWI data address segment (1-3 bytes).
Referenced by at24cxx_acknowledge_polling(), at24cxx_read_byte(), at24cxx_read_continuous(), at24cxx_read_page(), at24cxx_write_byte(), at24cxx_write_continuous(), at24cxx_write_page(), freertos_twi_read_packet_async(), freertos_twi_write_packet_async(), main(), qt_read_regs(), read_page_from_eeprom(), twi_master_pdc_read(), twi_master_pdc_write(), twi_master_read(), twi_master_write(), twi_probe(), wm8731_write_register(), and write_page_to_eeprom().
void* twi_packet::buffer |
Where to find the data to be transferred.
Referenced by at24cxx_acknowledge_polling(), at24cxx_read_byte(), at24cxx_read_continuous(), at24cxx_read_page(), at24cxx_write_byte(), at24cxx_write_continuous(), at24cxx_write_page(), freertos_twi_read_packet_async(), freertos_twi_write_packet_async(), main(), mxt_validate_message(), read_page_from_eeprom(), twi_master_pdc_read(), twi_master_pdc_write(), twi_master_read(), twi_master_write(), twi_probe(), wm8731_write_register(), and write_page_to_eeprom().
uint8_t twi_packet::chip |
TWI chip address to communicate with.
Referenced by at24cxx_read_byte(), at24cxx_read_continuous(), at24cxx_read_page(), at24cxx_write_byte(), at24cxx_write_continuous(), at24cxx_write_page(), freertos_twi_read_packet_async(), freertos_twi_write_packet_async(), main(), mcp980x_read_register(), mcp980x_write_register(), read_page_from_eeprom(), twi_master_pdc_read(), twi_master_pdc_write(), twi_master_read(), twi_master_write(), twi_probe(), wm8731_write_register(), and write_page_to_eeprom().
uint32_t twi_packet::length |
How many bytes do we want to transfer.
Referenced by at24cxx_acknowledge_polling(), at24cxx_read_byte(), at24cxx_read_continuous(), at24cxx_read_page(), at24cxx_write_byte(), at24cxx_write_continuous(), at24cxx_write_page(), freertos_twi_read_packet_async(), freertos_twi_write_packet_async(), main(), mcp980x_read_register(), mcp980x_write_register(), read_page_from_eeprom(), twi_master_pdc_read(), twi_master_pdc_write(), twi_master_read(), twi_master_write(), twi_probe(), wm8731_write_register(), and write_page_to_eeprom().