Macros | |
#define | TAL_FIRST_TIMER_ID (0) |
#define | TRX_CLOCK_OUTPUT_SELECTION 0 |
To configure the clock output configuration to the build, set the following define TRX_CLOCK_OUTPUT_SELECTION to the required value. More... | |
#define | TRX_IRQ_POLARITY 0 |
To change the transceiver's interrupt polarity, set the following define TRX_IRQ_POLARITY to the required value. More... | |
#define TAL_FIRST_TIMER_ID (0) |
Referenced by tal_reset().
#define TRX_CLOCK_OUTPUT_SELECTION 0 |
To configure the clock output configuration to the build, set the following define TRX_CLOCK_OUTPUT_SELECTION to the required value.
Value - meaning 0 off 1 26 MHz (default/reset) 2 32 MHz 3 16 MHz 4 8 MHz 5 4 MHz 6 2 MHz 7 1 MHz
Referenced by trx_init().
#define TRX_IRQ_POLARITY 0 |
To change the transceiver's interrupt polarity, set the following define TRX_IRQ_POLARITY to the required value.
Value - meaning 0 = Active HIGH (default/reset) 1 = Active LOW