Generic data structure used for all lwIP network interfaces.
The following fields should be filled in by the initialization function for the device driver: hwaddr_len, hwaddr[], mtu, flags
#include <netif.h>
Data Fields | |
u8_t | flags |
flags (see NETIF_FLAG_ above) More... | |
ip_addr_t | gw |
u8_t | hwaddr [NETIF_MAX_HWADDR_LEN] |
link level hardware address of this interface More... | |
u8_t | hwaddr_len |
number of bytes used in hwaddr More... | |
netif_input_fn | input |
This function is called by the network device driver to pass a packet up the TCP/IP stack. More... | |
ip_addr_t | ip_addr |
IP address configuration in network byte order. More... | |
netif_linkoutput_fn | linkoutput |
This function is called by the ARP module when it wants to send a packet on the interface. More... | |
u16_t | mtu |
maximum transfer unit (in bytes) More... | |
char | name [2] |
descriptive abbreviation More... | |
ip_addr_t | netmask |
struct netif * | next |
pointer to next in linked list More... | |
u8_t | num |
number of this interface More... | |
netif_output_fn | output |
This function is called by the IP module when it wants to send a packet on the interface. More... | |
void * | state |
This field can be set by the device driver and could point to state information for the device. More... | |
u8_t netif::flags |
flags (see NETIF_FLAG_ above)
Referenced by ip4_addr_isbroadcast(), ip_input(), ksz8851snl_low_level_init(), netif_add(), netif_remove(), netif_set_down(), netif_set_link_down(), netif_set_link_up(), netif_set_up(), and tcpip_input().
ip_addr_t netif::gw |
Referenced by netif_add(), and netif_set_gw().
u8_t netif::hwaddr |
link level hardware address of this interface
Referenced by ksz8851snl_low_level_init().
u8_t netif::hwaddr_len |
number of bytes used in hwaddr
Referenced by ksz8851snl_low_level_init().
netif_input_fn netif::input |
This function is called by the network device driver to pass a packet up the TCP/IP stack.
Referenced by ethernetif_input(), and netif_add().
ip_addr_t netif::ip_addr |
IP address configuration in network byte order.
Referenced by ip4_addr_isbroadcast(), ip_input(), ip_route(), netif_add(), and netif_set_ipaddr().
netif_linkoutput_fn netif::linkoutput |
This function is called by the ARP module when it wants to send a packet on the interface.
This function outputs the pbuf as-is on the link medium.
Referenced by ethernetif_init().
u16_t netif::mtu |
maximum transfer unit (in bytes)
Referenced by ksz8851snl_low_level_init().
char netif::name |
descriptive abbreviation
Referenced by ethernetif_init(), ip_input(), netif_add(), netif_find(), netif_set_default(), netif_set_gw(), netif_set_ipaddr(), and netif_set_netmask().
ip_addr_t netif::netmask |
Referenced by ip4_addr_isbroadcast(), ip_input(), ip_route(), netif_add(), and netif_set_netmask().
struct netif * netif::next |
pointer to next in linked list
Referenced by ip_input(), ip_route(), netif_add(), netif_find(), and netif_remove().
u8_t netif::num |
number of this interface
Referenced by netif_add(), and netif_find().
netif_output_fn netif::output |
This function is called by the IP module when it wants to send a packet on the interface.
This function typically first resolves the hardware address, then sends the packet.
Referenced by ethernetif_init().
void * netif::state |
This field can be set by the device driver and could point to state information for the device.
Referenced by ethernetif_init(), ksz8851snl_low_level_input(), ksz8851snl_low_level_output(), ksz8851snl_update(), and netif_add().