Microchip® Advanced Software Framework

nlme_pair_conf_tag Struct Reference

NLME-PAIR.confirm message structure.

#include <nwk_msg_types.h>

Data Fields

nwk_msg_code_t cmdcode ALIGN8BIT
 This identifies the message as NLME_PAIR_CONFIRM. More...
 
nwk_enum_t Status ALIGN8BIT
 
uint8_t PairingRef ALIGN8BIT
 
uint16_t RecVendorId ALIGN8BIT
 
uint8_t RecVendorString[7] ALIGN8BIT
 
uint8_t RecAppCapabilities ALIGN8BIT
 
uint8_t RecUserString[15] ALIGN8BIT
 
dev_type_t RecDevTypeList[DEVICE_TYPE_LIST_SIZEALIGN8BIT
 
profile_id_t RecProfileIdList[PROFILE_ID_LIST_SIZEALIGN8BIT