Microchip® Advanced Software Framework

nlme_pair_ind_tag Struct Reference

NLME-PAIR.indication message structure.

#include <nwk_msg_types.h>

Data Fields

nwk_msg_code_t cmdcode ALIGN8BIT
 This identifies the message as NLME_PAIR_INDICATION. More...
 
nwk_enum_t Status ALIGN8BIT
 
uint16_t SrcPANId ALIGN8BIT
 
uint64_t SrcIEEEAddr ALIGN8BIT
 
uint8_t OrgNodeCapabilities ALIGN8BIT
 
uint16_t OrgVendorId ALIGN8BIT
 
uint8_t OrgVendorString[7] ALIGN8BIT
 
uint8_t OrgAppCapabilities ALIGN8BIT
 
uint8_t OrgUserString[15] ALIGN8BIT
 
dev_type_t OrgDevTypeList[DEVICE_TYPE_LIST_SIZEALIGN8BIT
 
profile_id_t OrgProfileIdList[PROFILE_ID_LIST_SIZEALIGN8BIT
 
uint8_t KeyExTransferCount ALIGN8BIT
 
uint8_t ProvPairingRef ALIGN8BIT