Microchip® Advanced Software Framework

phy_layer_attrib_tag Struct Reference

#include <nwk_internal.h>

Data Fields

uint32_t ChannelsSupported
 
uint8_t CurrentChannel
 Current RF channel to be used for all transmissions and receptions. More...
 
uint64_t IeeeAddress
 64-bit (IEEE) address of the node. More...
 
uint16_t PANId
 16-bit PAN ID More...
 
uint16_t ShortAddress
 16-bit short address of the node. More...
 

uint32_t phy_layer_attrib_tag::ChannelsSupported
uint8_t phy_layer_attrib_tag::CurrentChannel

Current RF channel to be used for all transmissions and receptions.

uint64_t phy_layer_attrib_tag::IeeeAddress

64-bit (IEEE) address of the node.

uint16_t phy_layer_attrib_tag::PANId

16-bit PAN ID

uint16_t phy_layer_attrib_tag::ShortAddress

16-bit short address of the node.