Microchip® Advanced Software Framework

wdt_config Struct Reference

Watchdog Timer configuration structure.

Configuration structure for a Watchdog Timer instance. This structure could be initialized by the wdt_get_config_defaults() function before being modified by the user application.

#include <wdt_sam4l.h>

Data Fields

bool always_on
 If set, the watchdog will be enabled and locked to the current configuration (SFV bit). More...
 
uint32_t clk_src
 Clock source select. More...
 
bool disable_flash_cali
 Disable flash calibration redone after a watchdog reset. More...
 
bool disable_wdt_after_reset
 Disable the watchdog after a watchdog reset. More...
 
enum wdt_period timeout_period
 Number of CLK_CNT until the WDT expires. More...
 
uint32_t wdt_int
 WDT interrupt mode. More...
 
uint32_t wdt_mode
 WDT mode. More...
 
enum wdt_period window_period
 Number of CLK_CNT until the reset window opens. More...
 

bool wdt_config::always_on

If set, the watchdog will be enabled and locked to the current configuration (SFV bit).

Note
Only a reset unlocks the SFV bit.

Referenced by wdt_enable(), and wdt_get_config_defaults().

uint32_t wdt_config::clk_src

Clock source select.

Referenced by run_wdt_test_all(), wdt_get_config_defaults(), and wdt_init().

bool wdt_config::disable_flash_cali

Disable flash calibration redone after a watchdog reset.

Referenced by wdt_get_config_defaults(), and wdt_init().

bool wdt_config::disable_wdt_after_reset

Disable the watchdog after a watchdog reset.

Referenced by wdt_get_config_defaults(), wdt_init(), and wdt_reset_mcu().

enum wdt_period wdt_config::timeout_period

Number of CLK_CNT until the WDT expires.

Referenced by main(), run_wdt_test_all(), wdt_get_config_defaults(), wdt_init(), and wdt_reset_mcu().

uint32_t wdt_config::wdt_int

WDT interrupt mode.

Referenced by wdt_get_config_defaults(), and wdt_init().

uint32_t wdt_config::wdt_mode
enum wdt_period wdt_config::window_period

Number of CLK_CNT until the reset window opens.

Referenced by run_wdt_test_all(), wdt_get_config_defaults(), and wdt_init().