This file contains the SAM4L QTouch Library pin, register and sensors configuration options for Capacitive Touch acquisition using the CATB module.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | AT_DISCHARGE_PIN_SELECTED (DIS_PB03) |
Autonomous QTouch Discharge pin selected. More... | |
#define | AT_SP_SELECTED (SP_PB04) |
Autonomous QTouch Sensor Pin selected. More... | |
Acquisition method manifest constants. | |
The following constants can be used to select the desired Touch acquisition methods to be used with the SAM4L QTouch Library. Choose QTouch, and Autonomous QTouch methods by setting the corresponding macro to 1. | |
#define | DEF_TOUCH_QTOUCH (1) |
When 1, QTouch Group A method acquisition is used. More... | |
#define | DEF_TOUCH_AUTONOMOUS_QTOUCH (1) |
When 1, Autonomous QTouch method acquisition is used. More... | |
#define | DEF_TOUCH_QDEBUG_ENABLE_QT (0) |
Enable/Disable QDebug for touch debug information communication with QTouch Studio PC Software. More... | |
#define | DEF_TOUCH_QDEBUG_ENABLE_AT (0) |
#define | DEF_TOUCH_QDEBUG_ENABLE |
QTouch Pin Configuration Options. | |
#define | QT_SENSOR_PINS_SELECTED SP_PB04, SP_PA04, SP_PA05, SP_PB02 |
QTouch Sensor pins's selected. More... | |
#define | QT_NUM_SENSOR_PINS_SELECTED (4u) |
QTouch Number of Sensor pins's. More... | |
#define | QT_DISCHARGE_PIN_SELECTED (DIS_PB03) |
QTouch Discharge pin selected. More... | |
QTouch Sensor Configuration options. | |
#define | QT_NUM_SENSORS (2u) |
QTouch number of Sensors. More... | |
#define | QT_NUM_ROTORS_SLIDERS (1u) |
QTouch number of Rotors and Sliders. More... | |
QTouch Clock and Register Configuration Options. | |
#define | QT_CLOCK_SEL (0u) |
CATB Clock Acquisition Clock Source Select 0: The RC oscillator is selected as acquisition clock and is used as timing source for the measurements. More... | |
#define | QT_DISCHARGET (1000u) |
CATB Discharge time. More... | |
#define | QT_CHARGET (0u) |
CATB Charge time. More... | |
#define | QT_REPEAT (3u) |
CATB Repeat measurements. More... | |
QTouch DMA Channel Options. | |
#define | QT_DMA_CHANNEL_0 (0u) |
QTouch DMA Channel 0. More... | |
#define | QT_DMA_CHANNEL_1 (1u) |
QTouch DMA Channel 0. More... | |
QTouch Global acquisition parameters. | |
Refer the Touch Library User guide for more information on these parameters. | |
#define | QT_DI (4u) |
QTouch Sensor detect integration (DI) limit. More... | |
#define | QT_NEG_DRIFT_RATE (20u) |
QTouch Sensor negative drift rate. More... | |
#define | QT_POS_DRIFT_RATE (5u) |
QTouch Sensor positive drift rate. More... | |
#define | QT_MAX_ON_DURATION (0u) |
QTouch Sensor maximum on duration. More... | |
#define | QT_DRIFT_HOLD_TIME (20u) |
QTouch Sensor drift hold time. More... | |
#define | QT_POS_RECAL_DELAY (10u) |
QTouch Positive Recalibration delay. More... | |
#define | QT_RECAL_THRESHOLD (RECAL_50) |
QTouch Sensor recalibration threshold. More... | |
QTouch Callback functions. | |
#define | QT_FILTER_CALLBACK (NULL) |
QTouch Filter callback function. More... | |
Autonomous QTouch Clock and Register Configuration Options. | |
#define | AT_CLOCK_SEL (0u) |
CATB Clock Acquisition Clock Source Select 0: The RC oscillator is selected as acquisition clock and is used as timing source for the measurements. More... | |
#define | AT_DISCHARGET (2000000u) |
CATB Discharge time. More... | |
#define | AT_CHARGET (0u) |
CATB Charge time. More... | |
#define | AT_REPEAT (0u) |
CATB Repeat measurements. More... | |
#define | AT_SPREAD (0u) |
Enable/Disable Spread Spectrum based acquisition. More... | |
#define | AT_THRESHOLD (15u) |
#define | AT_DI (3u) |
QTouch Sensor detect integration (DI) limit. More... | |
#define AT_CHARGET (0u) |
CATB Charge time.
Select the Number of CATB Acquisition clock cycles to provide time to Charge.
#define AT_CLOCK_SEL (0u) |
CATB Clock Acquisition Clock Source Select 0: The RC oscillator is selected as acquisition clock and is used as timing source for the measurements.
1: The GCLK is selected as acquisition clock and is used as the timing source for measurements.
#define AT_DI (3u) |
QTouch Sensor detect integration (DI) limit.
Range: 0u to 255u.
#define AT_DISCHARGE_PIN_SELECTED (DIS_PB03) |
Autonomous QTouch Discharge pin selected.
Specify the Discharge pins to be used for QTouch. Refer qt_discharge_pin_options_t enum in touch_api_sam4l.h file.
#define AT_DISCHARGET (2000000u) |
CATB Discharge time.
Select the Number of CATB Acquisition clock cycles to provide time to Discharge.
#define AT_REPEAT (0u) |
CATB Repeat measurements.
Select the Number of times acquisition should be repeated. Range: 0u to 8u.
#define AT_SP_SELECTED (SP_PB04) |
Autonomous QTouch Sensor Pin selected.
Specify the Sense pair to be used for Autonomous QTouch. Refer qt_sensor_pin_options_t enum in touch_api_sam4l.h file.
#define AT_SPREAD (0u) |
Enable/Disable Spread Spectrum based acquisition.
#define AT_THRESHOLD (15u) |
#define DEF_TOUCH_AUTONOMOUS_QTOUCH (1) |
When 1, Autonomous QTouch method acquisition is used.
When 0, Autonomous QTouch method acquisition is not used.
#define DEF_TOUCH_QDEBUG_ENABLE |
#define DEF_TOUCH_QDEBUG_ENABLE_AT (0) |
#define DEF_TOUCH_QDEBUG_ENABLE_QT (0) |
Enable/Disable QDebug for touch debug information communication with QTouch Studio PC Software.
When 1, QDebug debug data communication to QTouch Studio is enabled. When 0, QDebug debug data communication to QTouch Studio is disabled.
#define DEF_TOUCH_QTOUCH (1) |
When 1, QTouch Group A method acquisition is used.
When 0, QTouch Group A method acquisition is not used.
#define QT_CHARGET (0u) |
CATB Charge time.
Select the Number of CATB Acquisition clock cycles to provide time to Charge.The measured capacitance is charged for 2^(CHARGET) clcok cycles of the acquisition clock(selected with CKSEL) before each discharge measurement.
#define QT_CLOCK_SEL (0u) |
CATB Clock Acquisition Clock Source Select 0: The RC oscillator is selected as acquisition clock and is used as timing source for the measurements.
1: The GCLK is selected as acquisition clock and is used as the timing source for measurements.
#define QT_DI (4u) |
QTouch Sensor detect integration (DI) limit.
Range: 0u to 255u.
#define QT_DISCHARGE_PIN_SELECTED (DIS_PB03) |
QTouch Discharge pin selected.
Specify the Discharge pins to be used for QTouch. Refer qt_discharge_pin_options_t enum in touch_api_sam4l.h file.
#define QT_DISCHARGET (1000u) |
CATB Discharge time.
Select the Number of CATB Acquisition clock cycles to provide time to Discharge.
#define QT_DMA_CHANNEL_0 (0u) |
QTouch DMA Channel 0.
Specify the DMA Channel option 0 to be used by the CATB module to transfer Sensor configuration data from memory to CATB registers.. Range: 0u to 11u.
Referenced by touch_sensors_measure().
#define QT_DMA_CHANNEL_1 (1u) |
QTouch DMA Channel 0.
Specify the DMA Channel option 0 to be used by the CAT module to transfer Sensor configuration data from CATB registers to memory. Range: 0u to 11u.
Referenced by touch_sensors_measure().
#define QT_DRIFT_HOLD_TIME (20u) |
QTouch Sensor drift hold time.
Units: 200ms Default value: 20 (hold off drifting for 4 seconds after leaving detect). Range: 1u to 255u.
#define QT_FILTER_CALLBACK (NULL) |
QTouch Filter callback function.
A filter callback (when not NULL) is called by the Touch Library each time a new set of Signal values are available. An Example filter callback function prototype. void qt_filter_callback( touch_filter_data_t *p_filter_data );
#define QT_MAX_ON_DURATION (0u) |
QTouch Sensor maximum on duration.
Units: 200ms (Example: a value 5u indicated Max ON duration of 1 second.) Default value: 0 (No maximum ON time limit). Range: 0u to 255u.
#define QT_NEG_DRIFT_RATE (20u) |
QTouch Sensor negative drift rate.
Units: 200ms Default value: 20u = 4 seconds. Range: 1u to 127u.
#define QT_NUM_ROTORS_SLIDERS (1u) |
QTouch number of Rotors and Sliders.
Specify the total number of QTouch Rotors and Sliders to be used by the Touch Library. The number of Rotors and Sliders mentioned here is part of the Total number of sensors specified in the QT_NUM_SENSORS macro. When no rotors or slider are required, specify a value of 0u.
#define QT_NUM_SENSOR_PINS_SELECTED (4u) |
QTouch Number of Sensor pins's.
Specify the Total number of Sensor pins's selected using the QT_SENSOR_PINS_SELECTED macro.
#define QT_NUM_SENSORS (2u) |
QTouch number of Sensors.
Specify the number of QTouch touch sensors to be used by the Touch Library. A sensor is either a key, rotor or slider. Example configuration: If the configuration has 6 keys (a key is formed using one Sensor Pin), one rotor (a QTouch rotor is formed using 3 Sensor Pins) and one slider (a QTouch slider is formed using 3 Sensor Pins), then the number of sensors is 6 key + 1 rotor + 1 slider = 8 sensors. Range: 1u to QT_NUM_SENSOR_PINS_SELECTED.
#define QT_POS_DRIFT_RATE (5u) |
QTouch Sensor positive drift rate.
Units: 200ms Default value: 5u = 1 second. Range: 1u to 127u.
#define QT_POS_RECAL_DELAY (10u) |
QTouch Positive Recalibration delay.
Default value: 10. Range: 1u to 255u.
#define QT_RECAL_THRESHOLD (RECAL_50) |
QTouch Sensor recalibration threshold.
Default: RECAL_50 (recalibration threshold = 50% of detection threshold). Range: refer recal_threshold_t enum in touch_api_sam4l.h.
#define QT_REPEAT (3u) |
CATB Repeat measurements.
Select the Number of times acquisition should be repeated. Range: 0u to 8u.
QTouch Sensor pins's selected.
Specify the Sensor pins's to be used for QTouch, seperated by a comma. Refer qt_sensor_pin_options_t enum in touch_api_sam4l.h file.
NOTE: DO NOT INCLUDE BRACKETS (), SINCE THIS MACRO IS BEING PLACED INSIDE AN ARRAY.