BLE DTM.
Copyright (c) 2017-2018 Microchip Technology Inc. and its subsidiaries.
#include <asf.h>
#include "platform.h"
#include "at_ble_api.h"
#include "at_ble_trace.h"
#include "console_serial.h"
#include "serial_fifo.h"
#include "ble_utils.h"
#include "conf_serialdrv.h"
#include "serial_bridge.h"
#include "conf_extint.h"
#include "serial_drv.h"
#include "timer_hw.h"
Functions | |
static void | ble_critical_alert (uint32_t on_ms, uint32_t off_ms) |
static void | ble_dtm_init (void) |
static void | ble_init (void) |
void | button_cb (void) |
int | main (void) |
Variables | |
uint32_t | event_params_memory [256] = {0} |
uint32_t | event_pool_memory [256] = {0} |
at_ble_init_config_t | pf_cfg |
uint32_t | rx_fifo_memory [256] = {0} |
PRINT EVENTS | |
volatile bool | button_pressed = false |
Determine if button is pressed. More... | |
|
static |
References delay_ms.
Referenced by ble_init().
|
static |
References ble_init().
Referenced by main().
|
static |
UART baudrate value one of at_ble_uart_baudrate_tag values
References platform_api_list_tag::at_ble_create_signal, platform_api_list_tag::at_ble_create_timer, platform_api_list_tag::at_ble_delete_signal, platform_api_list_tag::at_ble_delete_timer, platform_api_list_tag::at_ble_gpio_set, at_ble_init(), platform_api_list_tag::at_ble_reconfigure_usart, platform_api_list_tag::at_ble_recv_async, platform_api_list_tag::at_ble_reset_signal, platform_api_list_tag::at_ble_send_sync, platform_api_list_tag::at_ble_sleep, platform_api_list_tag::at_ble_start_timer, platform_api_list_tag::at_ble_stop_timer, AT_BLE_SUCCESS, platform_api_list_tag::at_ble_trigger_signal, AT_BLE_UART, platform_api_list_tag::at_ble_wait_for_signal, AT_BTLC1000_MR, AT_BTLC1000_ZR, ble_critical_alert(), BTLC1000_EXT_PIN9, at_ble_init_config_t::btlc1000_module_version, at_ble_bus_info_t::btlc1000_uart_pinout_switch, at_ble_bus_info_t::bus_baudrate, at_ble_init_config_t::bus_info, at_ble_bus_info_t::bus_type, at_ble_init_config_t::event_mem_pool, at_ble_init_config_t::event_params_mem_pool, event_params_memory, event_pool_memory, at_ble_bus_info_t::host_external_wakeup_gpio, at_ble_init_config_t::memPool, at_ble_mempool_t::memSize, at_ble_mempool_t::memStartAdd, NULL, at_ble_init_config_t::platform_api_list, platform_configure_hw_fc_uart(), platform_configure_primary_uart(), platform_create_signal(), platform_create_timer(), platform_delete_signal(), platform_delete_timer(), platform_dtm_interface_receive(), platform_gpio_set(), platform_init(), platform_recv_async(), platform_reset_signal(), platform_send_sync(), platform_sleep(), platform_start_timer(), platform_stop_timer(), platform_trigger_signal(), platform_wait_for_signal(), at_ble_init_config_t::rx_fifo_mem_pool, rx_fifo_memory, TRACE_LVL_DISABLE, and trace_set_level().
Referenced by ble_dtm_init().
void button_cb | ( | void | ) |
References button_pressed.
int main | ( | void | ) |
References platform_api_list_tag::at_ble_create_timer, platform_api_list_tag::at_ble_delete_timer, AT_BLE_EXTERNAL_WAKEUP, platform_api_list_tag::at_ble_gpio_set, AT_BLE_HIGH, platform_api_list_tag::at_ble_reconfigure_usart, platform_api_list_tag::at_ble_recv_async, platform_api_list_tag::at_ble_send_sync, platform_api_list_tag::at_ble_sleep, platform_api_list_tag::at_ble_start_timer, platform_api_list_tag::at_ble_stop_timer, ble_dtm_init(), board_init(), delay_init, NULL, at_ble_init_config_t::platform_api_list, platform_gpio_set(), platform_start_rx(), platform_stop_stack_timers(), serial_bridge_init(), serial_bridge_task(), and sysclk_init().
uint32_t event_params_memory[256] = {0} |
uint32_t event_pool_memory[256] = {0} |
at_ble_init_config_t pf_cfg |
uint32_t rx_fifo_memory[256] = {0} |