This module contains WILC BSP APIs declarations.
Copyright (c) 2016-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | BSP_MIN(x, y) ((x)>(y)?(y):(x)) |
#define | CONST const |
#define | FALSE (0) |
#define | NM_BSP_B_L_16(x) (x) |
#define | NM_BSP_B_L_32(x) (x) |
#define | NMI_API |
#define | NULL ((void*)0) |
#define | TRUE (1) |
Typedefs | |
typedef signed short | sint16 |
Range of values between -32768 to 32767. More... | |
typedef signed long | sint32 |
Range of values between -2147483648 to 2147483647. More... | |
typedef signed char | sint8 |
Range of values between -128 to 127. More... | |
typedef void(* | tpfNmBspIsr )(void) |
Pointer to function. Used as a data type of ISR function registered by nm_bsp_register_isr. More... | |
typedef unsigned short | uint16 |
Range of values between 0 to 65535. More... | |
typedef unsigned long | uint32 |
Range of values between 0 to 4294967295. More... | |
typedef unsigned char | uint8 |
Range of values between 0 to 255. More... | |
Functions | |
sint8 | nm_bsp_deinit (void) |
De-iInitialize BSP. More... | |
void | nm_bsp_free (void *pvMemBuffer) |
Free memory. More... | |
sint8 | nm_bsp_init (void) |
Initialization for bsp (Board Support Package) such as Reset and Chip Enable Pins for WILC, delays, register ISR, enable/disable IRQ for WILC, ...etc. You must use this function in the head of your application to enable WILC and Host Driver communicate each other. More... | |
void | nm_bsp_interrupt_ctrl (uint8 u8Enable) |
Enable/Disable interrupts. More... | |
void * | nm_bsp_malloc (uint32 u32Size) |
Allocate memory. More... | |
void | nm_bsp_register_isr (tpfNmBspIsr pfIsr) |
Register the host interface interrupt service routine. More... | |
void | nm_bsp_reset (void) |
Reset NMC1500 SoC by setting CHIP_EN and RESET_N signals low, CHIP_EN high then RESET_N high. More... | |
void | nm_bsp_sleep (uint32 u32TimeMsec) |
Used to put the host to sleep for the specified duration (in milliseconds). Forcing the host to sleep for extended period may lead to host not being able to respond to WINC board events. It is important to be considerate while choosing the sleep period. More... | |
#define NM_BSP_B_L_16 | ( | x | ) | (x) |
#define NM_BSP_B_L_32 | ( | x | ) | (x) |
Referenced by m2m_wifi_set_static_ip(), recv(), and recvfrom().