QSPI flash memory driver for S25FL1XX.
Copyright (c) 2015-2018 Microchip Technology Inc. and its subsidiaries.
|
static uint8_t | s25fl1xx_check_protected_addr (uint8_t status1, uint32_t addr) |
| Check weather the address of addr is protected. More...
|
|
void | s25fl1xx_continous_read_mode_reset (struct qspid_t *qspid) |
| Issue 'CContinuous Read Mode' command, the device can return to normal SPI command mode, in which all commands can be accepts. More...
|
|
uint8_t | s25fl1xx_data_protect (struct qspid_t *qspid, bool dir, enum block_size protect_size) |
| Protect the contents of the serial flash device. More...
|
|
uint8_t | s25fl1xx_data_unprotect (struct qspid_t *qspid) |
| Unprotected the contents of the serial flash device. More...
|
|
static void | s25fl1xx_disable_write (struct qspid_t *qspid) |
| Disable write option to serial flash memory. More...
|
|
void | s25fl1xx_enable_wrap (struct qspid_t *qspid, uint8_t byte_align) |
| Enables critical writes operation on a serial flash device, such as sector protection, status register, etc. More...
|
|
static void | s25fl1xx_enable_write (struct qspid_t *qspid) |
| Enable write option to serial flash memory. More...
|
|
void | s25fl1xx_enter_continous_read_mode (struct qspid_t *qspid) |
| Reads data from the specified address on the serial flash. More...
|
|
uint8_t | s25fl1xx_erase_64k_block (struct qspid_t *qspid, uint32_t address) |
| Erases the specified 64KB block of the serial firmware dataflash. More...
|
|
uint8_t | s25fl1xx_erase_chip (struct qspid_t *qspid) |
| Erases all the content of the memory chip. More...
|
|
uint8_t | s25fl1xx_erase_sector (struct qspid_t *qspid, uint32_t address) |
| Erases the specified block of the serial firmware dataflash. More...
|
|
static void | s25fl1xx_exec_command (struct qspid_t *qspid, uint8_t instr, uint32_t *tx_data, uint32_t *rx_data, enum qspi_access read_write, uint32_t size) |
| Send command to the serial flash. More...
|
|
enum status_code | s25fl1xx_initialize (Qspi *qspi, struct qspi_config_t *mode_config, uint32_t use_default_config) |
| Initialize QSPI serial memory mode. More...
|
|
static void | s25fl1xx_memory_access (struct qspid_t *qspid, uint8_t instr, uint32_t addr, uint32_t *tx_data, uint32_t *rx_data, enum qspi_access read_write, uint32_t size, uint8_t secure) |
| Read/write data from serial flash memory. More...
|
|
uint8_t | s25fl1xx_protect (struct qspid_t *qspid) |
| Unprotected the contents of the serial flash device. More...
|
|
uint8_t | s25fl1xx_read (struct qspid_t *qspid, uint32_t *data, uint32_t size, uint32_t address) |
| Reads data from the specified address on the serial flash. More...
|
|
uint8_t | s25fl1xx_read_dual (struct qspid_t *qspid, uint32_t *data, uint32_t size, uint32_t address) |
| Reads data from the specified address on the serial flash. More...
|
|
uint8_t | s25fl1xx_read_dual_io (struct qspid_t *qspid, uint32_t *data, uint32_t size, uint32_t address, uint8_t cont_mode, uint8_t secure) |
| Reads data from the specified address on the serial flash. More...
|
|
uint32_t | s25fl1xx_read_jedec_id (struct qspid_t *qspid) |
| Reads and returns the serial flash device ID. More...
|
|
uint8_t | s25fl1xx_read_quad (struct qspid_t *qspid, uint32_t *data, uint32_t size, uint32_t address) |
| Reads data from the specified address on the serial flash. More...
|
|
uint8_t | s25fl1xx_read_quad_io (struct qspid_t *qspid, uint32_t *data, uint32_t size, uint32_t address, uint8_t cont_mode, uint8_t secure) |
| Reads data from the specified address on the serial flash. More...
|
|
static uint32_t | s25fl1xx_read_status (struct qspid_t *qspid) |
| Reads and returns the status register of the serial flash. More...
|
|
static uint8_t | s25fl1xx_read_status1 (struct qspid_t *qspid) |
| Reads and returns the status register of the serial flash. More...
|
|
static uint8_t | s25fl1xx_read_status2 (struct qspid_t *qspid) |
| Reads and returns the status register of the serial flash. More...
|
|
static uint8_t | s25fl1xx_read_status3 (struct qspid_t *qspid) |
| Reads and returns the status register of the serial flash. More...
|
|
void | s25fl1xx_set_quad_mode (struct qspid_t *qspid, uint8_t mode) |
| Enables critical writes operation on a serial flash device, such as sector protection, status register, etc. More...
|
|
void | s25fl1xx_set_read_latency_control (struct qspid_t *qspid, uint8_t latency) |
| Enables critical writes operation on a serial flash device, such as sector protection, status register, etc. More...
|
|
void | s25fl1xx_soft_reset (struct qspid_t *qspid) |
| s25fl1d software reset. More...
|
|
uint8_t | s25fl1xx_unprotect (struct qspid_t *qspid) |
| Unprotected the control bits of the serial flash device. More...
|
|
static void | s25fl1xx_wait_memory_access_end (struct qspid_t *qspid) |
| Wait for transfer to finish calling the SPI driver ISR. More...
|
|
uint8_t | s25fl1xx_write (struct qspid_t *qspid, uint32_t *pdata, uint32_t size, uint32_t address, uint8_t secure) |
| Writes data at the specified address on the serial firmware dataflash. More...
|
|
static void | s25fl1xx_write_status (struct qspid_t *qspid, uint8_t *status) |
| Writes the given value in the status register of the serial flash device. More...
|
|
static void | s25fl1xx_write_volatile_status (struct qspid_t *qspid, uint8_t *status) |
| Writes the given value in the status register of the serial flash device. More...
|
|