LCD Glass component.
This is the quick start guide for the Display - ILI93XX Controller, with step-by-step instructions on how to configure and use the driver for a specific use case.The code examples can be copied into e.g the main application loop or any other function that will need to control the ili93xx LCD Glass component module. Now ili9325 and ili9341 are supported.
This use case will demonstrate how to initialize the ili93xx LCD Glass module.
This module requires the following driver
Add this to the main loop or a setup function: