This module contains M2M Wi-Fi APIs implementation.
Copyright (c) 2016-2021 Microchip Technology Inc. and its subsidiaries.
#include "driver/include/m2m_wifi.h"
#include "driver/source/m2m_hif.h"
#include "driver/source/nmasic.h"
#include <string.h>
Macros | |
#define | WIFI_1X_TLS_HS_FLAGS_DEFAULT |
#define | WIFI_1X_TLS_HS_FLAGS_PEER_AUTH NBIT1 |
#define | WIFI_1X_TLS_HS_FLAGS_PEER_CERTTIMECHECK NBIT2 |
#define | WIFI_1X_TLS_HS_FLAGS_REQUIRE_TIME NBIT3 |
#define | WIFI_1X_TLS_HS_FLAGS_RSV5 NBIT5 |
#define | WIFI_1X_TLS_HS_FLAGS_RSV7 NBIT7 |
#define | WIFI_1X_TLS_HS_FLAGS_SESSION_CACHING NBIT4 |
#define | WIFI_1X_TLS_HS_FLAGS_SPECIFY_ROOTCERT NBIT6 |
Functions | |
static sint8 | m2m_validate_ap_parameters (CONST tstrM2MAPModeConfig *pstrM2MAPModeConfig) |
static sint8 | m2m_validate_scan_options (tstrM2MScanOption *ptstrM2MScanOption) |
sint8 | m2m_wifi_1x_get_option (tenu1xOption enuOptionName, void *pOptionValue, size_t *pOptionLen) |
API to get (read) options relating to Wi-Fi connection using WPA(2) Enterprise authentication. More... | |
sint8 | m2m_wifi_1x_set_option (tenu1xOption enuOptionName, const void *pOptionValue, size_t OptionLen) |
API to set (write) options relating to Wi-Fi connection using WPA(2) Enterprise authentication. More... | |
static void | m2m_wifi_cb (uint8 u8OpCode, uint16 u16DataSize, uint32 u32Addr) |
NMI_API sint8 | m2m_wifi_conf_auto_rate (tstrConfAutoRate *pstrConfAutoRate) |
Allow the host MCU app to configure auto TX rate selection algorithm. The application can use this API to tweak the algorithm performance. Moreover, it allows the application to force a specific WLAN PHY rate for transmitted data packets to favor range vs. throughput needs. More... | |
sint8 | m2m_wifi_configure_sntp (uint8 *pu8NTPServerName, uint8 u8NTPServerNameLength, tenuSNTPUseDHCP useDHCP) |
Configures what NTP server the SNTP client should use. More... | |
sint8 | m2m_wifi_connect (char *pcSsid, uint8 u8SsidLen, uint8 u8SecType, void *pvAuthInfo, uint16 u16Ch) |
Legacy asynchronous API to request connection to a specified access point. More... | |
sint8 | m2m_wifi_connect_1x_mschap2 (tenuCredStoreOption enuCredStoreOption, tstrNetworkId *pstrNetworkId, tstrAuth1xMschap2 *pstrAuth1xMschap2) |
Asynchronous API to connect to an access point using WPA(2) Enterprise authentication with MS-CHAP-V2 credentials. More... | |
sint8 | m2m_wifi_connect_1x_tls (tenuCredStoreOption enuCredStoreOption, tstrNetworkId *pstrNetworkId, tstrAuth1xTls *pstrAuth1xTls) |
Asynchronous API to connect to an access point using WPA(2) Enterprise authentication with MS-CHAP-V2 credentials. More... | |
sint8 | m2m_wifi_connect_open (tenuCredStoreOption enuCredStoreOption, tstrNetworkId *pstrNetworkId) |
Asynchronous API to connect to an access point using open authentication. More... | |
static sint8 | m2m_wifi_connect_prepare_msg (tenuCredStoreOption enuCredStoreOption, tenuM2mSecType enuAuthType, uint16 u16AuthSize, tstrNetworkId *pstrNetworkId, tstrM2mWifiConnHdr *pstrWifiConn) |
sint8 | m2m_wifi_connect_psk (tenuCredStoreOption enuCredStoreOption, tstrNetworkId *pstrNetworkId, tstrAuthPsk *pstrAuthPsk) |
Asynchronous API to connect to an access point using WPA(2) PSK authentication. More... | |
sint8 | m2m_wifi_connect_sc (char *pcSsid, uint8 u8SsidLen, uint8 u8SecType, void *pvAuthInfo, uint16 u16Ch, uint8 u8NoSaveCred) |
Legacy asynchronous API to request connection to a specific AP with the option to save credentials in Flash. More... | |
sint8 | m2m_wifi_connect_wep (tenuCredStoreOption enuCredStoreOption, tstrNetworkId *pstrNetworkId, tstrAuthWep *pstrAuthWep) |
Asynchronous API to connect to an access point using WEP authentication. More... | |
sint8 | m2m_wifi_default_connect (void) |
Asynchronous API that attempts to reconnect to the last-associated access point. More... | |
sint8 | m2m_wifi_deinit (void *arg) |
Synchronous API to de-initialize the WINC driver and host interface. More... | |
sint8 | m2m_wifi_delete_sc (char *pcSsid, uint8 u8SsidLen) |
Asynchronous API that deletes connection credentials (PSK, WEP key, 802.1X password) from WINC flash. Either deletes all credentials, or for a specific SSID. More... | |
sint8 | m2m_wifi_disable_ap (void) |
Synchronous API to disable access point mode on the WINC. More... | |
sint8 | m2m_wifi_disable_roaming (void) |
Disable WiFi STA roaming. More... | |
sint8 | m2m_wifi_disconnect (void) |
Synchronous API to request disconnection from a network. More... | |
sint8 | m2m_wifi_download_mode () |
Prepares the WINC before downloading any data (Firmware, Certificates, etc). More... | |
sint8 | m2m_wifi_enable_ap (CONST tstrM2MAPConfig *pstrM2MAPConfig) |
Asynchronous API to enable access point (AKA "hot-spot") mode on the WINC. More... | |
sint8 | m2m_wifi_enable_ap_ext (CONST tstrM2MAPModeConfig *pstrM2MAPModeConfig) |
Asynchronous API to enable access point (AKA "hot-spot") mode on the WINC with extended options. More... | |
sint8 | m2m_wifi_enable_dhcp (uint8 u8DhcpEn) |
Asynchronous function to control the DHCP client functionality within the WINC. More... | |
sint8 | m2m_wifi_enable_firmware_logs (uint8 u8Enable) |
Enable or Disable logs in run time (Disable Firmware logs will enhance the firmware start-up time and performance) More... | |
sint8 | m2m_wifi_enable_roaming (uint8 bEnableDhcp) |
Enable WiFi STA roaming. More... | |
sint8 | m2m_wifi_enable_sntp (uint8 bEnable) |
Asynchronous API to enable or disable the native Simple Network Time Protocol(SNTP) client running on the WINC. More... | |
sint8 | m2m_wifi_enable_XO_during_sleep (uint8 bXOSleepEnable) |
Specifies whether the crystal oscillator is left on or off during deep sleep (defaults to off). More... | |
sint8 | m2m_wifi_get_connection_info (void) |
Asynchronous API for retrieving the WINC connection status. More... | |
sint8 | m2m_wifi_get_firmware_version (tstrM2mRev *pstrRev) |
Synchronous API to obtain the firmware version currently running on the WINC IC. More... | |
sint8 | m2m_wifi_get_mac_address (uint8 *pu8MacAddr) |
Request the current MAC address of the device (the working mac address). (the function is Blocking until response received) More... | |
uint8 | m2m_wifi_get_num_ap_found (void) |
Reads the number of AP's found in the last Scan Request, The function read the number of AP's from global variable which updated in the wifi_cb in M2M_WIFI_RESP_SCAN_DONE. More... | |
sint8 | m2m_wifi_get_otp_mac_address (uint8 *pu8MacAddr, uint8 *pu8IsValid) |
Request the MAC address stored on the OTP (one time programmable) memory of the device. (the function is Blocking until response received) More... | |
uint8 | m2m_wifi_get_sleep_mode (void) |
Get the current Power save mode. More... | |
uint8 | m2m_wifi_get_state (void) |
Get the wifi state. More... | |
sint8 | m2m_wifi_get_system_time (void) |
Asynchronous API to obtain the system time in use by the WINC. More... | |
sint8 | m2m_wifi_handle_events (void *arg) |
Synchronous M2M event handler function. More... | |
sint8 | m2m_wifi_init (tstrWifiInitParam *pWifiInitParam) |
Synchronous API to initialize the WINC driver. More... | |
sint8 | m2m_wifi_init_hold () |
First part of m2m_wifi_init, up to the point of initializing SPI for flash access. More... | |
sint8 | m2m_wifi_init_start (tstrWifiInitParam *pWifiInitParam) |
Second part of m2m_wifi_init, continuing from where m2m_wifi_init_hold left off. More... | |
sint8 | m2m_wifi_p2p (uint8 u8Channel) |
sint8 | m2m_wifi_p2p_disconnect (void) |
sint8 | m2m_wifi_prng_get_random_bytes (uint8 *pu8PrngBuff, uint16 u16PrngSize) |
Get random bytes using the PRNG bytes. More... | |
sint8 | m2m_wifi_reinit (tstrWifiInitParam *pWifiInitParam) |
De-initialize and then initialize wifi. Resets the WINC. More... | |
sint8 | m2m_wifi_reinit_hold (void) |
First part of m2m_wifi_reinit, up to the point of initializing SPI for flash access. More... | |
sint8 | m2m_wifi_reinit_start (tstrWifiInitParam *pWifiInitParam) |
Second part of m2m_wifi_reinit, continuing from where m2m_wifi_reinit_hold left off. More... | |
sint8 | m2m_wifi_req_client_ctrl (uint8 u8Cmd) |
Send a command to the PS Client (An WINC board running the ps_firmware), if the PS client send any commands it will be received in wifi_cb M2M_WIFI_RESP_CLIENT_INFO. More... | |
sint8 | m2m_wifi_req_curr_rssi (void) |
Request the current RSSI for the current connected AP, the response received in wifi_cb M2M_WIFI_RESP_CURRENT_RSSI. More... | |
sint8 | m2m_wifi_req_scan_result (uint8 index) |
Reads the AP information from the Scan Result list with the given index, the response received in wifi_cb M2M_WIFI_RESP_SCAN_RESULT, the response pointer should be casted with tstrM2mWifiscanResult structure. More... | |
sint8 | m2m_wifi_req_server_init (uint8 ch) |
Initialize the PS Server, The WINC support non secure communication with another WINC, (SERVER/CLIENT) through one byte command (probe request and probe response) without any connection setup. More... | |
sint8 | m2m_wifi_request_dhcp_client (void) |
Legacy (deprecated) Asynchronous API for starting a DHCP client on the WINC. More... | |
sint8 | m2m_wifi_request_dhcp_server (uint8 *addr) |
Legacy (deprecated) asynchronous function to start a DHCP client on the WINC. More... | |
sint8 | m2m_wifi_request_scan (uint8 ch) |
Asynchronous API to request the WINC to scan for networks. More... | |
sint8 | m2m_wifi_request_scan_passive (uint8 ch, uint16 scan_time) |
Similar to m2m_wifi_request_scan but performs passive scanning instead of active scanning. More... | |
sint8 | m2m_wifi_request_scan_ssid_list (uint8 ch, uint8 *u8Ssidlist) |
Asynchronous wi-fi scan request on the given channel and the hidden scan list. More... | |
sint8 | m2m_wifi_request_sleep (uint32 u32SlpReqTime) |
Asynchronous API to place the WINC into sleep mode for a specified period of time. More... | |
sint8 | m2m_wifi_send_crl (tstrTlsCrlInfo *pCRL) |
Asynchronous API that notifies the WINC with the Certificate Revocation List. More... | |
sint8 | m2m_wifi_send_ethernet_pkt (uint8 *pu8Packet, uint16 u16PacketSize) |
Asynchronous API to queue an Ethernet packet for transmission by the WINC. More... | |
sint8 | m2m_wifi_set_battery_voltage (uint16 u16BattVoltx100) |
Set the battery voltage to update the firmware calculations. Not implemented in WINC3400 firmware. More... | |
sint8 | m2m_wifi_set_cust_InfoElement (uint8 *pau8M2mCustInfoElement) |
Asynchronous API to add or remove a user-defined Information Element. More... | |
sint8 | m2m_wifi_set_device_name (uint8 *pu8DeviceName, uint8 u8DeviceNameLength) |
Set the WINC3400 device name which is used as P2P device name. More... | |
sint8 | m2m_wifi_set_gain_table_idx (uint8 u8GainTableIdx) |
set the gain table index corresponding to a specific WiFi region More... | |
sint8 | m2m_wifi_set_gains (tstrM2mWifiGainsParams *pstrM2mGain) |
Set the chip PPA gain for 11b/11gn. More... | |
sint8 | m2m_wifi_set_lsn_int (tstrM2mLsnInt *pstrM2mLsnInt) |
Set the Wi-Fi listen interval for power save operation. It is represented in units of AP Beacon periods. More... | |
sint8 | m2m_wifi_set_mac_address (uint8 au8MacAddress[6]) |
Asynchronous API for assigning a MAC address to the WINC. More... | |
sint8 | m2m_wifi_set_power_profile (uint8 u8PwrMode) |
Change the power profile mode Not implemented in WINC3400 firmware. More... | |
sint8 | m2m_wifi_set_scan_options (tstrM2MScanOption *ptstrM2MScanOption) |
Synchronous API for configuring the behaviour of the WINC network scanning functions. More... | |
sint8 | m2m_wifi_set_scan_region (uint16 ScanRegion) |
Synchronous API for configuring the regulatory restrictions that may affect the WINC scanning behaviour. More... | |
sint8 | m2m_wifi_set_sleep_mode (uint8 PsTyp, uint8 BcastEn) |
Set the power saving mode for the WINC3400. More... | |
sint8 | m2m_wifi_set_static_ip (tstrM2MIPConfig *pstrStaticIPConf) |
Asynchronous API to manually assign a (static) IP address to the WINC. More... | |
sint8 | m2m_wifi_set_stop_scan_on_first (uint8 u8StopScanOption) |
Synchronous API for enabling/disabling the stop scan on first result of the WINC IC's network scanning functions. More... | |
sint8 | m2m_wifi_set_system_time (uint32 u32UTCSeconds) |
Asynchronous function for setting the system time within the WINC. More... | |
sint8 | m2m_wifi_set_tx_power (uint8 u8TxPwrLevel) |
set the TX power tenuM2mTxPwrLevel More... | |
sint8 | m2m_wifi_start_provision_mode (tstrM2MAPConfig *pstrM2MAPConfig, char *pcHttpServerDomainName, uint8 bEnableHttpRedirect) |
Asynchronous API for control of Wi-Fi provisioning functionality. More... | |
sint8 | m2m_wifi_start_provision_mode_ext (tstrM2MAPModeConfig *pstrAPModeConfig, char *pcHttpServerDomainName, uint8 bEnableHttpRedirect) |
Asynchronous API for control of Wi-Fi provisioning functionality with extended options. More... | |
sint8 | m2m_wifi_stop_provision_mode (void) |
Synchronous API for terminating provisioning mode on the WINC. More... | |
sint8 | m2m_wifi_wps (uint8 u8TriggerType, const char *pcPinNumber) |
Asynchronous API to engage the WINC Wi-Fi Protected Setup (enrollee) function. More... | |
sint8 | m2m_wifi_wps_disable (void) |
Asynchronous API that disables Wi-Fi Protected Setup mode in the WINC. More... | |
void | m2m_wifi_yield (void) |
Yield from processing more synchronous M2M events. More... | |
Variables | |
static uint8 | gau81xRootSha1 [20] = {0} |
static tpfAppWifiCb | gpfAppWifiCb = NULL |
static uint32 | gu321xTlsHsFlags = WIFI_1X_TLS_HS_FLAGS_DEFAULT |
static volatile uint8 | gu8ChNum |
static volatile uint8 | gu8scanInProgress = 0 |
static volatile uint8 | gu8WifiState = WIFI_STATE_DEINIT |