This struct includes everything that is necessary to execute a function for a netconn in another thread context (mainly used to process netconns in the tcpip_thread context to be thread safe).
#include <api_msg.h>
Data Fields | |
struct netconn * | conn |
The netconn which to process - always needed: it includes the semaphore which is used to block the application thread until the function finished. More... | |
err_t | err |
The return value of the function executed in tcpip_thread. More... | |
union { | |
struct { | |
ip_addr_t * ipaddr | |
u8_t local | |
u16_t * port | |
} ad | |
used for do_getaddr More... | |
struct netbuf * b | |
used for do_send More... | |
struct { | |
ip_addr_t * ipaddr | |
u16_t port | |
} bc | |
used for do_bind and do_connect More... | |
struct { | |
u8_t proto | |
} n | |
used for do_newconn More... | |
struct { | |
u32_t len | |
} r | |
used for do_recv More... | |
struct { | |
u8_t shut | |
} sd | |
used for do_close (/shutdown) More... | |
struct { | |
u8_t apiflags | |
const void * dataptr | |
size_t len | |
} w | |
used for do_write More... | |
} | msg |
Depending on the executed function, one of these union members is used. More... | |
struct { ... } api_msg_msg::ad |
used for do_getaddr
Referenced by do_getaddr(), and netconn_getaddr().
u8_t api_msg_msg::apiflags |
struct netbuf* api_msg_msg::b |
used for do_send
Referenced by do_send(), and netconn_send().
struct { ... } api_msg_msg::bc |
used for do_bind and do_connect
Referenced by do_bind(), do_connect(), netconn_bind(), and netconn_connect().
struct netconn* api_msg_msg::conn |
The netconn which to process - always needed: it includes the semaphore which is used to block the application thread until the function finished.
Referenced by do_bind(), do_close(), do_connect(), do_delconn(), do_disconnect(), do_getaddr(), do_listen(), do_newconn(), do_recv(), do_send(), do_write(), netconn_accept(), netconn_bind(), netconn_close_shutdown(), netconn_connect(), netconn_delete(), netconn_disconnect(), netconn_getaddr(), netconn_listen_with_backlog(), netconn_new_with_proto_and_callback(), netconn_recv_data(), netconn_recved(), netconn_send(), netconn_write_partly(), pcb_new(), and tcpip_apimsg().
const void* api_msg_msg::dataptr |
err_t api_msg_msg::err |
The return value of the function executed in tcpip_thread.
Referenced by do_bind(), do_close(), do_close_internal(), do_connect(), do_connected(), do_delconn(), do_disconnect(), do_getaddr(), do_listen(), do_newconn(), do_recv(), do_send(), do_write(), do_writemore(), err_tcp(), pcb_new(), and tcpip_apimsg().
ip_addr_t* api_msg_msg::ipaddr |
size_t api_msg_msg::len |
u32_t api_msg_msg::len |
u8_t api_msg_msg::local |
union { ... } api_msg_msg::msg |
Depending on the executed function, one of these union members is used.
Referenced by do_bind(), do_close(), do_close_internal(), do_connect(), do_delconn(), do_getaddr(), do_listen(), do_recv(), do_send(), do_write(), do_writemore(), netconn_bind(), netconn_close_shutdown(), netconn_connect(), netconn_getaddr(), netconn_listen_with_backlog(), netconn_new_with_proto_and_callback(), netconn_recv_data(), netconn_recved(), netconn_send(), netconn_write_partly(), and pcb_new().
struct { ... } api_msg_msg::n |
used for do_newconn
Referenced by netconn_new_with_proto_and_callback(), and pcb_new().
u16_t api_msg_msg::port |
u16_t* api_msg_msg::port |
u8_t api_msg_msg::proto |
struct { ... } api_msg_msg::r |
used for do_recv
Referenced by do_recv(), netconn_recv_data(), and netconn_recved().
struct { ... } api_msg_msg::sd |
used for do_close (/shutdown)
Referenced by do_close(), do_close_internal(), do_delconn(), and netconn_close_shutdown().
u8_t api_msg_msg::shut |
struct { ... } api_msg_msg::w |
used for do_write
Referenced by do_write(), do_writemore(), and netconn_write_partly().