#include "lwip/opt.h"
#include "lwip/api_msg.h"
#include "lwip/netifapi.h"
#include "lwip/pbuf.h"
#include "lwip/api.h"
#include "lwip/sys.h"
#include "lwip/timers.h"
#include "lwip/netif.h"
Data Structures | |
struct | tcpip_msg |
Macros | |
#define | LOCK_TCPIP_CORE() |
#define | LWIP_TCPIP_THREAD_ALIVE() |
Define this to something that triggers a watchdog. More... | |
#define | TCPIP_APIMSG(m) tcpip_apimsg(m) |
#define | TCPIP_APIMSG_ACK(m) sys_sem_signal(&m->conn->op_completed) |
#define | tcpip_callback(f, ctx) tcpip_callback_with_block(f, ctx, 1) |
#define | TCPIP_NETIFAPI(m) tcpip_netifapi(m) |
#define | TCPIP_NETIFAPI_ACK(m) sys_sem_signal(&m->sem) |
#define | UNLOCK_TCPIP_CORE() |
Typedefs | |
typedef void(* | tcpip_callback_fn )(void *ctx) |
Function prototype for functions passed to tcpip_callback() More... | |
typedef void(* | tcpip_init_done_fn )(void *arg) |
Function prototype for the init_done function passed to tcpip_init. More... | |
Enumerations | |
enum | tcpip_msg_type { TCPIP_MSG_API, TCPIP_MSG_INPKT, TCPIP_MSG_TIMEOUT, TCPIP_MSG_UNTIMEOUT, TCPIP_MSG_CALLBACK, TCPIP_MSG_CALLBACK_STATIC } |
Functions | |
err_t | mem_free_callback (void *m) |
A simple wrapper function that allows you to free heap memory from interrupt context. More... | |
err_t | pbuf_free_callback (struct pbuf *p) |
A simple wrapper function that allows you to free a pbuf from interrupt context. More... | |
err_t | tcpip_apimsg (struct api_msg *apimsg) |
Call the lower part of a netconn_* function This function is then running in the thread context of tcpip_thread and has exclusive access to lwIP core code. More... | |
err_t | tcpip_callback_with_block (tcpip_callback_fn function, void *ctx, u8_t block) |
Call a specific function in the thread context of tcpip_thread for easy access synchronization. More... | |
void | tcpip_callbackmsg_delete (struct tcpip_callback_msg *msg) |
Free a callback message allocated by tcpip_callbackmsg_new(). More... | |
struct tcpip_callback_msg * | tcpip_callbackmsg_new (tcpip_callback_fn function, void *ctx) |
Allocate a structure for a static callback message and initialize it. More... | |
void | tcpip_init (tcpip_init_done_fn tcpip_init_done, void *arg) |
Initialize this module: More... | |
err_t | tcpip_input (struct pbuf *p, struct netif *inp) |
Pass a received packet to tcpip_thread for input processing. More... | |
err_t | tcpip_timeout (u32_t msecs, sys_timeout_handler h, void *arg) |
call sys_timeout in tcpip_thread More... | |
err_t | tcpip_trycallback (struct tcpip_callback_msg *msg) |
Try to post a callback-message to the tcpip_thread mbox This is intended to be used to send "static" messages from interrupt context. More... | |
err_t | tcpip_untimeout (sys_timeout_handler h, void *arg) |
call sys_untimeout in tcpip_thread More... | |
#define LOCK_TCPIP_CORE | ( | ) |
Referenced by do_write(), tcpip_input(), and tcpip_thread().
#define LWIP_TCPIP_THREAD_ALIVE | ( | ) |
Define this to something that triggers a watchdog.
This is called from tcpip_thread after processing a message.
Referenced by tcpip_thread().
#define TCPIP_APIMSG | ( | m | ) | tcpip_apimsg(m) |
#define TCPIP_APIMSG_ACK | ( | m | ) | sys_sem_signal(&m->conn->op_completed) |
Referenced by do_bind(), do_disconnect(), do_getaddr(), do_listen(), do_newconn(), do_recv(), do_send(), and do_write().
#define tcpip_callback | ( | f, | |
ctx | |||
) | tcpip_callback_with_block(f, ctx, 1) |
#define TCPIP_NETIFAPI | ( | m | ) | tcpip_netifapi(m) |
#define TCPIP_NETIFAPI_ACK | ( | m | ) | sys_sem_signal(&m->sem) |
#define UNLOCK_TCPIP_CORE | ( | ) |
Referenced by do_write(), tcpip_input(), and tcpip_thread().
Function prototype for functions passed to tcpip_callback()
Function prototype for the init_done function passed to tcpip_init.
enum tcpip_msg_type |
A simple wrapper function that allows you to free heap memory from interrupt context.
m | the heap memory to free |
References mem_free(), and tcpip_callback_with_block().
A simple wrapper function that allows you to free a pbuf from interrupt context.
p | The pbuf (chain) to be dereferenced. |
References pbuf_free_int(), and tcpip_callback_with_block().
Call the lower part of a netconn_* function This function is then running in the thread context of tcpip_thread and has exclusive access to lwIP core code.
apimsg | a struct containing the function to call and its parameters |
References tcpip_msg::apimsg, api_msg_msg::conn, api_msg_msg::err, ERR_VAL, api_msg::msg, tcpip_msg::msg, netconn::op_completed, sys_arch_sem_wait(), sys_mbox_post(), sys_mbox_valid(), TCPIP_MSG_API, and tcpip_msg::type.
Referenced by netconn_close_shutdown(), netconn_connect(), and netconn_delete().
err_t tcpip_callback_with_block | ( | tcpip_callback_fn | function, |
void * | ctx, | ||
u8_t | block | ||
) |
Call a specific function in the thread context of tcpip_thread for easy access synchronization.
A function called in that way may access lwIP core code without fearing concurrent access.
f | the function to call |
ctx | parameter passed to f |
block | 1 to block until the request is posted, 0 to non-blocking mode |
References tcpip_msg::cb, tcpip_msg::ctx, ERR_MEM, ERR_OK, ERR_VAL, memp_free(), memp_malloc(), tcpip_msg::msg, NULL, sys_mbox_post(), sys_mbox_trypost(), sys_mbox_valid(), TCPIP_MSG_CALLBACK, and tcpip_msg::type.
Referenced by mem_free_callback(), and pbuf_free_callback().
void tcpip_callbackmsg_delete | ( | struct tcpip_callback_msg * | msg | ) |
Free a callback message allocated by tcpip_callbackmsg_new().
msg | the message to free |
References memp_free().
struct tcpip_callback_msg* tcpip_callbackmsg_new | ( | tcpip_callback_fn | function, |
void * | ctx | ||
) |
Allocate a structure for a static callback message and initialize it.
This is intended to be used to send "static" messages from interrupt context.
function | the function to call |
ctx | parameter passed to function |
References tcpip_msg::cb, tcpip_msg::ctx, memp_malloc(), tcpip_msg::msg, NULL, TCPIP_MSG_CALLBACK_STATIC, and tcpip_msg::type.
void tcpip_init | ( | tcpip_init_done_fn | initfunc, |
void * | arg | ||
) |
Initialize this module:
initfunc | a function to call when tcpip_thread is running and finished initializing |
arg | argument to pass to initfunc |
References arg, ERR_OK, LWIP_ASSERT, lwip_init(), NULL, sys_mbox_new(), sys_mutex_new, sys_thread_new(), tcpip_init_done, tcpip_init_done_arg, TCPIP_MBOX_SIZE, tcpip_thread(), TCPIP_THREAD_PRIO, and TCPIP_THREAD_STACKSIZE.
Referenced by init_ethernet().
Pass a received packet to tcpip_thread for input processing.
p | the received packet, p->payload pointing to the Ethernet header or to an IP header (if inp doesn't have NETIF_FLAG_ETHARP or NETIF_FLAG_ETHERNET flags) |
inp | the network interface on which the packet was received |
References ERR_MEM, ERR_OK, ERR_VAL, ethernet_input(), netif::flags, tcpip_msg::inp, ip_input(), LOCK_TCPIP_CORE, LWIP_DEBUGF, memp_free(), memp_malloc(), tcpip_msg::msg, NETIF_FLAG_ETHARP, NETIF_FLAG_ETHERNET, NULL, tcpip_msg::p, sys_mbox_trypost(), sys_mbox_valid(), TCPIP_DEBUG, TCPIP_MSG_INPKT, tcpip_msg::type, and UNLOCK_TCPIP_CORE.
Referenced by ethernet_configure_interface(), and netif_init().
err_t tcpip_timeout | ( | u32_t | msecs, |
sys_timeout_handler | h, | ||
void * | arg | ||
) |
call sys_timeout in tcpip_thread
msec | time in milliseconds for timeout |
h | function to be called on timeout |
arg | argument to pass to timeout function h |
References arg, ERR_MEM, ERR_OK, ERR_VAL, h, memp_malloc(), tcpip_msg::msecs, tcpip_msg::msg, NULL, sys_mbox_post(), sys_mbox_valid(), TCPIP_MSG_TIMEOUT, tcpip_msg::tmo, and tcpip_msg::type.
err_t tcpip_trycallback | ( | struct tcpip_callback_msg * | msg | ) |
Try to post a callback-message to the tcpip_thread mbox This is intended to be used to send "static" messages from interrupt context.
msg | pointer to the message to post |
References ERR_VAL, sys_mbox_trypost(), and sys_mbox_valid().
err_t tcpip_untimeout | ( | sys_timeout_handler | h, |
void * | arg | ||
) |
call sys_untimeout in tcpip_thread
msec | time in milliseconds for timeout |
h | function to be called on timeout |
arg | argument to pass to timeout function h |
References arg, ERR_MEM, ERR_OK, ERR_VAL, h, memp_malloc(), tcpip_msg::msg, NULL, sys_mbox_post(), sys_mbox_valid(), TCPIP_MSG_UNTIMEOUT, tcpip_msg::tmo, and tcpip_msg::type.