This file contains TAL API function declarations.
#include <stdint.h>
#include <stdbool.h>
#include "pal.h"
#include "tal_config.h"
#include "bmm.h"
#include "stack_config.h"
#include "return_val.h"
#include "tal_types.h"
#include "mac_build_config.h"
Data Structures | |
struct | frame_info_tag |
Globally used frame information structure. More... | |
union | pib_value_t |
PIB attribute value type. More... | |
Macros | |
#define | BAND_2400 (1) |
2.4 GHz (channels 11 through 26) More... | |
#define | BAND_900 (0) |
868 / 910 MHz (channels 0 through 10) using BPSK More... | |
#define | mac_i_pan_coordinator (0x0B) |
Attribute id of mac_i_pan_coordinator PIB. More... | |
#define | MAX_FRAME_DURATION (NO_OF_SYMBOLS_PREAMBLE_SFD + (aMaxPHYPacketSize + 1) * SYMBOLS_PER_OCTET) |
Maximum number of symbols in a frame for the current PHY. More... | |
#define | MAX_SYMBOL_TIME (0x0FFFFFFF) |
The maximum time in symbols for a 32 bit timer. More... | |
#define | NO_OF_SYMBOLS_PREAMBLE_SFD (NO_SYMBOLS_PREAMBLE + NO_SYMBOLS_SFD) |
Number of symbols forming the synchronization header (SHR) for the current PHY. More... | |
#define | NO_SYMBOLS_PREAMBLE (8) |
#define | NO_SYMBOLS_SFD (2) |
#define | RF_BAND BAND_2400 |
#define | SYMBOL_MASK (0x0FFFFFFF) |
Symbol mask for ingnoring most significant nibble. More... | |
#define | SYMBOLS_PER_OCTET (2) |
4 bits form one symbol since O-QPSK is used More... | |
#define | TAL_CONVERT_SYMBOLS_TO_US(symbols) ((uint32_t)(symbols) << 4) |
Conversion of symbols to microseconds. More... | |
#define | TAL_CONVERT_US_TO_SYMBOLS(time) ((time) >> 4) |
Conversion of microseconds to symbols. More... | |
#define | TAL_GET_BEACON_INTERVAL_TIME(BO) ((1UL * aBaseSuperframeDuration) << (BO)) |
Beacon Interval time in symbols. More... | |
#define | TAL_GET_SUPERFRAME_DURATION_TIME(SO) ((1UL * aBaseSuperframeDuration) << (SO)) |
Superframe Duration time in symbols. More... | |
Typedefs | |
typedef enum csma_mode_tag | csma_mode_t |
CSMA Mode supported by transceiver. More... | |
typedef struct frame_info_tag | frame_info_t |
Globally used frame information structure. More... | |
typedef enum sleep_mode_tag | sleep_mode_t |
Sleep Mode supported by transceiver. More... | |
Enumerations | |
enum | csma_mode_tag { NO_CSMA_NO_IFS, NO_CSMA_WITH_IFS, CSMA_UNSLOTTED, CSMA_SLOTTED } |
CSMA Mode supported by transceiver. More... | |
enum | SHORTENUM { ASSOCIATIONREQUEST = (0x01), ASSOCIATIONRESPONSE, DISASSOCIATIONNOTIFICATION, DATAREQUEST, PANIDCONFLICTNOTIFICAION, ORPHANNOTIFICATION, BEACONREQUEST, COORDINATORREALIGNMENT, ORPHANREALIGNMENT, BEACON_MESSAGE, DATAREQUEST_IMPL_POLL, NULL_FRAME, MCPS_MESSAGE } |
MAC Message types. More... | |
enum | sleep_mode_tag { SLEEP_MODE_1 } |
Sleep Mode supported by transceiver. More... | |
Functions | |
static uint32_t | tal_add_time_symbols (uint32_t a, uint32_t b) |
Adds two time values. More... | |
void | tal_generate_rand_seed (void) |
Generates a 16-bit random number used as initial seed for srand() More... | |
retval_t | tal_init (void) |
Initializes the TAL. More... | |
retval_t | tal_pib_get (uint8_t attribute, uint8_t *value) |
Gets a TAL PIB attribute. More... | |
retval_t | tal_pib_set (uint8_t attribute, pib_value_t *value) |
Sets a TAL PIB attribute. More... | |
retval_t | tal_reset (bool set_default_pib) |
Resets TAL state machine and sets the default PIB values if requested. More... | |
uint8_t | tal_rx_enable (uint8_t state) |
Switches receiver on or off. More... | |
void | tal_rx_frame_cb (frame_info_t *rx_frame) |
User call back function for frame reception. More... | |
static uint32_t | tal_sub_time_symbols (uint32_t a, uint32_t b) |
Subtract two time values. More... | |
void | tal_task (void) |
TAL task handling. More... | |
retval_t | tal_trx_sleep (sleep_mode_t mode) |
Sets the transceiver to sleep. More... | |
retval_t | tal_trx_wakeup (void) |
Wakes up the transceiver from sleep. More... | |
retval_t | tal_tx_frame (frame_info_t *tx_frame, csma_mode_t csma_mode, bool perform_frame_retry) |
Requests to TAL to transmit frame. More... | |
void | tal_tx_frame_done_cb (retval_t status, frame_info_t *frame) |
User call back function for frame transmission. More... | |
Variables | |
uint8_t | tal_pib_CCAMode |
CCA Mode. More... | |
uint8_t | tal_pib_CurrentChannel |
Current RF channel to be used for all transmissions and receptions. More... | |
uint8_t | tal_pib_CurrentPage |
Current channel page. More... | |
uint64_t | tal_pib_IeeeAddress |
64-bit (IEEE) address of the node. More... | |
uint8_t | tal_pib_MaxBE |
The maximum value of the backoff exponent BE in the CSMA-CA algorithm. More... | |
uint8_t | tal_pib_MaxCSMABackoffs |
The maximum number of back-offs the CSMA-CA algorithm will attempt before declaring a CSMA_CA failure. More... | |
uint16_t | tal_pib_MaxFrameDuration |
Maximum number of symbols in a frame: = phySHRDuration + ceiling([aMaxPHYPacketSize + 1] x phySymbolsPerOctet) More... | |
uint8_t | tal_pib_MaxFrameRetries |
The maximum number of retries allowed after a transmission failure. More... | |
uint8_t | tal_pib_MinBE |
The minimum value of the backoff exponent BE in the CSMA-CA algorithm. More... | |
uint16_t | tal_pib_PANId |
16-bit PAN ID More... | |
bool | tal_pib_PrivatePanCoordinator |
Indicates if the node is a PAN coordinator or not. More... | |
uint16_t | tal_pib_ShortAddress |
16-bit short address of the node. More... | |
uint8_t | tal_pib_SHRDuration |
Duration of the synchronization header (SHR) in symbols for the current PHY. More... | |
uint32_t | tal_pib_SupportedChannels |
Supported channels. More... | |
uint8_t | tal_pib_SymbolsPerOctet |
Number of symbols per octet for the current PHY. More... | |
uint8_t | tal_pib_TransmitPower |
Default value of transmit power of transceiver using IEEE defined format of phyTransmitPower. More... | |
#define BAND_2400 (1) |
2.4 GHz (channels 11 through 26)
#define BAND_900 (0) |
868 / 910 MHz (channels 0 through 10) using BPSK
#define mac_i_pan_coordinator (0x0B) |
Attribute id of mac_i_pan_coordinator PIB.
#define MAX_FRAME_DURATION (NO_OF_SYMBOLS_PREAMBLE_SFD + (aMaxPHYPacketSize + 1) * SYMBOLS_PER_OCTET) |
Maximum number of symbols in a frame for the current PHY.
This value is the base for the PHY PIB attribute phyMaxFrameDuration.
#define MAX_SYMBOL_TIME (0x0FFFFFFF) |
The maximum time in symbols for a 32 bit timer.
Referenced by tal_sub_time_symbols().
#define NO_OF_SYMBOLS_PREAMBLE_SFD (NO_SYMBOLS_PREAMBLE + NO_SYMBOLS_SFD) |
Number of symbols forming the synchronization header (SHR) for the current PHY.
This value is the base for the PHY PIB attribute phySHRDuration.
#define NO_SYMBOLS_PREAMBLE (8) |
#define NO_SYMBOLS_SFD (2) |
#define RF_BAND BAND_2400 |
#define SYMBOL_MASK (0x0FFFFFFF) |
Symbol mask for ingnoring most significant nibble.
Referenced by tal_add_time_symbols(), and tal_sub_time_symbols().
#define SYMBOLS_PER_OCTET (2) |
4 bits form one symbol since O-QPSK is used
#define TAL_CONVERT_SYMBOLS_TO_US | ( | symbols | ) | ((uint32_t)(symbols) << 4) |
Conversion of symbols to microseconds.
#define TAL_CONVERT_US_TO_SYMBOLS | ( | time | ) | ((time) >> 4) |
Conversion of microseconds to symbols.
#define TAL_GET_BEACON_INTERVAL_TIME | ( | BO | ) | ((1UL * aBaseSuperframeDuration) << (BO)) |
Beacon Interval time in symbols.
#define TAL_GET_SUPERFRAME_DURATION_TIME | ( | SO | ) | ((1UL * aBaseSuperframeDuration) << (SO)) |
Superframe Duration time in symbols.
typedef enum csma_mode_tag csma_mode_t |
CSMA Mode supported by transceiver.
typedef struct frame_info_tag frame_info_t |
Globally used frame information structure.
typedef enum sleep_mode_tag sleep_mode_t |
Sleep Mode supported by transceiver.
enum csma_mode_tag |
enum SHORTENUM |
enum sleep_mode_tag |
|
inlinestatic |
Adds two time values.
This function adds two time values
a | Time value 1 |
b | Time value 2 |
References SYMBOL_MASK.
void tal_generate_rand_seed | ( | void | ) |
Generates a 16-bit random number used as initial seed for srand()
This function generates a 16-bit random number by means of using the Random Number Generator from the transceiver. The Random Number Generator generates 2-bit random values. These 2-bit random values are concatenated to the required 16-bit random seed. The generated random 16-bit number is feed into function srand() as initial seed. The transceiver state is initally set to RX_ON. After the completion of the random seed generation, the trancseiver is set to TRX_OFF.
retval_t tal_init | ( | void | ) |
Initializes the TAL.
This function is called to initialize the TAL. The transceiver is initialized, the TAL PIBs are set to their default values, and the TAL state machine is set to TAL_IDLE state.
retval_t tal_pib_get | ( | uint8_t | attribute, |
uint8_t * | value | ||
) |
Gets a TAL PIB attribute.
This function is called to retrieve the transceiver information base attributes.
[in] | attribute | TAL infobase attribute ID |
[out] | value | TAL infobase attribute value |
retval_t tal_pib_set | ( | uint8_t | attribute, |
pib_value_t * | value | ||
) |
Sets a TAL PIB attribute.
This function is called to set the transceiver information base attributes.
attribute | TAL infobase attribute ID |
value | TAL infobase attribute value to be set |
retval_t tal_reset | ( | bool | set_default_pib | ) |
Resets TAL state machine and sets the default PIB values if requested.
set_default_pib | Defines whether PIB values need to be set to its default values |
uint8_t tal_rx_enable | ( | uint8_t | state | ) |
Switches receiver on or off.
This function switches the receiver on (PHY_RX_ON) or off (PHY_TRX_OFF).
state | New state of receiver |
void tal_rx_frame_cb | ( | frame_info_t * | rx_frame | ) |
User call back function for frame reception.
rx_frame | Pointer to received frame structure of type frame_info_t or to received frame array |
|
inlinestatic |
Subtract two time values.
This function subtracts two time values taking care of roll over.
a | Time value 1 |
b | Time value 2 |
References MAX_SYMBOL_TIME, and SYMBOL_MASK.
void tal_task | ( | void | ) |
TAL task handling.
This function
retval_t tal_trx_sleep | ( | sleep_mode_t | mode | ) |
Sets the transceiver to sleep.
This function sets the transceiver to sleep state.
mode | Defines sleep mode of transceiver SLEEP or PHY_TRX_OFF) |
retval_t tal_trx_wakeup | ( | void | ) |
Wakes up the transceiver from sleep.
This function awakes the transceiver from sleep state.
retval_t tal_tx_frame | ( | frame_info_t * | tx_frame, |
csma_mode_t | csma_mode, | ||
bool | perform_frame_retry | ||
) |
Requests to TAL to transmit frame.
This function is called by the MAC to deliver a frame to the TAL to be transmitted by the transceiver.
tx_frame | Pointer to the frame_info_t structure or to frame array to be transmitted |
csma_mode | Indicates mode of csma-ca to be performed for this frame |
perform_frame_retry | Indicates whether to retries are to be performed for this frame |
void tal_tx_frame_done_cb | ( | retval_t | status, |
frame_info_t * | frame | ||
) |
User call back function for frame transmission.
status | Status of frame transmission attempt |
frame | Pointer to frame structure of type frame_info_t |
uint8_t tal_pib_CCAMode |
CCA Mode.
uint8_t tal_pib_CurrentChannel |
Current RF channel to be used for all transmissions and receptions.
uint8_t tal_pib_CurrentPage |
Current channel page.
uint64_t tal_pib_IeeeAddress |
64-bit (IEEE) address of the node.
uint8_t tal_pib_MaxBE |
The maximum value of the backoff exponent BE in the CSMA-CA algorithm.
uint8_t tal_pib_MaxCSMABackoffs |
The maximum number of back-offs the CSMA-CA algorithm will attempt before declaring a CSMA_CA failure.
uint16_t tal_pib_MaxFrameDuration |
Maximum number of symbols in a frame: = phySHRDuration + ceiling([aMaxPHYPacketSize + 1] x phySymbolsPerOctet)
uint8_t tal_pib_MaxFrameRetries |
The maximum number of retries allowed after a transmission failure.
uint8_t tal_pib_MinBE |
The minimum value of the backoff exponent BE in the CSMA-CA algorithm.
uint16_t tal_pib_PANId |
16-bit PAN ID
bool tal_pib_PrivatePanCoordinator |
Indicates if the node is a PAN coordinator or not.
uint16_t tal_pib_ShortAddress |
16-bit short address of the node.
uint8_t tal_pib_SHRDuration |
Duration of the synchronization header (SHR) in symbols for the current PHY.
uint32_t tal_pib_SupportedChannels |
Supported channels.
uint8_t tal_pib_SymbolsPerOctet |
Number of symbols per octet for the current PHY.
uint8_t tal_pib_TransmitPower |
Default value of transmit power of transceiver using IEEE defined format of phyTransmitPower.