Functions | |
eExecStatus | e_ethernet_cmd_get_config (eModId xModId, signed short FsNavId, int ac, signed portCHAR *av[], signed portCHAR **ppcStringReply) |
The set sensor config command: set the value of a config field of a sensor. Takes three parameters. The first parameter is the sensor's name, the second parameter is the config field name, the third parameter is the value. Format: set_sensor_config sensorname field=value. More... | |
eExecStatus | e_ethernet_cmd_set_config (eModId xModId, signed short FsNavId, int ac, signed portCHAR *av[], signed portCHAR **ppcStringReply) |
The get sensor config command: get the config fields value of a sensor. Takes one parameter, that is the sensor's name. Format: get_sensor_config sensorname. More... | |
eExecStatus | e_ip_stat (eModId xModId, signed short FsNavId, int ac, signed portCHAR *av[], signed portCHAR **ppcStringReply) |
The development only ip statck stats: display the TCP/IP stack stats on COM2. No parameters. Format: ipstat. More... | |
portTASK_FUNCTION (vStartEthernetTask, pvParameters) | |
configure lwIP and MACB, start lwIP layer, start servers tasks through lwIP services. More... | |
void | v_ethernet_stopResources (void) |
Stop the Ethernet module resources. More... | |
void | vEthernetGetGWAddr (portCHAR *pcConfig) |
get the current GW address : formatted as follow : XXX.XXX.XXX.XXX More... | |
void | vEthernetGetIPAddr (portCHAR *pcConfig) |
get the current IP address : formatted as follow : XXX.XXX.XXX.XXX More... | |
void | vEthernetGetMACAddr (portCHAR *pcConfig) |
get the current MAC address : formatted as follow : XX:XX:XX:XX:XX:XX More... | |
void | vEthernetGetSubnetMask (portCHAR *pcConfig) |
get the current Subnet mask : formatted as follow : XXX.XXX.XXX.XXX More... | |
void | vStartEthernetTaskLauncher (unsigned portBASE_TYPE uxPriority) |
Create the vStartEthernetTask task. More... | |
eExecStatus e_ethernet_cmd_get_config | ( | eModId | xModId, |
signed short | FsNavId, | ||
int | ac, | ||
signed portCHAR * | av[], | ||
signed portCHAR ** | ppcStringReply | ||
) |
The set sensor config command: set the value of a config field of a sensor. Takes three parameters. The first parameter is the sensor's name, the second parameter is the config field name, the third parameter is the value. Format: set_sensor_config sensorname field=value.
xModId | Input. The module that is calling this function. |
FsNavId | Ignored. |
ac | Input. The argument counter. For this command, should be 3. |
av | Input. The argument vector. |
ppcStringReply | Input/Output. The response string. If Input is NULL, no response string will be output. Else a malloc for the response string is performed here; the caller must free this string. |
References buf, NULL, pvPortMalloc(), SHELL_ERRMSG_MEMALLOC, SHELL_EXECSTATUS_KO, SHELL_EXECSTATUS_OK, vEthernetGetGWAddr(), vEthernetGetIPAddr(), vEthernetGetMACAddr(), and vEthernetGetSubnetMask().
Referenced by e_syscmds_cmd_get_config().
eExecStatus e_ethernet_cmd_set_config | ( | eModId | xModId, |
signed short | FsNavId, | ||
int | ac, | ||
signed portCHAR * | av[], | ||
signed portCHAR ** | ppcStringReply | ||
) |
The get sensor config command: get the config fields value of a sensor. Takes one parameter, that is the sensor's name. Format: get_sensor_config sensorname.
xModId | Input. The module that is calling this function. |
FsNavId | Ignored. |
ac | Input. The argument counter. For this command, should be 1. |
av | Input. The argument vector. |
ppcStringReply | Input/Output. The response string. If Input is NULL, no response string will be output. Else a malloc for the response string is performed here; the caller must free this string. |
References config_file_set_value(), ETHERNET_CONFIG_FILE, NULL, pvPortMalloc(), SHELL_ERRMSG_CONFIGERROR, SHELL_EXECSTATUS_KO, SHELL_EXECSTATUS_OK, and SHELL_MSG_REBOOT.
Referenced by e_syscmds_cmd_set_config().
eExecStatus e_ip_stat | ( | eModId | xModId, |
signed short | FsNavId, | ||
int | ac, | ||
signed portCHAR * | av[], | ||
signed portCHAR ** | ppcStringReply | ||
) |
The development only ip statck stats: display the TCP/IP stack stats on COM2. No parameters. Format: ipstat.
xModId | Input. The module that is calling this function. |
FsNavId | Ignored. |
ac | Input. The argument counter. Ignored. |
av | Input. The argument vector. Ignored |
ppcStringReply | Input/Output. The response string. If Input is NULL, no response string will be output. Else a malloc for the response string is performed here; the caller must free this string. |
References NULL, SHELL_EXECSTATUS_OK, and stats_display.
portTASK_FUNCTION | ( | vStartEthernetTask | , |
pvParameters | |||
) |
configure lwIP and MACB, start lwIP layer, start servers tasks through lwIP services.
configure lwIP and MACB, start lwIP layer, start servers tasks through lwIP services.
uxPriority | Input. priority for the task, it should be low |
configure lwIP and MACB, start lwIP layer, start servers tasks through lwIP services.
pvParameters | Input; not used. |
uxPriority | Input. priority for the task, it should be low |
References CTRLPANEL_SMTP_CLIENT_PRIORITY, CTRLPANEL_SMTP_CLIENT_STACK_SIZE, CTRLPANEL_TFTP_SERVER_PRIORITY, CTRLPANEL_TFTP_SERVER_STACK_SIZE, CTRLPANEL_WEB_SERVER_PRIORITY, CTRLPANEL_WEB_SERVER_STACK_SIZE, gpio_enable_module(), lwipBASIC_SMTP_CLIENT_PRIORITY, lwipBASIC_SMTP_CLIENT_STACK_SIZE, lwipBASIC_TFTP_SERVER_PRIORITY, lwipBASIC_TFTP_SERVER_STACK_SIZE, lwipBASIC_WEB_SERVER_PRIORITY, lwipBASIC_WEB_SERVER_STACK_SIZE, NULL, prvlwIPInit(), sys_thread_new(), and vTaskDelete().
void v_ethernet_stopResources | ( | void | ) |
Stop the Ethernet module resources.
References vDisableMACBOperations().
Referenced by e_syscmds_reboot().
void vEthernetGetGWAddr | ( | portCHAR * | pcConfig | ) |
get the current GW address : formatted as follow : XXX.XXX.XXX.XXX
pcConfig | Input/Output. The response string. If Input is NULL, no response string will be output. The caller has to allocate this buffer |
References netif::gw, MACB_if, ntohl, NULL, and sprintf().
Referenced by e_ethernet_cmd_get_config().
void vEthernetGetIPAddr | ( | portCHAR * | pcConfig | ) |
get the current IP address : formatted as follow : XXX.XXX.XXX.XXX
pcConfig | Input/Output. The response string. If Input is NULL, no response string will be output. The caller has to allocate this buffer |
References netif::ip_addr, MACB_if, ntohl, NULL, and sprintf().
Referenced by e_ethernet_cmd_get_config(), and prvEthernetConfigureInterface().
void vEthernetGetMACAddr | ( | portCHAR * | pcConfig | ) |
get the current MAC address : formatted as follow : XX:XX:XX:XX:XX:XX
pcConfig | Input/Output. The response string. If Input is NULL, no response string will be output. The caller has to allocate this buffer |
References netif::hwaddr, MACB_if, NULL, and sprintf().
Referenced by e_ethernet_cmd_get_config().
void vEthernetGetSubnetMask | ( | portCHAR * | pcConfig | ) |
get the current Subnet mask : formatted as follow : XXX.XXX.XXX.XXX
pcConfig | Input/Output. The response string. If Input is NULL, no response string will be output. The caller has to allocate this buffer |
References MACB_if, netif::netmask, ntohl, NULL, and sprintf().
Referenced by e_ethernet_cmd_get_config().
void vStartEthernetTaskLauncher | ( | unsigned portBASE_TYPE | uxPriority | ) |
Create the vStartEthernetTask task.
uxPriority | Input; priority of the task to create. |
References configMINIMAL_STACK_SIZE, NULL, and xTaskCreate.
Referenced by main(), and portTASK_FUNCTION().