Microchip® Advanced Software Framework

 All Data Structures Namespaces Files Functions Variables Typedefs Enumerations Enumerator Friends Macros Groups Pages
TOUCH - Resistive Touch

This driver offers resistive touch measurements by using the on-chip ADC.

In addition it offers calibration and a callback function for the application.

To improve the overall results four ADC channels are used to measure the touch position. That means the measurements are done from each direction of the touch surface.

Modules

 

Data Structures

struct  rtouch_calibration_matrix_struct
 Calibration matrix coefficients, computed from three calibration points. More...
 
struct  rtouch_calibration_point_struct
 Info for one calibration point, raw samples and actual panel position. More...
 
struct  rtouch_calibration_points_struct
 Collection of the three calibration points required to compute calibration. More...
 
struct  rtouch_event_struct
 User-friendly touch event structure. More...
 

Typedefs

typedef struct
rtouch_calibration_matrix_struct 
rtouch_calibration_matrix_t
 Calibration matrix coefficients, computed from three calibration points. More...
 
typedef struct
rtouch_calibration_point_struct 
rtouch_calibration_point_t
 Info for one calibration point, raw samples and actual panel position. More...
 
typedef struct
rtouch_calibration_points_struct 
rtouch_calibration_points_t
 Collection of the three calibration points required to compute calibration. More...
 
typedef void(* rtouch_event_handler_t )(rtouch_event_t const *event)
 Type definition for a user touch event callback function. More...
 
typedef struct rtouch_event_struct rtouch_event_t
 User-friendly touch event structure. More...
 
typedef enum rtouch_event_type_enum rtouch_event_type_t
 Event type used by event struct rtouch_event_t. More...
 

Enumerations

enum  rtouch_event_type_enum {
  RTOUCH_NO_EVENT,
  RTOUCH_PRESS,
  RTOUCH_MOVE,
  RTOUCH_RELEASE
}
 Event type used by event struct rtouch_event_t. More...
 

Functions

void rtouch_compute_calibration_matrix (rtouch_calibration_points_t const *points, rtouch_calibration_matrix_t *matrix)
 Compute a raw coordinate to screen coordinate calibration matrix. More...
 
void rtouch_disable (void)
 Disables the resistive touch screen driver. More...
 
void rtouch_enable (void)
 Enables touch detection of the driver once initialized. More...
 
void rtouch_get_calibration_matrix (rtouch_calibration_matrix_t *destination)
 Gets the currently set touch driver calibration matrix. More...
 
void rtouch_get_event (rtouch_event_t *event)
 Retrieve the last touch event. More...
 
rtouch_event_handler_t rtouch_get_event_handler (void)
 Gets the currently set touch screen event handler callback function. More...
 
void rtouch_init (void)
 
bool rtouch_is_touched (void)
 Determine if the screen is currently being touched. More...
 
void rtouch_set_calibration_matrix (rtouch_calibration_matrix_t const *source)
 Set the touch driver calibration matrix. More...
 
void rtouch_set_event_handler (rtouch_event_handler_t handler)
 Set the touch screen event handler callback function. More...
 

Calibration matrix coefficients, computed from three calibration points.

Info for one calibration point, raw samples and actual panel position.

Collection of the three calibration points required to compute calibration.

typedef void(* rtouch_event_handler_t)(rtouch_event_t const *event)

Type definition for a user touch event callback function.

User-friendly touch event structure.

Event type used by event struct rtouch_event_t.

Event type used by event struct rtouch_event_t.

Enumerator
RTOUCH_NO_EVENT 
RTOUCH_PRESS 
RTOUCH_MOVE 
RTOUCH_RELEASE 

void rtouch_compute_calibration_matrix ( rtouch_calibration_points_t const *  points,
rtouch_calibration_matrix_t matrix 
)

Compute a raw coordinate to screen coordinate calibration matrix.

This function computes a calibration matrix from a set of three calibration points provided by the caller. Use the raw sample values from the event struct when filling data into the calibration point struct. The calibration matrix will be copied into the struct also provided by the user. Use the rtouch_SetCalibrationMatrix() function to assign a calibration matrix to the driver.

Parameters
pointsPointer to a calibration point set.
matrixPointer to the struct where the matrix will be copied.

References rtouch_calibration_matrix_struct::A, rtouch_calibration_matrix_struct::B, rtouch_calibration_matrix_struct::C, rtouch_calibration_matrix_struct::D, rtouch_calibration_matrix_struct::E, rtouch_calibration_matrix_struct::F, rtouch_calibration_matrix_struct::K, rtouch_calibration_point_struct::panelX, rtouch_calibration_point_struct::panelY, rtouch_calibration_points_struct::point1, rtouch_calibration_points_struct::point2, rtouch_calibration_points_struct::point3, rtouch_calibration_point_struct::rawX, and rtouch_calibration_point_struct::rawY.

Referenced by rtouch_calibrate().

void rtouch_disable ( void  )

Disables the resistive touch screen driver.

This function disables the driver, stopping all touch detection and sampling. This will save power.

References rtouch, rtouch_disable_adc_int(), rtouch_disable_detect_int(), RTOUCH_DISABLED, rtouch_ground_x_surface(), and rtouch_ground_y_surface().

Referenced by rtouch_init().

void rtouch_enable ( void  )

Enables touch detection of the driver once initialized.

This function enables the driver, resuming touch detecting and sampling.

References rtouch, rtouch_clear_adc_flag(), rtouch_clear_detect_flag(), RTOUCH_DISABLED, rtouch_enable_adc_int(), rtouch_enable_detect_int(), rtouch_ground_x_surface(), RTOUCH_NO_EVENT, RTOUCH_NOT_TOUCHED, and rtouch_pullup_y_surface().

Referenced by main().

void rtouch_get_calibration_matrix ( rtouch_calibration_matrix_t destination)

Gets the currently set touch driver calibration matrix.

This function retrieves the current calibration matrix from the driver. Use this function to store a calibration matrix to e.g. EEPROM.

Parameters
destinationPointer to struct where matrix will be copied.

References rtouch.

void rtouch_get_event ( rtouch_event_t event)

Retrieve the last touch event.

This function will copy the last event information to a struct. The caller is responsible for providing memory.

Parameters
eventPointer to the struct where event will be copied.

References rtouch.

Referenced by rtouch_calibrate().

rtouch_event_handler_t rtouch_get_event_handler ( void  )

Gets the currently set touch screen event handler callback function.

This function returns the old event handler. Use this to store the old handler while replacing it for a short while, e.g. for calibration.

Returns
Current event handler pointer.

References rtouch.

Referenced by rtouch_calibrate().

bool rtouch_is_touched ( void  )

Determine if the screen is currently being touched.

This function returns true if the touch panel is currently touched.

Returns
true if panel touched.

References rtouch, RTOUCH_MOVE, and RTOUCH_PRESS.

Referenced by rtouch_calibrate().

void rtouch_set_calibration_matrix ( rtouch_calibration_matrix_t const *  source)

Set the touch driver calibration matrix.

This function assigns a calibration matrix to the driver. The calibration matrix must be retained in RAM while the driver is used.

Parameters
sourcePointer to matrix data.

References rtouch.

Referenced by rtouch_calibrate().

void rtouch_set_event_handler ( rtouch_event_handler_t  handler)

Set the touch screen event handler callback function.

This function sets a new touch event handler. The handler is called whenever the position or state of the touch screen changes.

Parameters
handlerPointer to new event handler, or NULL to disable handler.

References rtouch.

Referenced by main(), and rtouch_calibrate().