See Quick start guide for the maXTouch component.
This component provides low-level read/write access to the configuration and data registers on a maXTouch device. It has only been tested on mxt143E parts, but it should be easy to add support for other maXTouch devices. This is a common API for all supported architectures in ASF.
The component is not interrupt driven and the maXTouch device has to be polled to see if there are any pending messages, and the mxt_read_message function reads out the messages pending. For reading out only touch events, the mxt_read_touch_event function can be used. As mentioned the component is not interrupt driven, but by configuring a pin change interrupt on the CHG pin, the application can receive interrupts when there are messages pending.
|
status_code_t | mxt_close_device (struct mxt_device *device) |
| Closes the twi connection and frees memory. More...
|
|
int8_t | mxt_get_message_count (struct mxt_device *device) |
| Get pending message count. More...
|
|
uint16_t | mxt_get_object_address (struct mxt_device *device, uint8_t object_id, uint8_t instance) |
| Get memory address to object. More...
|
|
enum mxt_object_type | mxt_get_object_type (struct mxt_device *device, struct mxt_conf_messageprocessor_t5 *message) |
| Get object type from message. More...
|
|
status_code_t | mxt_init_device (struct mxt_device *device, twi_master_t interface, uint8_t chip_adr, uint32_t chgpin) |
| Initialize maXTouch device connected to TWIx module. More...
|
|
bool | mxt_is_message_pending (struct mxt_device *device) |
| Report if there is any pending messages in the queue. More...
|
|
status_code_t | mxt_load_configuration (struct mxt_device *device, void *configuration_data) |
|
status_code_t | mxt_probe_device (twi_master_t interface, uint8_t chip_adr) |
| Probe for a maXTouch connected to a specific TWI line. More...
|
|
status_code_t | mxt_process_messages (struct mxt_device *device) |
| Process message queue on maXTouch device. More...
|
|
status_code_t | mxt_read_config_object (struct mxt_device *device, mxt_memory_adr memory_adr, void *obj_data) |
| Read object configuration. More...
|
|
status_code_t | mxt_read_config_reg (struct mxt_device *device, mxt_memory_adr memory_adr, uint8_t *value) |
| Read object register. More...
|
|
status_code_t | mxt_read_message (struct mxt_device *device, struct mxt_conf_messageprocessor_t5 *message) |
| Get next message in queue. More...
|
|
status_code_t | mxt_read_touch_event (struct mxt_device *device, struct mxt_touch_event *touch_event) |
| Read next touch event in queue, skip other events (other events are lost) More...
|
|
void | mxt_set_message_handler (struct mxt_device *device, mxt_message_handler_t handler) |
| Set message handler. More...
|
|
status_code_t | mxt_write_config_object (struct mxt_device *device, mxt_memory_adr memory_adr, void *obj_data) |
| Write object configuration. More...
|
|
status_code_t | mxt_write_config_reg (struct mxt_device *device, mxt_memory_adr memory_adr, uint8_t value) |
| Write object register. More...
|
|
#define MXT_COMMSCONFIG_T18_CHG_MODE_bp 2 |
#define MXT_COMMSCONFIG_T18_DISMNTR_bp 7 |
#define MXT_DETECT_EVENT 128 |
#define MXT_GEN_COMMANDPROCESSOR_BACKUPNV 1 |
#define MXT_GEN_COMMANDPROCESSOR_CALIBRATE 2 |
#define MXT_GEN_COMMANDPROCESSOR_DIAGNOSTIC 5 |
#define MXT_GEN_COMMANDPROCESSOR_REPORTALL 3 |
#define MXT_GEN_COMMANDPROCESSOR_RESET 0 |
#define MXT_MOVE_EVENT 16 |
#define MXT_PRESS_EVENT 64 |
#define MXT_RELEASE_EVENT 32 |
#define MXT_SUPPRESS_EVENT 2 |
#define MXT_UNGRIP_EVENT 1 |
#define MXT_VECTOR_EVENT 8 |
Message handler prototype.
- Parameters
-
*device | Pointer to mxt_device struct |
*message | Pointer to mxt_message struct |
Object types.
Enumerator |
---|
MXT_GEN_MESSAGEPROCESSOR_T5 |
|
MXT_GEN_COMMANDPROCESSOR_T6 |
|
MXT_GEN_POWERCONFIG_T7 |
|
MXT_GEN_ACQUISITIONCONFIG_T8 |
|
MXT_TOUCH_MULTITOUCHSCREEN_T9 |
|
MXT_SPT_COMMSCONFIG_T18 |
|
MXT_SPT_MESSAGECOUNT_T44 |
|
MXT_PROCG_TOUCHSUPPRESSION_T48 |
|
int8_t mxt_get_message_count |
( |
struct mxt_device * |
device | ) |
|
uint16_t mxt_get_object_address |
( |
struct mxt_device * |
device, |
|
|
uint8_t |
object_id, |
|
|
uint8_t |
instance |
|
) |
| |
Initialize maXTouch device connected to TWIx module.
- Parameters
-
*interface | Pointer to TWI register set |
*device | Pointer to mxt_device instance |
chip_adr | I2C address to maXTouch device |
chgpin | IOPORT pin instance attached to the maXTouch device's /CHG pin |
- Returns
- Operation result status code
References mxt_device::chgpin, ERR_BAD_DATA, mxt_device::handler, mxt_device::interface, mxt_device::multitouch_report_offset, mxt_device::mxt_chip_adr, mxt_create_report_id_map(), mxt_get_report_id_offset(), mxt_info_le_to_cpu(), mxt_read_info_block(), MXT_TOUCH_MULTITOUCHSCREEN_T9, mxt_validate_info_block(), NULL, status, and STATUS_OK.
Probe for a maXTouch connected to a specific TWI line.
- Parameters
-
interface | Pointer to TWI register set |
*chip_adr | I2C address to maXTouch device |
- Returns
- Operation result status code
References buffer, ERR_BAD_ADDRESS, mxt_info_object::family_ID, length, MXT_FAMILY_143E, MXT_MEM_ADDR, MXT_VARIANT_143E, status, STATUS_OK, twi_master_read(), twi_package_t, TWI_SUCCESS, and mxt_info_object::variant_ID.
Get next message in queue.
- Parameters
-
*device | Pointer to mxt_device instance |
*message | Pointer to mxt_message instance |
- Returns
- Operation result status code
References ERR_IO_ERROR, mxt_device::interface, mxt_device::mxt_chip_adr, MXT_GEN_MESSAGEPROCESSOR_T5, mxt_get_object_address(), MXT_TWI_MSG_SIZE_T5, mxt_validate_message(), STATUS_OK, twi_master_read(), and twi_package_t.
Referenced by mxt_process_messages(), and mxt_read_touch_event().
Read next touch event in queue, skip other events (other events are lost)
- Parameters
-
- Returns
- Operation result status code
References ERR_BAD_DATA, mxt_touch_event::id, mxt_conf_messageprocessor_t5::message, mxt_device::multitouch_report_offset, mxt_get_object_type(), mxt_is_message_pending(), mxt_read_message(), MXT_TOUCH_MULTITOUCHSCREEN_T9, mxt_conf_messageprocessor_t5::reportid, mxt_touch_event::size, status, mxt_touch_event::status, STATUS_OK, mxt_touch_event::x, and mxt_touch_event::y.