Microchip® Advanced Software Framework

twim_package_t Struct Reference

Information concerning the data transmission.

#include <twim.h>

Data Fields

uint8_t addr [3]
 TWI address/commands to issue to the other chip (node). More...
 
uint8_t addr_length
 Length of the TWI data address segment (1-3 bytes). More...
 
void * buffer
 Where to find the data to be written. More...
 
uint32_t chip
 TWI chip address to communicate with. More...
 
uint32_t length
 How many bytes do we want to write. More...
 
bool no_wait
 Whether to wait if bus is busy (false) or return immediately (true) More...
 

uint8_t twim_package_t::addr[3]

TWI address/commands to issue to the other chip (node).

Referenced by twim_read_packet(), and twim_write_packet().

uint8_t twim_package_t::addr_length

Length of the TWI data address segment (1-3 bytes).

Referenced by twim_read_packet(), and twim_write_packet().

void* twim_package_t::buffer

Where to find the data to be written.

Referenced by ISR(), twim_read_packet(), and twim_write_packet().

uint32_t twim_package_t::chip

TWI chip address to communicate with.

Referenced by twim_read_packet(), and twim_write_packet().

uint32_t twim_package_t::length

How many bytes do we want to write.

Referenced by ISR(), twim_read_packet(), and twim_write_packet().

bool twim_package_t::no_wait

Whether to wait if bus is busy (false) or return immediately (true)