#include "trans_dsp16_twiddle_factors.h"
Macros | |
#define | DSP16_Q_CONVERT(x) DSP16_Q((x)/2.) |
This macro is used to convert the raw data according to the algorithm's optimization we need. More... | |
Variables | |
1024 elements twiddle factors table | |
A_ALIGNED TWIDDLE_FACTORS_PREFIX_TAB dsp16_t | dsp16_twiddle_factors [DSP16_N_TWIDDLE_FACTORS/2+2] |
This table has been generated using the following algorithm: More... | |
A_ALIGNED TWIDDLE_FACTORS_PREFIX_TAB dsp16_t | dsp16_twiddle_factors2 [DSP16_N_TWIDDLE_FACTORS] |
This table has been generated using the following algorithm: More... | |
#define DSP16_Q_CONVERT | ( | x | ) | DSP16_Q((x)/2.) |
This macro is used to convert the raw data according to the algorithm's optimization we need.
A_ALIGNED TWIDDLE_FACTORS_PREFIX_TAB dsp16_t dsp16_twiddle_factors[DSP16_N_TWIDDLE_FACTORS/2+2] |
This table has been generated using the following algorithm:
It is a one dimensional array containing the real parts (even parts) and imaginary parts (odd parts) of the w value.
Referenced by dsp16_trans_complexfft(), dsp16_trans_complexifft(), and dsp16_trans_realcomplexfft().
A_ALIGNED TWIDDLE_FACTORS_PREFIX_TAB dsp16_t dsp16_twiddle_factors2[DSP16_N_TWIDDLE_FACTORS] |
This table has been generated using the following algorithm:
It is a one dimensional array containing the real parts (4*i parts) and imaginary parts (4*i+1 parts) of the w2 value and the real parts (4*i+2 parts) and imaginary parts (4*i+3 parts) of the w3 value.
Referenced by dsp16_trans_complexfft(), dsp16_trans_complexifft(), and dsp16_trans_realcomplexfft().