Declaration of main function used by example.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | main_resume_action (void) |
Turn on a led to notify active mode Called when the USB line is resumed from the suspend state. More... | |
bool | main_setup_in_received (void) |
Manage the reception of setup request IN. More... | |
bool | main_setup_out_received (void) |
Manage the reception of setup request OUT. More... | |
void | main_sof_action (void) |
Manages the leds behaviors Called when a start of frame is received on USB line each 1ms. More... | |
void | main_suspend_action (void) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More... | |
void | main_vendor_disable (void) |
Notify via user interface that enumeration is disabled This is called by vendor interface when USB Host disable it. More... | |
bool | main_vendor_enable (void) |
Notify via user interface that enumeration is ok This is called by vendor interface when USB Host enable it. More... | |
void main_resume_action | ( | void | ) |
Turn on a led to notify active mode Called when the USB line is resumed from the suspend state.
Turn on a led to notify active mode Called when the USB line is resumed from the suspend state.
References main_b_suspend_event, and ui_wakeup().
bool main_setup_in_received | ( | void | ) |
Manage the reception of setup request IN.
true | if request accepted |
References main_buf_loopback, min, udd_ctrl_request_t::payload, udd_ctrl_request_t::payload_size, udd_ctrl_request_t::req, udd_g_ctrlreq, ui_loop_back_state(), and usb_setup_req_t::wLength.
bool main_setup_out_received | ( | void | ) |
Manage the reception of setup request OUT.
true | if request accepted |
References main_buf_loopback, min, udd_ctrl_request_t::payload, udd_ctrl_request_t::payload_size, udd_ctrl_request_t::req, udd_g_ctrlreq, ui_loop_back_state(), and usb_setup_req_t::wLength.
void main_sof_action | ( | void | ) |
Manages the leds behaviors Called when a start of frame is received on USB line each 1ms.
Manages the leds behaviors Called when a start of frame is received on USB line each 1ms.
References main_b_cdc_enable, main_b_generic_enable, main_b_mouse_enable, main_b_msc_enable, main_b_sof_event, main_b_vendor_enable, udd_get_frame_number(), and ui_process().
void main_suspend_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state.
Called by UDD when a suspend is received Callback running when USB Host set USB line in suspend state.
References main_b_resume_event, and ui_powerdown().
void main_vendor_disable | ( | void | ) |
Notify via user interface that enumeration is disabled This is called by vendor interface when USB Host disable it.
References main_b_vendor_enable.
bool main_vendor_enable | ( | void | ) |
Notify via user interface that enumeration is ok This is called by vendor interface when USB Host enable it.
true | if vendor startup is successfully done |
References main_b_vendor_enable, main_buf_iso_sel, main_vendor_bulk_in_received(), main_vendor_int_in_received(), main_vendor_iso_out_received(), and UDD_EP_TRANSFER_OK.