Microchip® Advanced Software Framework

 All Data Structures Namespaces Files Functions Variables Typedefs Enumerations Enumerator Friends Macros Groups Pages
USB Device Driver (UDD)

The UDD driver provides a low-level abstraction of the device controller hardware.

Most events coming from the hardware such as interrupts, which may cause the UDD to call into the UDC and UDI.

Modules

 USBC Device Driver
 USBC low-level driver for USB Device mode.
 

Data Structures

struct  udd_ctrl_request_t
 Global variable to give and record information of the setup request management. More...
 

Macros

#define Udd_setup_is_in()   (USB_REQ_DIR_IN == (udd_g_ctrlreq.req.bmRequestType & USB_REQ_DIR_MASK))
 Return true if the setup request udd_g_ctrlreq indicates IN data transfer. More...
 
#define Udd_setup_is_out()   (USB_REQ_DIR_OUT == (udd_g_ctrlreq.req.bmRequestType & USB_REQ_DIR_MASK))
 Return true if the setup request udd_g_ctrlreq indicates OUT data transfer. More...
 
#define Udd_setup_recipient()   (udd_g_ctrlreq.req.bmRequestType & USB_REQ_RECIP_MASK)
 Return the recipient of the SETUP request udd_g_ctrlreq. More...
 
#define Udd_setup_type()   (udd_g_ctrlreq.req.bmRequestType & USB_REQ_TYPE_MASK)
 Return the type of the SETUP request udd_g_ctrlreq. More...
 

Typedefs

typedef void(* udd_callback_halt_cleared_t )(void)
 End of halt callback function type. More...
 
typedef void(* udd_callback_trans_t )(udd_ep_status_t status, iram_size_t nb_transfered, udd_ep_id_t ep)
 End of transfer callback function type. More...
 
typedef uint8_t udd_ep_id_t
 Endpoint identifier. More...
 

Enumerations

enum  udd_ep_status_t {
  UDD_EP_TRANSFER_OK = 0,
  UDD_EP_TRANSFER_ABORT = 1
}
 Endpoint transfer status Returned in parameters of callback register via udd_ep_run routine. More...
 

Functions

void udd_attach (void)
 Attach device to the bus when possible. More...
 
void udd_detach (void)
 Detaches the device from the bus. More...
 
void udd_disable (void)
 Disables the USB Device mode. More...
 
void udd_enable (void)
 Enables the USB Device mode. More...
 
uint16_t udd_get_frame_number (void)
 Returns the current start of frame number. More...
 
uint16_t udd_get_micro_frame_number (void)
 Returns the current micro start of frame number. More...
 
uint8_t udd_getaddress (void)
 Returns the USB address of device. More...
 
bool udd_include_vbus_monitoring (void)
 Authorizes the VBUS event. More...
 
bool udd_is_high_speed (void)
 Test whether the USB Device Controller is running at high speed or not. More...
 
void udd_send_remotewakeup (void)
 The USB driver sends a resume signal called Upstream Resume. More...
 
void udd_set_address (uint8_t address)
 Changes the USB address of device. More...
 
void udd_set_setup_payload (uint8_t *payload, uint16_t payload_size)
 Load setup payload. More...
 

Variables

udd_ctrl_request_t udd_g_ctrlreq
 Global variable to give and record information about setup request management. More...
 

High speed test mode management

The following functions allow the device to jump to a specific test mode required in high speed mode.

void udd_test_mode_j (void)
 
void udd_test_mode_k (void)
 
void udd_test_mode_se0_nak (void)
 
void udd_test_mode_packet (void)
 

UDC callbacks to provide for UDD

The following callbacks are used by UDD.

bool udc_process_setup (void)
 Decodes and manages a setup request. More...
 
void udc_reset (void)
 Reset the UDC. More...
 
void udc_sof_notify (void)
 To signal that a SOF is occurred. More...
 

#define Udd_setup_is_in ( )    (USB_REQ_DIR_IN == (udd_g_ctrlreq.req.bmRequestType & USB_REQ_DIR_MASK))

Return true if the setup request udd_g_ctrlreq indicates IN data transfer.

Referenced by udc_process_setup(), udc_reqstd(), udd_ctrl_setup_received(), udi_cdc_comm_setup(), udi_dfu_atmel_setup(), udi_hid_setup(), udi_msc_setup(), udi_phdc_setup(), and udi_vendor_setup().

#define Udd_setup_is_out ( )    (USB_REQ_DIR_OUT == (udd_g_ctrlreq.req.bmRequestType & USB_REQ_DIR_MASK))

Return true if the setup request udd_g_ctrlreq indicates OUT data transfer.

Referenced by udi_cdc_comm_setup(), udi_dfu_atmel_setup(), udi_hid_setup(), udi_msc_setup(), udi_phdc_setup(), and udi_vendor_setup().

#define Udd_setup_recipient ( )    (udd_g_ctrlreq.req.bmRequestType & USB_REQ_RECIP_MASK)

Return the recipient of the SETUP request udd_g_ctrlreq.

See Also
usb_recipient

Referenced by udc_process_setup(), and udc_reqstd().

#define Udd_setup_type ( )    (udd_g_ctrlreq.req.bmRequestType & USB_REQ_TYPE_MASK)

Return the type of the SETUP request udd_g_ctrlreq.

See Also
usb_reqtype.

Referenced by udc_process_setup(), udi_cdc_comm_setup(), udi_dfu_atmel_setup(), udi_hid_setup(), udi_msc_setup(), udi_phdc_setup(), and udi_vendor_setup().

typedef void(* udd_callback_halt_cleared_t)(void)

End of halt callback function type.

Registered by routine udd_ep_wait_stall_clear() Callback called when endpoint stall is cleared.

typedef void(* udd_callback_trans_t)(udd_ep_status_t status, iram_size_t nb_transfered, udd_ep_id_t ep)

End of transfer callback function type.

Registered by routine udd_ep_run() Callback called by USB interrupt after data transfer or abort (reset,...).

Parameters
statusUDD_EP_TRANSFER_OK, if transfer is complete
statusUDD_EP_TRANSFER_ABORT, if transfer is aborted
nnumber of data transfered
typedef uint8_t udd_ep_id_t

Endpoint identifier.

Endpoint transfer status Returned in parameters of callback register via udd_ep_run routine.

Enumerator
UDD_EP_TRANSFER_OK 
UDD_EP_TRANSFER_ABORT 

bool udc_process_setup ( void  )

Decodes and manages a setup request.

The driver call it when a SETUP packet is received. The udd_g_ctrlreq contains the data of SETUP packet. If this callback accepts the setup request then it must return 1 and eventually update udd_g_ctrlreq to send or receive data.

Returns
1 if the request is accepted, otherwise 0.

Decodes and manages a setup request.

This function parses a USB SETUP request and submits an appropriate response back to the host or, in the case of SETUP OUT requests with data, sets up a buffer for receiving the data payload.

The main standard requests defined by the USB 2.0 standard are handled internally. The interface requests are sent to UDI, and the specific request sent to a specific application callback.

Returns
true if the request is supported, else the request is stalled by UDD

References udd_ctrl_request_t::callback, NULL, udd_ctrl_request_t::over_under_run, udd_ctrl_request_t::payload_size, udd_ctrl_request_t::req, udc_req_ep(), udc_req_iface(), udc_reqstd(), udd_g_ctrlreq, Udd_setup_is_in, Udd_setup_recipient, Udd_setup_type, USB_REQ_RECIP_ENDPOINT, USB_REQ_RECIP_INTERFACE, USB_REQ_TYPE_STANDARD, and usb_setup_req_t::wLength.

Referenced by udd_ctrl_setup_received().

void udc_sof_notify ( void  )

To signal that a SOF is occurred.

The UDC must send the signal to all UDIs enabled

References usb_conf_desc_t::bNumInterfaces, udc_config_speed_t::desc, NULL, udi_api_t::sof_notify, udc_num_configuration, udc_ptr_conf, and udc_config_speed_t::udi_apis.

void udd_attach ( void  )

Attach device to the bus when possible.

Warning
If a VBus control is included in driver, then it will attach device when an acceptable Vbus level from the host is detected.

References cpu_irq_restore(), cpu_irq_save(), Is_otg_clock_usable, otg_freeze_clock, otg_unfreeze_clock, udd_ack_reset, udd_ack_sof, udd_ack_wake_up, udd_attach_device, udd_enable_reset_interrupt, udd_enable_sof_interrupt, udd_enable_suspend_interrupt, udd_enable_wake_up_interrupt, udd_raise_suspend, and udd_sleep_mode().

Referenced by udc_attach(), and udd_enable().

void udd_detach ( void  )

Detaches the device from the bus.

The driver must remove pull-up on USB line D- or D+.

References otg_freeze_clock, otg_unfreeze_clock, udd_detach_device, and udd_sleep_mode().

Referenced by udc_detach(), and udd_disable().

uint16_t udd_get_frame_number ( void  )

Returns the current start of frame number.

Returns
current start of frame number.

References udd_frame_number.

Referenced by main_sof_action(), and udi_cdc_tx_send().

uint16_t udd_get_micro_frame_number ( void  )

Returns the current micro start of frame number.

Returns
current micro start of frame number required in high speed mode.

References udd_micro_frame_number.

Referenced by udi_cdc_tx_send().

uint8_t udd_getaddress ( void  )

Returns the USB address of device.

Returns
USB address

References udd_get_configured_address.

Referenced by udc_req_std_dev_set_configuration().

bool udd_include_vbus_monitoring ( void  )

Authorizes the VBUS event.

Returns
true, if the VBUS monitoring is possible.

Referenced by udc_include_vbus_monitoring().

bool udd_is_high_speed ( void  )

Test whether the USB Device Controller is running at high speed or not.

Returns
true if the Device is running at high speed mode, otherwise false.

References Is_udd_full_speed_mode.

Referenced by main_vendor_iso_out_received(), udc_req_std_dev_get_descriptor(), udc_req_std_dev_set_configuration(), udc_req_std_dev_set_feature(), and udi_cdc_tx_send().

void udd_send_remotewakeup ( void  )

The USB driver sends a resume signal called Upstream Resume.

References otg_unfreeze_clock, udd_b_idle, udd_initiate_remote_wake_up, and udd_sleep_mode().

Referenced by udc_remotewakeup().

void udd_set_address ( uint8_t  address)

Changes the USB address of device.

Parameters
addressNew USB address

References udd_configure_address, udd_disable_address, and udd_enable_address.

Referenced by udc_valid_address().

void udd_test_mode_j ( void  )
void udd_test_mode_k ( void  )
void udd_test_mode_packet ( void  )
void udd_test_mode_se0_nak ( void  )