Copyright (C) 2006-2010, Brainspark B.V.
This file is part of PolarSSL (http://www.polarssl.org) Lead Maintainer: Paul Bakker <polarssl_maintainer at polarssl.org>
All rights reserved.
This program is free software; you can redistribute it and/or modify it under the terms of the GNU General Public License as published by the Free Software Foundation; either version 2 of the License, or (at your option) any later version.
This program is distributed in the hope that it will be useful, but WITHOUT ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License for more details.
You should have received a copy of the GNU General Public License along with this program; if not, write to the Free Software Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA.
#include "polarssl/rsa.h"
Data Structures | |
struct | _x509_buf |
struct | _x509_cert |
struct | _x509_crl |
struct | _x509_crl_entry |
struct | _x509_name |
struct | _x509_node |
struct | _x509_raw |
struct | _x509_time |
Typedefs | |
typedef struct _x509_buf | x509_buf |
typedef struct _x509_cert | x509_cert |
typedef struct _x509_crl | x509_crl |
typedef struct _x509_crl_entry | x509_crl_entry |
typedef struct _x509_name | x509_name |
typedef struct _x509_node | x509_node |
typedef struct _x509_raw | x509_raw |
typedef struct _x509_time | x509_time |
Functions | |
void | x509_crl_free (x509_crl *crl) |
Unallocate all CRL data. More... | |
void | x509_free (x509_cert *crt) |
Unallocate all certificate data. More... | |
int | x509_self_test (int verbose) |
Checkup routine. More... | |
int | x509parse_cert_info (char *buf, size_t size, const char *prefix, const x509_cert *crt) |
Returns an informational string about the certificate. More... | |
int | x509parse_crl (x509_crl *chain, const unsigned char *buf, int buflen) |
Parse one or more CRLs and add them to the chained list. More... | |
int | x509parse_crl_info (char *buf, size_t size, const char *prefix, const x509_crl *crl) |
Returns an informational string about the CRL. More... | |
int | x509parse_crlfile (x509_crl *chain, const char *path) |
Load one or more CRLs and add them to the chained list. More... | |
int | x509parse_crt (x509_cert *chain, const unsigned char *buf, int buflen) |
Parse one or more certificates and add them to the chained list. More... | |
int | x509parse_crtfile (x509_cert *chain, const char *path) |
Load one or more certificates and add them to the chained list. More... | |
int | x509parse_dn_gets (char *buf, size_t size, const x509_name *dn) |
Store the certificate DN in printable form into buf; no more than size characters will be written. More... | |
int | x509parse_key (rsa_context *rsa, const unsigned char *key, int keylen, const unsigned char *pwd, int pwdlen) |
Parse a private RSA key. More... | |
int | x509parse_keyfile (rsa_context *rsa, const char *path, const char *password) |
Load and parse a private RSA key. More... | |
int | x509parse_time_expired (const x509_time *time) |
Check a given x509_time against the system time and check if it is valid. More... | |
int | x509parse_verify (x509_cert *crt, x509_cert *trust_ca, x509_crl *ca_crl, const char *cn, int *flags) |
Verify the certificate signature. More... | |
#define ASN1_BIT_STRING 0x03 |
#define ASN1_BMP_STRING 0x1E |
#define ASN1_BOOLEAN 0x01 |
#define ASN1_CONSTRUCTED 0x20 |
#define ASN1_CONTEXT_SPECIFIC 0x80 |
#define ASN1_GENERALIZED_TIME 0x18 |
#define ASN1_IA5_STRING 0x16 |
#define ASN1_INTEGER 0x02 |
#define ASN1_NULL 0x05 |
#define ASN1_OCTET_STRING 0x04 |
#define ASN1_OID 0x06 |
#define ASN1_PRIMITIVE 0x00 |
#define ASN1_PRINTABLE_STRING 0x13 |
#define ASN1_SEQUENCE 0x10 |
#define ASN1_SET 0x11 |
#define ASN1_T61_STRING 0x14 |
#define ASN1_UNIVERSAL_STRING 0x1C |
#define ASN1_UTC_TIME 0x17 |
#define ASN1_UTF8_STRING 0x0C |
#define BADCERT_CN_MISMATCH 4 |
#define BADCERT_EXPIRED 1 |
#define BADCERT_NOT_TRUSTED 8 |
#define BADCERT_REVOKED 2 |
#define BADCRL_EXPIRED 32 |
#define BADCRL_NOT_TRUSTED 16 |
#define OID_CN "\x55\x04\x03" |
#define OID_PKCS1 "\x2A\x86\x48\x86\xF7\x0D\x01\x01" |
#define OID_PKCS1_RSA "\x2A\x86\x48\x86\xF7\x0D\x01\x01\x01" |
#define OID_PKCS1_RSA_SHA "\x2A\x86\x48\x86\xF7\x0D\x01\x01\x05" |
#define OID_PKCS9 "\x2A\x86\x48\x86\xF7\x0D\x01\x09" |
#define OID_PKCS9_EMAIL "\x2A\x86\x48\x86\xF7\x0D\x01\x09\x01" |
#define OID_X520 "\x55\x04" |
#define PEM_LINE_LENGTH 72 |
#define PKCS9_EMAIL 1 |
#define POLARSSL_ERR_ASN1_INVALID_DATA 0x001C |
#define POLARSSL_ERR_ASN1_INVALID_LENGTH 0x0018 |
#define POLARSSL_ERR_ASN1_LENGTH_MISMATCH 0x001A |
#define POLARSSL_ERR_ASN1_OUT_OF_DATA 0x0014 |
#define POLARSSL_ERR_ASN1_UNEXPECTED_TAG 0x0016 |
#define POLARSSL_ERR_X509_CERT_INVALID_ALG -0x00C0 |
#define POLARSSL_ERR_X509_CERT_INVALID_DATE -0x0100 |
#define POLARSSL_ERR_X509_CERT_INVALID_EXTENSIONS -0x0160 |
#define POLARSSL_ERR_X509_CERT_INVALID_FORMAT -0x0060 |
#define POLARSSL_ERR_X509_CERT_INVALID_NAME -0x00E0 |
#define POLARSSL_ERR_X509_CERT_INVALID_PEM -0x0040 |
#define POLARSSL_ERR_X509_CERT_INVALID_PUBKEY -0x0120 |
#define POLARSSL_ERR_X509_CERT_INVALID_SERIAL -0x00A0 |
#define POLARSSL_ERR_X509_CERT_INVALID_SIGNATURE -0x0140 |
#define POLARSSL_ERR_X509_CERT_INVALID_VERSION -0x0080 |
#define POLARSSL_ERR_X509_CERT_SIG_MISMATCH -0x01E0 |
#define POLARSSL_ERR_X509_CERT_UNKNOWN_PK_ALG -0x01C0 |
#define POLARSSL_ERR_X509_CERT_UNKNOWN_SIG_ALG -0x01A0 |
#define POLARSSL_ERR_X509_CERT_UNKNOWN_VERSION -0x0180 |
#define POLARSSL_ERR_X509_CERT_VERIFY_FAILED -0x0200 |
#define POLARSSL_ERR_X509_FEATURE_UNAVAILABLE -0x0020 |
#define POLARSSL_ERR_X509_KEY_INVALID_ENC_IV -0x0280 |
#define POLARSSL_ERR_X509_KEY_INVALID_FORMAT -0x0260 |
#define POLARSSL_ERR_X509_KEY_INVALID_PEM -0x0220 |
#define POLARSSL_ERR_X509_KEY_INVALID_VERSION -0x0240 |
#define POLARSSL_ERR_X509_KEY_PASSWORD_MISMATCH -0x02E0 |
#define POLARSSL_ERR_X509_KEY_PASSWORD_REQUIRED -0x02C0 |
#define POLARSSL_ERR_X509_KEY_UNKNOWN_ENC_ALG -0x02A0 |
#define POLARSSL_ERR_X509_POINT_ERROR -0x0300 |
#define POLARSSL_ERR_X509_VALUE_TO_LENGTH -0x0320 |
#define X509_ISSUER 0x01 |
#define X509_OUTPUT_DER 0x01 |
#define X509_OUTPUT_PEM 0x02 |
#define X509_SUBJECT 0x02 |
#define X520_COMMON_NAME 3 |
#define X520_COUNTRY 6 |
#define X520_LOCALITY 7 |
#define X520_ORG_UNIT 11 |
#define X520_ORGANIZATION 10 |
#define X520_STATE 8 |
typedef struct _x509_cert x509_cert |
typedef struct _x509_crl_entry x509_crl_entry |
typedef struct _x509_name x509_name |
typedef struct _x509_node x509_node |
typedef struct _x509_time x509_time |
void x509_crl_free | ( | x509_crl * | crl | ) |
Unallocate all CRL data.
crt | CRL chain to free |
void x509_free | ( | x509_cert * | crt | ) |
Unallocate all certificate data.
crt | Certificate chain to free |
int x509_self_test | ( | int | verbose | ) |
Checkup routine.
int x509parse_cert_info | ( | char * | buf, |
size_t | size, | ||
const char * | prefix, | ||
const x509_cert * | crt | ||
) |
Returns an informational string about the certificate.
buf | Buffer to write to |
size | Maximum size of buffer |
prefix | A line prefix |
crt | The X509 certificate to represent |
int x509parse_crl | ( | x509_crl * | chain, |
const unsigned char * | buf, | ||
int | buflen | ||
) |
Parse one or more CRLs and add them to the chained list.
chain | points to the start of the chain |
buf | buffer holding the CRL data |
buflen | size of the buffer |
int x509parse_crl_info | ( | char * | buf, |
size_t | size, | ||
const char * | prefix, | ||
const x509_crl * | crl | ||
) |
Returns an informational string about the CRL.
buf | Buffer to write to |
size | Maximum size of buffer |
prefix | A line prefix |
crt | The X509 CRL to represent |
int x509parse_crlfile | ( | x509_crl * | chain, |
const char * | path | ||
) |
Load one or more CRLs and add them to the chained list.
chain | points to the start of the chain |
path | filename to read the CRLs from |
int x509parse_crt | ( | x509_cert * | chain, |
const unsigned char * | buf, | ||
int | buflen | ||
) |
Parse one or more certificates and add them to the chained list.
chain | points to the start of the chain |
buf | buffer holding the certificate data |
buflen | size of the buffer |
int x509parse_crtfile | ( | x509_cert * | chain, |
const char * | path | ||
) |
Load one or more certificates and add them to the chained list.
chain | points to the start of the chain |
path | filename to read the certificates from |
int x509parse_dn_gets | ( | char * | buf, |
size_t | size, | ||
const x509_name * | dn | ||
) |
Store the certificate DN in printable form into buf; no more than size characters will be written.
buf | Buffer to write to |
size | Maximum size of buffer |
dn | The X509 name to represent |
int x509parse_key | ( | rsa_context * | rsa, |
const unsigned char * | key, | ||
int | keylen, | ||
const unsigned char * | pwd, | ||
int | pwdlen | ||
) |
Parse a private RSA key.
rsa | RSA context to be initialized |
key | input buffer |
keylen | size of the buffer |
pwd | password for decryption (optional) |
pwdlen | size of the password |
int x509parse_keyfile | ( | rsa_context * | rsa, |
const char * | path, | ||
const char * | password | ||
) |
Load and parse a private RSA key.
rsa | RSA context to be initialized |
path | filename to read the private key from |
pwd | password to decrypt the file (can be NULL) |
int x509parse_time_expired | ( | const x509_time * | time | ) |
Check a given x509_time against the system time and check if it is valid.
time | x509_time to check |
int x509parse_verify | ( | x509_cert * | crt, |
x509_cert * | trust_ca, | ||
x509_crl * | ca_crl, | ||
const char * | cn, | ||
int * | flags | ||
) |
Verify the certificate signature.
crt | a certificate to be verified |
trust_ca | the trusted CA chain |
ca_crl | the CRL chain for trusted CA's |
cn | expected Common Name (can be set to NULL if the CN must not be verified) |
flags | result of the verification |