Microchip® Advanced Software Framework

qdebug Directory Reference

Files

file  QDebug_at32uc3l.c
 This file contains the QDebug public API that can be used to transfer data from a Touch Device to QTouch Studio using the QT600 USB Bridge.
 
file  QDebug_at32uc3l.h
 This file contains the QDebug public API that can be used to transfer data from a Touch Device to QTouch Studio using the QT600 USB Bridge.
 
file  QDebugTransport.c
 
file  QDebugTransport.h