Microchip® Advanced Software Framework

 All Data Structures Namespaces Files Functions Variables Typedefs Enumerations Enumerator Friends Macros Groups Pages
Related Project(s)

In this section you can find all the projects related to the Calendar service.

Example(s)

Calendar service example 2 for STK600-RCUC3L4

An example application that calculates the time difference between two dates, and lights up a led if the resulting time is correct.

Calendar service example 2 for UC3-L0 Xplained

An example application that calculates the time difference between two dates, and lights up a led if the resulting time is correct.

Calendar service example for STK600-RCUC3L4

An example application that converts a date to a timestamp and lights up a led if the timestamp is correct.

Calendar service example for UC3-L0 Xplained

An example application that converts a date to a timestamp and lights up a led if the timestamp is correct.

Unit-test(s)

Calendar driver unit tests on STK600-RCUC3L4

Unit tests for calendar functionality

Calendar driver unit tests on UC3-L0 Xplained

Unit tests for calendar functionality