Microchip® Advanced Software Framework

hid/device/mouse/unit_tests/unit_tests.h File Reference

Declaration of main function used by HID mouse unit test.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

Functions

void main_mouse_disable (void)
 Called by HID interface Callback running when USB Host disable mouse interface. More...
 
bool main_mouse_enable (void)
 Called by HID interface Callback running when USB Host enable mouse interface. More...
 
void main_remotewakeup_disable (void)
 Called by UDC when USB Host request to disable remote wakeup. More...
 
void main_remotewakeup_enable (void)
 Called by UDC when USB Host request to enable remote wakeup. More...
 
void main_resume_action (void)
 Called by UDD when the USB line exit of suspend state. More...
 
void main_sof_action (void)
 Called when a start of frame is received on USB line. More...
 
void main_suspend_action (void)
 Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More...
 
void main_vbus_action (bool b_high)
 Called when Vbus line state change. More...
 

void main_mouse_disable ( void  )

Called by HID interface Callback running when USB Host disable mouse interface.

bool main_mouse_enable ( void  )

Called by HID interface Callback running when USB Host enable mouse interface.

Return values
trueif mouse startup is ok
void main_remotewakeup_disable ( void  )

Called by UDC when USB Host request to disable remote wakeup.

void main_remotewakeup_enable ( void  )

Called by UDC when USB Host request to enable remote wakeup.

void main_resume_action ( void  )

Called by UDD when the USB line exit of suspend state.

void main_sof_action ( void  )

Called when a start of frame is received on USB line.

void main_suspend_action ( void  )

Enters the application in low power mode Callback called when USB host sets USB line in suspend state.

void main_vbus_action ( bool  b_high)

Called when Vbus line state change.