Copyright (C) 2006-2010, Brainspark B.V.
This file is part of PolarSSL (http://www.polarssl.org) Lead Maintainer: Paul Bakker <polarssl_maintainer at polarssl.org>
All rights reserved.
This program is free software; you can redistribute it and/or modify it under the terms of the GNU General Public License as published by the Free Software Foundation; either version 2 of the License, or (at your option) any later version.
This program is distributed in the hope that it will be useful, but WITHOUT ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License for more details.
You should have received a copy of the GNU General Public License along with this program; if not, write to the Free Software Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA.
Data Structures | |
struct | sha1_context |
SHA-1 context structure. More... | |
Functions | |
void | sha1 (const unsigned char *input, int ilen, unsigned char output[20]) |
Output = SHA-1( input buffer ) More... | |
int | sha1_file (const char *path, unsigned char output[20]) |
Output = SHA-1( file contents ) More... | |
void | sha1_finish (sha1_context *ctx, unsigned char output[20]) |
SHA-1 final digest. More... | |
void | sha1_hmac (const unsigned char *key, int keylen, const unsigned char *input, int ilen, unsigned char output[20]) |
Output = HMAC-SHA-1( hmac key, input buffer ) More... | |
void | sha1_hmac_finish (sha1_context *ctx, unsigned char output[20]) |
SHA-1 HMAC final digest. More... | |
void | sha1_hmac_reset (sha1_context *ctx) |
SHA-1 HMAC context reset. More... | |
void | sha1_hmac_starts (sha1_context *ctx, const unsigned char *key, int keylen) |
SHA-1 HMAC context setup. More... | |
void | sha1_hmac_update (sha1_context *ctx, const unsigned char *input, int ilen) |
SHA-1 HMAC process buffer. More... | |
int | sha1_self_test (int verbose) |
Checkup routine. More... | |
void | sha1_starts (sha1_context *ctx) |
SHA-1 context setup. More... | |
void | sha1_update (sha1_context *ctx, const unsigned char *input, int ilen) |
SHA-1 process buffer. More... | |
void sha1 | ( | const unsigned char * | input, |
int | ilen, | ||
unsigned char | output[20] | ||
) |
Output = SHA-1( input buffer )
input | buffer holding the data |
ilen | length of the input data |
output | SHA-1 checksum result |
int sha1_file | ( | const char * | path, |
unsigned char | output[20] | ||
) |
Output = SHA-1( file contents )
path | input file name |
output | SHA-1 checksum result |
void sha1_finish | ( | sha1_context * | ctx, |
unsigned char | output[20] | ||
) |
SHA-1 final digest.
ctx | SHA-1 context |
output | SHA-1 checksum result |
void sha1_hmac | ( | const unsigned char * | key, |
int | keylen, | ||
const unsigned char * | input, | ||
int | ilen, | ||
unsigned char | output[20] | ||
) |
Output = HMAC-SHA-1( hmac key, input buffer )
key | HMAC secret key |
keylen | length of the HMAC key |
input | buffer holding the data |
ilen | length of the input data |
output | HMAC-SHA-1 result |
void sha1_hmac_finish | ( | sha1_context * | ctx, |
unsigned char | output[20] | ||
) |
SHA-1 HMAC final digest.
ctx | HMAC context |
output | SHA-1 HMAC checksum result |
void sha1_hmac_reset | ( | sha1_context * | ctx | ) |
SHA-1 HMAC context reset.
ctx | HMAC context to be reset |
void sha1_hmac_starts | ( | sha1_context * | ctx, |
const unsigned char * | key, | ||
int | keylen | ||
) |
SHA-1 HMAC context setup.
ctx | HMAC context to be initialized |
key | HMAC secret key |
keylen | length of the HMAC key |
void sha1_hmac_update | ( | sha1_context * | ctx, |
const unsigned char * | input, | ||
int | ilen | ||
) |
SHA-1 HMAC process buffer.
ctx | HMAC context |
input | buffer holding the data |
ilen | length of the input data |
int sha1_self_test | ( | int | verbose | ) |
Checkup routine.
void sha1_starts | ( | sha1_context * | ctx | ) |
SHA-1 context setup.
ctx | context to be initialized |
void sha1_update | ( | sha1_context * | ctx, |
const unsigned char * | input, | ||
int | ilen | ||
) |
SHA-1 process buffer.
ctx | SHA-1 context |
input | buffer holding the data |
ilen | length of the input data |