Atmel Data Visualizer tool support routines.
This file contains routines for using the Atmel Data Visualizer tool. Various functions and structure definitions provide initialization, data formatting, and actual transmission of application data to a remote host for display.
The Atmel Data Visualizer (ADV) tool is a standalone Windows application that provides a graphical display of data sent from a remote target. It is available as a separate download. For more information on downloading and installing the ADV tool, visit Atmel Data Visualizer
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
#include <stdio.h>
#include <string.h>
#include <stdlib.h>
#include <asf.h>
#include "data_visualizer.h"
Macros | |
#define | PKT_XMIT_DELAY 2 /* delay after sending ADV packet (msec) */ |
Functions | |
void | adv_data_send_1 (uint8_t stream_num, uint32_t timestamp, int32_t value) |
Send data visualizer data packet with 1 data field. More... | |
void | adv_data_send_3 (uint8_t stream_num, uint32_t timestamp, int32_t value0, int32_t value1, int32_t value2) |
Send data visualizer data packet w/ 3 data fields. More... | |
COMPILER_PACK_SET (1) | |
#define PKT_XMIT_DELAY 2 /* delay after sending ADV packet (msec) */ |
Referenced by COMPILER_PACK_SET().
void adv_data_send_1 | ( | uint8_t | stream_num, |
uint32_t | timestamp, | ||
int32_t | value | ||
) |
Send data visualizer data packet with 1 data field.
Send Atmel Data Visualizer data packet with 1 data field.
This routine constructs a data visualizer data packet with one data value field and then transmits it. All multi-byte transmitted values use little endian byte order.
stream_num | The ID number of the visualizer data stream |
timestamp | A 32-bit timestamp value, in microseconds |
value | The data value to include in the transmitted packet |
Referenced by main().
void adv_data_send_3 | ( | uint8_t | stream_num, |
uint32_t | timestamp, | ||
int32_t | value0, | ||
int32_t | value1, | ||
int32_t | value2 | ||
) |
Send data visualizer data packet w/ 3 data fields.
Send Atmel Data Visualizer data packet w/ 3 data fields.
This routine constructs a data visualizer data packet with three data value fields and then transmits it. All multi-byte transmitted values use little endian byte order.
stream_num | The ID number of the visualizer data stream |
timestamp | A 32-bit timestamp value, in microseconds |
value0 | Data field 0 value |
value1 | Data field 1 value |
value2 | Data field 2 value |
Referenced by main().
COMPILER_PACK_SET | ( | 1 | ) |
References delay_ms, and PKT_XMIT_DELAY.