Utilities that convert pressure to altitude.
This is a collection of high-level utility functions that will convert a given pressure to an altitude within the Earth's atmosphere using the International Standard Atmosphere (ISA) model. The ISA is an ideal model of how pressure, temperature, density, and viscosity of the atmosphere change with altitude. The basic pressure_altitude_xxx() routines implement ISA equations in a fairly straightforward fashion without additional constraints. For example, the temperature decrease with altitude (lapse rate) is approximately -6.5 degrees Celsius per 1000 meters for standard atmosphere, but the actual rate varies from day to day and throughout the day.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
#include "physics.h"
Functions | |
scalar | pressure_altitude (scalar P) |
Get an ISA pressure altitude. More... | |
bool | pressure_isa_layer (int index=0) |
Specify a pressure-altitude layer. More... | |
void | pressure_sea_level (scalar P=CONST_STANDARD_ATM) |
Specify the (corrected) pressure-altitude sea level pressure. More... | |
Get an ISA pressure altitude.
Given atmospheric pressure "P" in pascals, this routine returns the associated barometric altitude ("pressure altitude") using International Standard Atmosphere (ISA) pressure model coefficients and equations.
P | The current atmospheric pressure in pascals. |
bool pressure_isa_layer | ( | int | index | ) |
Specify a pressure-altitude layer.
The routine sets the pressure_altitude() function to use a specified "layer" in domain [0, 6]. By default layer 0 is assumed. Calling this routine without arguments will set the pressure_altitude() to calculate barometric altitude assuming a pressure domain within ISA layer zero (P < 22 632 pascals).
index | The atmospheric layer index, zero by default. |
void pressure_sea_level | ( | scalar | P | ) |
Specify the (corrected) pressure-altitude sea level pressure.
This routine will calculate a bias to correct the ISA standard pressure at sea level (1 atm. = 101 325 Pa) for local variations in barometric pressure at mean sea level (MSL).
P | The current local pressure (pascals) at sea level. |
References Pb.