Microchip® Advanced Software Framework

sha204_example_led.h File Reference

LED module for ATSHA204 examples.

This file defines helper functions that use Xplained board LED's to indicate success or failure and byte values (device version for instance).

Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.

Functions

void display_status (uint8_t device_present_mask, uint8_t sha204_revision)
 This function displays information using LEDs about the SHA204 devices on the Security Xplained board. More...
 
void led_display_number (uint8_t value)
 This function displays a byte value using the Xplained LEDs. More...