Atmel Data Visualizer data packet components.
A complete data packet consists of an adv_data_start_t structure, followed by one or more adv_data_field_t structures containing the actual data values, followed by an adv_data_end_t structure.
#include <data_visualizer.h>
Data Fields | |
uint8_t | header1 |
uint8_t | header2 |
uint16_t | length |
uint8_t | stream_num |
uint32_t | time_stamp |
uint8_t | type |
uint8_t adv_data_start_t::header1 |
uint8_t adv_data_start_t::header2 |
uint16_t adv_data_start_t::length |
uint8_t adv_data_start_t::stream_num |
uint32_t adv_data_start_t::time_stamp |
uint8_t adv_data_start_t::type |