This structure contains the parameters for the sha204m_derive_key function.
#include <sha204_command_marshaling.h>
Data Fields | |
uint8_t * | mac |
pointer to MAC for this command More... | |
uint8_t * | rx_buffer |
pointer to receive buffer More... | |
uint8_t | target_key |
slot where derived key should be stored More... | |
uint8_t * | tx_buffer |
pointer to send buffer More... | |
uint8_t | use_random |
true if source for TempKey was random number More... | |
uint8_t* sha204_derive_key_parameters::mac |
pointer to MAC for this command
Referenced by sha204m_derive_key().
uint8_t* sha204_derive_key_parameters::rx_buffer |
pointer to receive buffer
Referenced by sha204m_derive_key().
uint8_t sha204_derive_key_parameters::target_key |
slot where derived key should be stored
Referenced by sha204m_derive_key().
uint8_t* sha204_derive_key_parameters::tx_buffer |
pointer to send buffer
Referenced by sha204m_derive_key().
uint8_t sha204_derive_key_parameters::use_random |
true if source for TempKey was random number
Referenced by sha204m_derive_key().