Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
ADCIFB - ADC Interface B

Driver for the ADCIFB (Analog-to-Digital Converter Interface B).

Provides functions for configuration of conversion parameters (up to 12-bit signed with 16x interpolation at 6 MHz), enabling channels (max. 32, see device datasheet for details) and conversion triggering. Resistive touch screen mode is not supported by this driver.

Data Structures

struct  adcifb_opt_t
 

Macros

#define ADCIFB_POLL_TIMEOUT   10000
 

Functions

static void adcifb_channels_disable (volatile avr32_adcifb_t *adcifb, uint32_t channels_mask)
 Disable one or several channels. More...
 
static void adcifb_channels_enable (volatile avr32_adcifb_t *adcifb, uint32_t channels_mask)
 Enable one or several channels. More...
 
static void adcifb_clear_all_interrupt_flags (volatile avr32_adcifb_t *adcifb)
 Clear all ADCIFB interrupt flags. More...
 
static void adcifb_clear_busy_interrupt_flag (volatile avr32_adcifb_t *adcifb)
 Clear ADCIFB Busy Interrupt flag. More...
 
static void adcifb_clear_compare_else_interrupt_flag (volatile avr32_adcifb_t *adcifb)
 Clear ADCIFB Compare Else interrupt flag. More...
 
static void adcifb_clear_compare_gt_interrupt_flag (volatile avr32_adcifb_t *adcifb)
 Clear ADCIFB Compare Greater than interrupt flag. More...
 
static void adcifb_clear_compare_lt_interrupt_flag (volatile avr32_adcifb_t *adcifb)
 Clear ADCIFB Compare Less than interrupt flag. More...
 
static void adcifb_clear_data_ready_interrupt_flag (volatile avr32_adcifb_t *adcifb)
 Clear ADCIFB Data Ready Interrupt flag. More...
 
static void adcifb_clear_interrupt_flag (volatile avr32_adcifb_t *adcifb, uint32_t interrupt_mask)
 Clear ADCIFB interrupt flags. More...
 
static void adcifb_clear_no_contact_interrupt_flag (volatile avr32_adcifb_t *adcifb)
 Clear ADCIFB No Contact Interrupt flag. More...
 
static void adcifb_clear_overrun_error_interrupt_flag (volatile avr32_adcifb_t *adcifb)
 Clear ADCIFB Overrun Error Interrupt flag. More...
 
static void adcifb_clear_pen_contact_interrupt_flag (volatile avr32_adcifb_t *adcifb)
 Clear ADCIFB Pen Contact Interrupt flag. More...
 
static void adcifb_clear_ready_interrupt_flag (volatile avr32_adcifb_t *adcifb)
 Clear ADCIFB Ready Interrupt flag. More...
 
int32_t adcifb_configure (volatile avr32_adcifb_t *adcifb, const adcifb_opt_t *p_adcifb_opt)
 Initialize the ADCIFB module (enable and configure). More...
 
int32_t adcifb_configure_trigger (volatile avr32_adcifb_t *adcifb, uint8_t trgmod, uint32_t trgper)
 Configure the ADCIFB trigger mode. More...
 
int32_t adcifb_disable (volatile avr32_adcifb_t *adcifb)
 Disable ADCIFB. More...
 
static void adcifb_disable_all_interrupts (volatile avr32_adcifb_t *adcifb)
 Disable all ADCIFB interrupts. More...
 
static void adcifb_disable_busy_interrupt (volatile avr32_adcifb_t *adcifb)
 Disable ADCIFB Busy Interrupt. More...
 
static void adcifb_disable_compare_else_interrupt (volatile avr32_adcifb_t *adcifb)
 Disable ADCIFB Compare Else interrupt. More...
 
static void adcifb_disable_compare_gt_interrupt (volatile avr32_adcifb_t *adcifb)
 Disable ADCIFB Compare Greater than interrupt. More...
 
static void adcifb_disable_compare_lt_interrupt (volatile avr32_adcifb_t *adcifb)
 Disable ADCIFB Compare Less than interrupt. More...
 
static void adcifb_disable_data_ready_interrupt (volatile avr32_adcifb_t *adcifb)
 Disable ADCIFB Data Ready Interrupt. More...
 
static void adcifb_disable_interrupt (volatile avr32_adcifb_t *adcifb, uint32_t interrupt_mask)
 Disable ADCIFB interrupts. More...
 
static void adcifb_disable_no_contact_interrupt (volatile avr32_adcifb_t *adcifb)
 Disable ADCIFB No Contact Interrupt. More...
 
static void adcifb_disable_overrun_error_interrupt (volatile avr32_adcifb_t *adcifb)
 Disable ADCIFB Overrun Error Interrupt. More...
 
static void adcifb_disable_pen_contact_interrupt (volatile avr32_adcifb_t *adcifb)
 Disable ADCIFB Pen Contact Interrupt. More...
 
static void adcifb_disable_ready_interrupt (volatile avr32_adcifb_t *adcifb)
 Disable ADCIFB Ready Interrupt. More...
 
static void adcifb_enable_analog_compare_mode (volatile avr32_adcifb_t *adcifb)
 Enable Analog Compare mode in ADCIFB. More...
 
static void adcifb_enable_analog_pin_output (volatile avr32_adcifb_t *adcifb)
 Enable Analog Pin output when using touch screen mode in ADCIFB. More...
 
static void adcifb_enable_busy_interrupt (volatile avr32_adcifb_t *adcifb)
 Enable ADCIFB Busy Interrupt. More...
 
static void adcifb_enable_compare_else_interrupt (volatile avr32_adcifb_t *adcifb)
 Enable ADCIFB Compare Else interrupt. More...
 
static void adcifb_enable_compare_gt_interrupt (volatile avr32_adcifb_t *adcifb)
 Enable ADCIFB Compare Greater than interrupt. More...
 
static void adcifb_enable_compare_lt_interrupt (volatile avr32_adcifb_t *adcifb)
 Enable ADCIFB Compare Less than interrupt. More...
 
static void adcifb_enable_data_ready_interrupt (volatile avr32_adcifb_t *adcifb)
 Enable ADCIFB Data Ready Interrupt. More...
 
static void adcifb_enable_interrupt (volatile avr32_adcifb_t *adcifb, uint32_t interrupt_mask)
 Enable ADCIFB interrupts. More...
 
static void adcifb_enable_no_contact_interrupt (volatile avr32_adcifb_t *adcifb)
 Enable ADCIFB No Contact Interrupt. More...
 
static void adcifb_enable_overrun_error_interrupt (volatile avr32_adcifb_t *adcifb)
 Enable ADCIFB Overrun Error Interrupt. More...
 
static void adcifb_enable_pen_contact_interrupt (volatile avr32_adcifb_t *adcifb)
 Enable ADCIFB Pen Contact Interrupt. More...
 
void adcifb_enable_pen_detect_mode (volatile avr32_adcifb_t *adcifb, uint8_t pen_dbc_period)
 Enable Pen Detect mode in ADCIFB. More...
 
static void adcifb_enable_ready_interrupt (volatile avr32_adcifb_t *adcifb)
 Enable ADCIFB Ready Interrupt. More...
 
void adcifb_enable_touch_screen_mode (volatile avr32_adcifb_t *adcifb, uint8_t touch_screen_pin_offset, bool analog_pin_output_enable)
 Enable Touch Screen mode in ADCIFB. More...
 
uint32_t adcifb_get_last_data (volatile avr32_adcifb_t *adcifb)
 Get Last Converted data. More...
 
bool adcifb_is_busy (volatile avr32_adcifb_t *adcifb)
 Check if the ADCIFB is busy. More...
 
bool adcifb_is_drdy (volatile avr32_adcifb_t *adcifb)
 Check if one or more data has been converted since the start of conversion and is available. More...
 
bool adcifb_is_ovre (volatile avr32_adcifb_t *adcifb)
 Check if one or more Overrun Error has occurred since the start of conversion. More...
 
bool adcifb_is_ready (volatile avr32_adcifb_t *adcifb)
 Check if the ADCIFB is ready to perform a conversion sequence. More...
 
static void adcifb_reset (volatile avr32_adcifb_t *adcifb)
 Resets the ADCIFB module(software reset) More...
 
static void adcifb_set_high_compare_value (volatile avr32_adcifb_t *adcifb, uint32_t compare_value)
 Set the ADCIFB Compare High Value Register. More...
 
static void adcifb_set_low_compare_value (volatile avr32_adcifb_t *adcifb, uint32_t compare_value)
 Set the ADCIFB Compare Low Value Register. More...
 
static void adcifb_set_pen_debouncing_period (volatile avr32_adcifb_t *adcifb, uint8_t pen_dbc_period)
 Set the ADCIFB Pen Detect Debouncing Period. More...
 
static void adcifb_set_touch_screen_pin_offset (volatile avr32_adcifb_t *adcifb, uint8_t touch_screen_pin_offset)
 Set the ADCIFB Touch Screen Pin Offset value. More...
 
int32_t adcifb_sr_statushigh_wait (volatile avr32_adcifb_t *adcifb, uint32_t statusMask)
 Wait for a status high in the ADCIFB SR status register. More...
 
static void adcifb_start_conversion_sequence (volatile avr32_adcifb_t *adcifb)
 Start an ADC conversion sequence (Software trigger) More...
 

#define ADCIFB_POLL_TIMEOUT   10000

The timeguard used for polling.

Referenced by adcifb_disable(), and adcifb_sr_statushigh_wait().

static void adcifb_channels_disable ( volatile avr32_adcifb_t *  adcifb,
uint32_t  channels_mask 
)
inlinestatic

Disable one or several channels.

Parameters
*adcifbBase address of the ADCIFB module
channels_maskBitmask of channels to disable
static void adcifb_channels_enable ( volatile avr32_adcifb_t *  adcifb,
uint32_t  channels_mask 
)
inlinestatic

Enable one or several channels.

Parameters
*adcifbBase address of the ADCIFB module
channels_maskBitmask of channels to enable

Referenced by init_adc().

static void adcifb_clear_all_interrupt_flags ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Clear all ADCIFB interrupt flags.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_clear_busy_interrupt_flag ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Clear ADCIFB Busy Interrupt flag.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_clear_compare_else_interrupt_flag ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Clear ADCIFB Compare Else interrupt flag.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_clear_compare_gt_interrupt_flag ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Clear ADCIFB Compare Greater than interrupt flag.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_clear_compare_lt_interrupt_flag ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Clear ADCIFB Compare Less than interrupt flag.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_clear_data_ready_interrupt_flag ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Clear ADCIFB Data Ready Interrupt flag.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_clear_interrupt_flag ( volatile avr32_adcifb_t *  adcifb,
uint32_t  interrupt_mask 
)
inlinestatic

Clear ADCIFB interrupt flags.

Parameters
*adcifbBase address of the ADCIFB module
interrupt_maskBitmask of interrupts to clear
static void adcifb_clear_no_contact_interrupt_flag ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Clear ADCIFB No Contact Interrupt flag.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_clear_overrun_error_interrupt_flag ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Clear ADCIFB Overrun Error Interrupt flag.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_clear_pen_contact_interrupt_flag ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Clear ADCIFB Pen Contact Interrupt flag.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_clear_ready_interrupt_flag ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Clear ADCIFB Ready Interrupt flag.

Parameters
*adcifbBase address of the ADCIFB module
int32_t adcifb_configure ( volatile avr32_adcifb_t *  adcifb,
const adcifb_opt_t p_adcifb_opt 
)

Initialize the ADCIFB module (enable and configure).

   Mandatory to call.
Parameters
*adcifbBase address of the ADCIFB module
p_adcifb_optStructure for the ADCIFB module configuration
Note
To avoid an infinite loop, this function checks ADCIFB READY status bit but no more than ADCIFB_POLL_TIMEOUT times.
Returns
Status.
Return values
0ADCIFB successfully enabled and configured
<0ADCIFB initialization failed.

References adcifb_sr_statushigh_wait(), adcifb_opt_t::ratio_clkadcifb_clkadc, adcifb_opt_t::resolution, adcifb_opt_t::shtim, adcifb_opt_t::sleep_mode_enable, and adcifb_opt_t::startup.

Referenced by init_adc().

int32_t adcifb_configure_trigger ( volatile avr32_adcifb_t *  adcifb,
uint8_t  trgmod,
uint32_t  trgper 
)

Configure the ADCIFB trigger mode.

Parameters
*adcifbBase address of the ADCIFB module
trgmodTrigger mode, one of AVR32_ADCIFB_TRGR_TRGMOD_* defines (cf adcifb_xxx.h part header file)
trgperDefines the Trigger period where Trigger Period = trgper *Tclk_adc (effective only if trigger_mode==AVR32_ADCIFB_TRGMOD_PT)
Returns
Status.
Return values
0ADCIFB trigger mode successfully configured
<0ADCIFB trigger mode configuration failed.

References PASS.

Referenced by init_adc().

int32_t adcifb_disable ( volatile avr32_adcifb_t *  adcifb)

Disable ADCIFB.

Parameters
*adcifbBase address of the ADCIFB module
Returns
Status.
Return values
0ADCIFB successfully disabled
<0ADCIFB configuration failed.

References adcifb_is_busy(), ADCIFB_POLL_TIMEOUT, and PASS.

static void adcifb_disable_all_interrupts ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Disable all ADCIFB interrupts.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_disable_busy_interrupt ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Disable ADCIFB Busy Interrupt.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_disable_compare_else_interrupt ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Disable ADCIFB Compare Else interrupt.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_disable_compare_gt_interrupt ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Disable ADCIFB Compare Greater than interrupt.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_disable_compare_lt_interrupt ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Disable ADCIFB Compare Less than interrupt.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_disable_data_ready_interrupt ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Disable ADCIFB Data Ready Interrupt.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_disable_interrupt ( volatile avr32_adcifb_t *  adcifb,
uint32_t  interrupt_mask 
)
inlinestatic

Disable ADCIFB interrupts.

Parameters
*adcifbBase address of the ADCIFB module
interrupt_maskBitmask of interrupts to disable
static void adcifb_disable_no_contact_interrupt ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Disable ADCIFB No Contact Interrupt.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_disable_overrun_error_interrupt ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Disable ADCIFB Overrun Error Interrupt.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_disable_pen_contact_interrupt ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Disable ADCIFB Pen Contact Interrupt.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_disable_ready_interrupt ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Disable ADCIFB Ready Interrupt.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_enable_analog_compare_mode ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Enable Analog Compare mode in ADCIFB.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_enable_analog_pin_output ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Enable Analog Pin output when using touch screen mode in ADCIFB.

Parameters
*adcifbBase address of the ADCIFB module

Referenced by adcifb_enable_touch_screen_mode().

static void adcifb_enable_busy_interrupt ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Enable ADCIFB Busy Interrupt.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_enable_compare_else_interrupt ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Enable ADCIFB Compare Else interrupt.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_enable_compare_gt_interrupt ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Enable ADCIFB Compare Greater than interrupt.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_enable_compare_lt_interrupt ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Enable ADCIFB Compare Less than interrupt.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_enable_data_ready_interrupt ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Enable ADCIFB Data Ready Interrupt.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_enable_interrupt ( volatile avr32_adcifb_t *  adcifb,
uint32_t  interrupt_mask 
)
inlinestatic

Enable ADCIFB interrupts.

Parameters
*adcifbBase address of the ADCIFB module
interrupt_maskBitmask of interrupts to enable
static void adcifb_enable_no_contact_interrupt ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Enable ADCIFB No Contact Interrupt.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_enable_overrun_error_interrupt ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Enable ADCIFB Overrun Error Interrupt.

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_enable_pen_contact_interrupt ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Enable ADCIFB Pen Contact Interrupt.

Parameters
*adcifbBase address of the ADCIFB module
void adcifb_enable_pen_detect_mode ( volatile avr32_adcifb_t *  adcifb,
uint8_t  pen_dbc_period 
)

Enable Pen Detect mode in ADCIFB.

Parameters
*adcifbBase address of the ADCIFB module
pen_dbc_periodPen Detect Debouncing Period

References adcifb_set_pen_debouncing_period().

static void adcifb_enable_ready_interrupt ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Enable ADCIFB Ready Interrupt.

Parameters
*adcifbBase address of the ADCIFB module
void adcifb_enable_touch_screen_mode ( volatile avr32_adcifb_t *  adcifb,
uint8_t  touch_screen_pin_offset,
bool  analog_pin_output_enable 
)

Enable Touch Screen mode in ADCIFB.

Parameters
*adcifbBase address of the ADCIFB module
touch_screen_pin_offsetThe Touch Screen Pin Offset field is used to indicate which AD pins are connected to the resistive touch screen film edges.
analog_pin_output_enableEnable Analog Pin Output in ADCIFB
Warning
If the selected I/O voltage configuration is incompatible with the ADC cell voltage specification, analog_pin_output_enable must stay cleared to avoid damaging the ADC. In this case the ADP pins must be used to drive VDD instead. If the I/O and ADC voltages are compatible, the AD pins can be used directly by writing a one to this bit. In this case the ADP pins can be ignored.

References adcifb_enable_analog_pin_output(), and adcifb_set_touch_screen_pin_offset().

uint32_t adcifb_get_last_data ( volatile avr32_adcifb_t *  adcifb)

Get Last Converted data.

Parameters
*adcifbBase address of the ADCIFB module
Returns
The value acquired (uint32_t)
Warning
The return value contains the converted data in the bits[0-11]; bits[16-23] contain the channel id that was last converted.

Referenced by main().

bool adcifb_is_busy ( volatile avr32_adcifb_t *  adcifb)

Check if the ADCIFB is busy.

Parameters
*adcifbBase address of the ADCIFB module
Returns
bool true if ADCIFB is busy. false if ADCIFB is idle.

Referenced by adcifb_disable().

bool adcifb_is_drdy ( volatile avr32_adcifb_t *  adcifb)

Check if one or more data has been converted since the start of conversion and is available.

Parameters
*adcifbBase address of the ADCIFB module
Returns
bool true if one or more data has been converted since the start of conversion and is available false if no data has been converted since the start of conversion

Referenced by main().

bool adcifb_is_ovre ( volatile avr32_adcifb_t *  adcifb)

Check if one or more Overrun Error has occurred since the start of conversion.

Parameters
*adcifbBase address of the ADCIFB module
Returns
bool true if an overrun has occurred false if no overrun occurred
bool adcifb_is_ready ( volatile avr32_adcifb_t *  adcifb)

Check if the ADCIFB is ready to perform a conversion sequence.

Parameters
*adcifbBase address of the ADCIFB module
Returns
bool true if ADCIFB is ready to perform conversion sequence. false if ADCIFB is not ready to perform conversion sequence.

Referenced by main().

static void adcifb_reset ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Resets the ADCIFB module(software reset)

Parameters
*adcifbBase address of the ADCIFB module
static void adcifb_set_high_compare_value ( volatile avr32_adcifb_t *  adcifb,
uint32_t  compare_value 
)
inlinestatic

Set the ADCIFB Compare High Value Register.

Parameters
*adcifbBase address of the ADCIFB module
compare_valueValue to be compared
static void adcifb_set_low_compare_value ( volatile avr32_adcifb_t *  adcifb,
uint32_t  compare_value 
)
inlinestatic

Set the ADCIFB Compare Low Value Register.

Parameters
*adcifbBase address of the ADCIFB module
compare_valueValue to be compared
static void adcifb_set_pen_debouncing_period ( volatile avr32_adcifb_t *  adcifb,
uint8_t  pen_dbc_period 
)
inlinestatic

Set the ADCIFB Pen Detect Debouncing Period.

Parameters
*adcifbBase address of the ADCIFB module
pen_dbc_periodDebouncing period

Referenced by adcifb_enable_pen_detect_mode().

static void adcifb_set_touch_screen_pin_offset ( volatile avr32_adcifb_t *  adcifb,
uint8_t  touch_screen_pin_offset 
)
inlinestatic

Set the ADCIFB Touch Screen Pin Offset value.

Parameters
*adcifbBase address of the ADCIFB module
touch_screen_pin_offsetOffset value

Referenced by adcifb_enable_touch_screen_mode().

int32_t adcifb_sr_statushigh_wait ( volatile avr32_adcifb_t *  adcifb,
uint32_t  statusMask 
)

Wait for a status high in the ADCIFB SR status register.

Parameters
*adcifbBase address of the ADCIFB module
statusMaskMask field of the status to poll
Returns
Status.
Return values
0Status is high.
<0ADCIFB_POLL_TIMEOUT Timeout expired before the status was high

References ADCIFB_POLL_TIMEOUT, and PASS.

Referenced by adcifb_configure().

static void adcifb_start_conversion_sequence ( volatile avr32_adcifb_t *  adcifb)
inlinestatic

Start an ADC conversion sequence (Software trigger)

Parameters
*adcifbBase address of the ADCIFB module

Referenced by main().