Macros | |
#define | _DEBUG_INTERFACE_ |
Enable/Disable QDebug for touch debug information communication with QTouch Studio PC Software. More... | |
#define | _QMATRIX_ |
#define | _ROTOR_SLIDER_ |
If ATxmega device is used. More... | |
#define | DEF_QT_DI 4u |
#define | DEF_QT_DRIFT_HOLD_TIME 20 /* 4s */ |
#define | DEF_QT_MAX_ON_DURATION 0 /* disabled */ |
#define | DEF_QT_NEG_DRIFT_RATE 20 /* 4s per LSB */ |
#define | DEF_QT_POS_DRIFT_RATE 5 /* 1s per LSB */ |
#define | DEF_QT_POS_RECAL_DELAY 3u |
#define | DEF_QT_RECAL_THRESHOLD RECAL_50 /* recal threshold = 50% of detect */ |
#define | DEF_QTOUCH_INTERFACE_TYPE (2) |
Select the type of interface to use for the debug protocol. More... | |
#define | MISO_BB 6 |
#define | MOSI_BB 5 |
#define | NUM_X_LINES 8 |
Define the Number X lines to be used. More... | |
#define | NUM_X_PORTS 1 |
Specify the number of ports on which X-lines that are distributed. More... | |
#define | NUM_Y_LINES 8 |
Define the Number Y lines and port for YA, YB to be used. More... | |
#define | PORT_NUM_1 1 |
#define | PORT_SMP G |
Specify the port for SMP. More... | |
#define | PORT_X_1 D |
Specify Which ports have X lines on them. More... | |
#define | PORT_YA B |
#define | PORT_YB F |
#define | PROJECT_ID 0x33 |
#define | QT_DELAY_CYCLES 4 |
Example configuration based on option selected in project options. More... | |
#define | QT_MAX_NUM_ROTORS_SLIDERS 4 |
#define | QT_NUM_CHANNELS 64 |
Number of Channels(dependent on the library used and application requirement). More... | |
#define | SCK_BB 7 |
#define | SHARED_YAYB 0 |
Specify if YA and YB share the same port. More... | |
#define | SMP_PIN 4 |
#define | SPI_BB_MISO E |
#define | SPI_BB_MOSI E |
#define | SPI_BB_SCK E |
#define | SPI_BB_SS E |
#define | SS_BB 4 |
Bit bang SPI port and pin configuration. More... | |
#define | TICKS_PER_MS 500u |
Total ticks per msec. More... | |
#define _DEBUG_INTERFACE_ |
Enable/Disable QDebug for touch debug information communication with QTouch Studio PC Software.
QDebug is enabled by defining the below macro.
#define _QMATRIX_ |
#define _ROTOR_SLIDER_ |
If ATxmega device is used.
Possible values: comment/uncomment the lines The following rules need to be followed while configuring the QTouch library for QTouch acquisition method.
#define QT_DELAY_CYCLES
The value for QT_NUM_CHANNELS should match the library chosen. For example, when using libavr5g4-64qm-8x-8y-krs-4rs.a library, set QT_NUM_CHANNELS to 64 only.
#define NUM_X_PORTS
#define PORT_NUM_1
#define PORT_NUM_2 <value, if using 2 X ports> #define PORT_NUM_3 <value, if using 3 X ports> #define PORT_X_1
#define PORT_X_2 <value, if using 2 X ports> #define PORT_X_3 <value, if using 3 X ports>
#define PORT_YA
#define PORT_YB
#define SMP_PIN
The value for QT_MAX_NUM_ROTOR_SLIDER should match the library chosen. For example, when using libavr5g4-64qm-8x-8y-krs-4rs.a library, set QT_MAX_NUM_ROTOR_SLIDER to 4 only.
#define DEF_QT_DI 4u |
Referenced by qt_set_parameters().
#define DEF_QT_DRIFT_HOLD_TIME 20 /* 4s */ |
Referenced by qt_set_parameters().
#define DEF_QT_MAX_ON_DURATION 0 /* disabled */ |
Referenced by qt_set_parameters().
#define DEF_QT_NEG_DRIFT_RATE 20 /* 4s per LSB */ |
Referenced by qt_set_parameters().
#define DEF_QT_POS_DRIFT_RATE 5 /* 1s per LSB */ |
Referenced by qt_set_parameters().
#define DEF_QT_POS_RECAL_DELAY 3u |
Referenced by qt_set_parameters().
#define DEF_QT_RECAL_THRESHOLD RECAL_50 /* recal threshold = 50% of detect */ |
Referenced by qt_set_parameters().
#define DEF_QTOUCH_INTERFACE_TYPE (2) |
Select the type of interface to use for the debug protocol.
When 0, QDebug interface type is on-chip SPI peripheral When 1, QDebug interface type is on-chip TWI peripheral When 2, QDebug interface type is Bit bang SPI
#define MISO_BB 6 |
Referenced by BitBangSPI_Master_Init(), and BitBangSPI_Send_Byte().
#define MOSI_BB 5 |
Referenced by BitBangSPI_Master_Init(), and BitBangSPI_Send_Byte().
#define NUM_X_LINES 8 |
Define the Number X lines to be used.
Possible values: 4 and 8 Depending on the library used.Please refer to the QTouch library user guide.pdf and library selection guide.xls more information on selecting the number of channels.
#define NUM_X_PORTS 1 |
Specify the number of ports on which X-lines that are distributed.
Note: Support is provided only for a maximum of 3 ports for X. ( Maximum possible value for NUM_X_PORTS is 3) Possible values: 1,2,3 Also, note that code memory increases with the number of ports used for X lines.
#define NUM_Y_LINES 8 |
Define the Number Y lines and port for YA, YB to be used.
Possible values: NUM_Y_LINES is 1, 2, 4 and 8 Depending on the library used. Please refer to the QTouch library user guide.pdf and library selection guide.xls for more information on selecting the number of channels, YA and YB ports.
#define PORT_NUM_1 1 |
#define PORT_SMP G |
Specify the port for SMP.
And Specify the pin for SMP on selected SMP port. Any GPIO pin not conflicting with the other touch pins used for the application
#define PORT_X_1 D |
Specify Which ports have X lines on them.
These macros are used to conditionally compile in support for ports driving X lines.
#define PORT_YA B |
#define PORT_YB F |
#define PROJECT_ID 0x33 |
Referenced by Transmit_Sign_On().
#define QT_DELAY_CYCLES 4 |
Example configuration based on option selected in project options.
For user configuration make changes to the custom user configuration section above. Info on the below configuration macros refer above notes. Delay cycles that determine the capacitance charge pulse width. Value of 0 will enable charge pulse width of 1 clock cycle, 1 will enable a width of 2 clock cycles and so on...
Possible values: 1,2,3,4,5,10,25
#define QT_MAX_NUM_ROTORS_SLIDERS 4 |
Referenced by Transmit_State().
#define QT_NUM_CHANNELS 64 |
Number of Channels(dependent on the library used and application requirement).
The least possible number more that the application needs. Please refer to the QTouch library user guide.pdf and library selection guide.xls more information on selecting the number of channels.
Possible values: 4, 8, 16, 32, 56, 64. in case of QMatrix.
Referenced by read_settings_from_eeprom(), Set_QM_Burst_Lengths(), Transmit_Burst_Lengths(), Transmit_Ref(), Transmit_Sensor_Config(), Transmit_Sign_On(), Transmit_Signals(), Transmit_State(), and write_burst_lenghts_to_eeprom().
#define SCK_BB 7 |
Referenced by BitBangSPI_Master_Init(), and BitBangSPI_Send_Byte().
#define SHARED_YAYB 0 |
Specify if YA and YB share the same port.
Set the value of the below macro to '1' if the YA and YB pins are share in same port.
#define SMP_PIN 4 |
#define SPI_BB_MISO E |
Referenced by BitBangSPI_Master_Init(), and BitBangSPI_Send_Byte().
#define SPI_BB_MOSI E |
Referenced by BitBangSPI_Master_Init(), and BitBangSPI_Send_Byte().
#define SPI_BB_SCK E |
Referenced by BitBangSPI_Master_Init(), and BitBangSPI_Send_Byte().
#define SPI_BB_SS E |
Referenced by BitBangSPI_Master_Init().
#define SS_BB 4 |
Bit bang SPI port and pin configuration.
Note: Ensure that the port pins mentioned below are not used for SNS/SNSK
Referenced by BitBangSPI_Master_Init().
#define TICKS_PER_MS 500u |
Total ticks per msec.
TICKS_PER_MS = (CLK_FREQ/TIMER_PRESCALER)*(1/1000) Current Clock frequency is 4Mhz, and Timer Prescaler is 8