Microchip® Advanced Software Framework

QDebug.c File Reference
#include "touch_api.h"
#include "QDebug.h"
#include "QDebugTransport.h"
#include "QDebugSettings.h"
#include "eeprom_access_mega.h"
#include "BitBangSPI_Master.h"

Functions

void QDebug_Init (void)
 This API initializes QDebug interface. More...
 
void QDebug_ProcessCommands (void)
 Command handler for the data received from QTouch Studio. More...
 
void QDebug_SendData (uint16_t qt_lib_flags)
 Send data to QTouch Studio based on the subscription. More...
 
void QDebug_SetSubscriptions (uint16_t once, uint16_t change, uint16_t allways)
 Set subscription values. More...
 
void Set_Channel_Config (void)
 Extract the data packet from QTouch Studio and set channel config. More...
 
void Set_Global_Config (void)
 Extract the data packet from QTouch Studio and set global config. More...
 
void Set_QM_Burst_Lengths (void)
 Set QMatrix burst lengths. More...
 
void Set_QT_User_Data (uint8_t *pdata)
 Extracts user data from QTouch Studio to touch mcu memory. More...
 
void Set_Subscriptions (void)
 Set Data Subscription values. More...
 
void Transmit_Burst_Lengths (void)
 Transmits the QMatrix burst length values to QTouch Studio. More...
 
void Transmit_Delta (void)
 Transmits the channel delta values to QTouch Studio. More...
 
void Transmit_Dummy (void)
 Transmits a dummy packet if no other subscriptions are set. More...
 
void Transmit_Global_Config (void)
 Transmits the global config struct to QTouch Studio. More...
 
void Transmit_QT_User_Data (uint8_t *pdata, uint16_t c)
 Transmits user data to QTouch Studio. More...
 
void Transmit_Ref (void)
 Transmits the channel reference values to QTouch Studio. More...
 
void Transmit_Sensor_Config (void)
 Transmits the channel config struct to QTouch Studio. More...
 
void Transmit_Sign_On (void)
 Transmits the sign on packet to QTouch Studio. More...
 
void Transmit_Signals (void)
 Transmits the measurement values for each channel to QTouch Studio. More...
 
void Transmit_State (void)
 Transmits the state values to QTouch Studio. More...
 
void Transmit_Time_Stamps (void)
 Transmits the application execution timestamp values to QTouch Studio. More...
 

Variables

static uint16_t delivery = 0
 Subscriptions. More...
 
qt_lib_siginfo_t lib_siginfo
 
uint8_t num_sensors
 
static uint16_t qgLibraryChanges = 0
 
uint8_t qgRefschanged
 These must somehow be updated from the library. More...
 
uint8_t qgStateschanged
 
static uint16_t qgSubsAllways = 0
 
static uint16_t qgSubsChange = 0
 
static uint16_t qgSubsOnce = 0
 
uint16_t timestamp1_hword
 Time stamp information. More...
 
uint16_t timestamp1_lword
 
uint16_t timestamp2_hword
 
uint16_t timestamp2_lword
 
uint16_t timestamp3_hword
 
uint16_t timestamp3_lword
 

void QDebug_Init ( void  )

This API initializes QDebug interface.

This API initializes QDebug interface, including the low level hardware interface (SPI, TWI, USART etc).

Note
Must be called before the main loop

References BitBangSPI_Master_Init(), Init_Buffers(), qt_lib_sig_info_t::library_version, qt_get_library_sig(), read_info_from_eeprom(), read_settings_from_eeprom(), write_burst_lenghts_to_eeprom(), write_global_settings_to_eeprom(), write_info_to_eeprom(), and write_sensor_settings_to_eeprom().

Referenced by main().

void QDebug_ProcessCommands ( void  )

Command handler for the data received from QTouch Studio.

Note
This function should be called in the main loop after measure_sensors to process the data received from QTOuch Studio.

References GetChar(), QT_CMD_DUMMY, QT_CMD_SET_CH_CONFIG, QT_CMD_SET_GLOBAL_CONFIG, QT_CMD_SET_QM_BURST_LENGTHS, QT_CMD_SET_SUBS, QT_CMD_SET_USER_DATA, Receive_Message(), RX_Buffer, RX_index, Set_Channel_Config(), Set_Global_Config(), Set_QM_Burst_Lengths(), Set_QT_User_Data(), and Set_Subscriptions().

Referenced by main().

void QDebug_SendData ( uint16_t  qt_lib_flags)

Send data to QTouch Studio based on the subscription.

Parameters
qt_lib_flags:Changeflag from measure_sensors.
Note
This function should be called in the main loop after measure_sensors to send the measured touch data

References delivery, qgLibraryChanges, qgSubsAllways, qgSubsChange, qgSubsOnce, QTLIB_CHANNEL_REF_CHANGE, QTLIB_ROTOR_SLIDER_POS_CHANGE, QTLIB_STATUS_CHANGE, SequenceH, SUBS_DELTA, SUBS_GLOBAL_CONFIG, SUBS_REF, SUBS_SENSOR_CONFIG, SUBS_SIGN_ON, SUBS_SIGNALS, SUBS_STATES, Transmit_Delta(), Transmit_Dummy(), Transmit_Global_Config(), Transmit_Ref(), Transmit_Sensor_Config(), Transmit_Sign_On(), Transmit_Signals(), and Transmit_State().

Referenced by main().

void QDebug_SetSubscriptions ( uint16_t  once,
uint16_t  change,
uint16_t  allways 
)

Set subscription values.

Note
This function can be used directly in main to set data subscription if 1way SPI interface is used.

References qgSubsAllways, qgSubsChange, and qgSubsOnce.

Referenced by Set_Subscriptions().

void Set_Channel_Config ( void  )

Extract the data packet from QTouch Studio and set channel config.

Note
Should only be called from the command handler.

References GetChar(), sensors, tag_sensor_t::threshold, tag_sensor_t::type_aks_pos_hyst, and write_sensor_settings_to_eeprom().

Referenced by QDebug_ProcessCommands().

void Set_QM_Burst_Lengths ( void  )

Set QMatrix burst lengths.

Extract the data packet from QTouch Studio and set QMatrix burst lengths.

Note
Should only be called from the command handler.

References GetChar(), qt_burst_lengths, QT_NUM_CHANNELS, and write_burst_lenghts_to_eeprom().

Referenced by QDebug_ProcessCommands().

void Set_QT_User_Data ( uint8_t *  pdata)

Extracts user data from QTouch Studio to touch mcu memory.

Parameters
datapointer
Note
The data can be binary data

References PutChar(), RX_Buffer, and Send_Message().

Referenced by QDebug_ProcessCommands().

void Set_Subscriptions ( void  )

Set Data Subscription values.

Note
Should only be called from the command handler.

References GetChar(), and QDebug_SetSubscriptions().

Referenced by QDebug_ProcessCommands().

void Transmit_Burst_Lengths ( void  )

Transmits the QMatrix burst length values to QTouch Studio.

Note
This value is available for each channel

References PutChar(), qt_burst_lengths, QT_NUM_CHANNELS, and Send_Message().

void Transmit_Delta ( void  )

Transmits the channel delta values to QTouch Studio.

Note
The value is equal to signal-reference

References num_sensors, PutChar(), QT_DELTAS, qt_get_sensor_delta(), and Send_Message().

Referenced by QDebug_SendData().

void Transmit_Dummy ( void  )

Transmits a dummy packet if no other subscriptions are set.

Note

References PutChar(), QT_DUMMY, and Send_Message().

Referenced by QDebug_SendData().

void Transmit_QT_User_Data ( uint8_t *  pdata,
uint16_t  c 
)

Transmits user data to QTouch Studio.

Parameters
datapointer, length of data in bytes
Note
The data will be binary data

References PutChar(), and Send_Message().

void Transmit_Ref ( void  )

Transmits the channel reference values to QTouch Studio.

Note

References tag_qt_touch_lib_measure_data_t::channel_references, PutChar(), qt_measure_data, QT_NUM_CHANNELS, QT_REFERENCES, and Send_Message().

Referenced by QDebug_SendData().

void Transmit_Sensor_Config ( void  )

Transmits the channel config struct to QTouch Studio.

Note

References PutChar(), QT_NUM_CHANNELS, QT_SENSOR_CONFIG, Send_Message(), and sensors.

Referenced by QDebug_SendData().

void Transmit_Sign_On ( void  )
void Transmit_Signals ( void  )

Transmits the measurement values for each channel to QTouch Studio.

Note

References tag_qt_touch_lib_measure_data_t::channel_signals, PutChar(), qt_measure_data, QT_NUM_CHANNELS, QT_SIGNALS, and Send_Message().

Referenced by QDebug_SendData().

void Transmit_Time_Stamps ( void  )

Transmits the application execution timestamp values to QTouch Studio.

Note
This value is a combination of current_time_ms_touch (high word) & timer counter register (low word)

References PutInt(), Send_Message(), timestamp1_hword, timestamp1_lword, timestamp2_hword, timestamp2_lword, timestamp3_hword, and timestamp3_lword.

uint16_t delivery = 0
static

Subscriptions.

Referenced by QDebug_SendData(), and Transmit_Sign_On().

qt_lib_siginfo_t lib_siginfo
uint16_t qgLibraryChanges = 0
static

Referenced by QDebug_SendData().

uint8_t qgRefschanged

These must somehow be updated from the library.

uint8_t qgStateschanged
uint16_t qgSubsAllways = 0
static
uint16_t qgSubsChange = 0
static
uint16_t qgSubsOnce = 0
static
uint16_t timestamp1_hword

Time stamp information.

uint16_t timestamp1_lword
uint16_t timestamp2_hword
uint16_t timestamp2_lword
uint16_t timestamp3_hword
uint16_t timestamp3_lword