#include "touch_api.h"
Macros | |
Subscription definitions. | |
#define | SUBS_SIGN_ON 0 |
#define | SUBS_GLOBAL_CONFIG 1 |
#define | SUBS_SENSOR_CONFIG 2 |
#define | SUBS_SIGNALS 3 |
#define | SUBS_REF 4 |
#define | SUBS_DELTA 5 |
#define | SUBS_STATES 6 |
PC commands. | |
#define | QT_CMD_DUMMY 0x10 |
#define | QT_CMD_SET_SUBS 0x11 |
#define | QT_CMD_SET_GLOBAL_CONFIG 0x12 |
#define | QT_CMD_SET_CH_CONFIG 0x13 |
#define | QT_CMD_SET_QM_BURST_LENGTHS 0x14 |
#define | QT_CMD_SET_USER_DATA 0x15 |
Touch MCU data packets. | |
#define | QT_DUMMY 0x20 |
#define | QT_SIGN_ON 0x21 |
#define | QT_GLOBAL_CONFIG 0x22 |
#define | QT_SENSOR_CONFIG 0x23 |
#define | QT_SIGNALS 0x24 |
#define | QT_REFERENCES 0x25 |
#define | QT_DELTAS 0x26 |
#define | QT_STATES 0x27 |
Functions | |
Public functions. | |
void | QDebug_Init (void) |
This API initializes QDebug interface, including the low level hardware interface (SPI, TWI, USART etc). More... | |
void | QDebug_ProcessCommands (void) |
Command handler for the data received from QTouch Studio. More... | |
void | QDebug_SendData (uint16_t qt_lib_flags) |
Send data to QTouch Studio based on the subscription. More... | |
void | QDebug_SetSubscriptions (uint16_t once, uint16_t change, uint16_t allways) |
Set subscription values. More... | |
Private functions. | |
void | Set_Global_Config (void) |
Extract the data packet from QTouch Studio and set global config. More... | |
void | Set_Channel_Config (void) |
Extract the data packet from QTouch Studio and set channel config. More... | |
void | Set_Subscriptions (void) |
Set Data Subscription values. More... | |
void | Set_Measurement_Period (void) |
Extract the data packet from QTouch Studio and set measurement period. More... | |
void | Set_QT_User_Data (uint8_t *) |
Extracts user data from QTouch Studio to touch mcu memory. More... | |
void | Set_QM_Burst_Lengths (void) |
Extract the data packet from QTouch Studio and set QMatrix burst lengths. More... | |
void | Transmit_Dummy (void) |
Transmits a dummy packet if no other subscriptions are set. More... | |
void | Transmit_Sign_On (void) |
Transmits the sign on packet to QTouch Studio. More... | |
void | Transmit_Global_Config (void) |
Transmits the global config struct to QTouch Studio. More... | |
void | Transmit_Sensor_Config (void) |
Transmits the channel config struct to QTouch Studio. More... | |
void | Transmit_Signals (void) |
Transmits the measurement values for each channel to QTouch Studio. More... | |
void | Transmit_Ref (void) |
Transmits the channel reference values to QTouch Studio. More... | |
void | Transmit_Delta (void) |
Transmits the channel delta values to QTouch Studio. More... | |
void | Transmit_State (void) |
Transmits the state values to QTouch Studio. More... | |
void | Transmit_QT_User_Data (uint8_t *pdata, uint16_t c) |
Transmits user data to QTouch Studio. More... | |
void | Transmit_Time_Stamps (void) |
Transmits the application execution timestamp values to QTouch Studio. More... | |
#define QT_CMD_DUMMY 0x10 |
Referenced by QDebug_ProcessCommands().
#define QT_CMD_SET_CH_CONFIG 0x13 |
Referenced by QDebug_ProcessCommands().
#define QT_CMD_SET_GLOBAL_CONFIG 0x12 |
Referenced by QDebug_ProcessCommands().
#define QT_CMD_SET_QM_BURST_LENGTHS 0x14 |
Referenced by QDebug_ProcessCommands().
#define QT_CMD_SET_SUBS 0x11 |
Referenced by QDebug_ProcessCommands().
#define QT_CMD_SET_USER_DATA 0x15 |
Referenced by QDebug_ProcessCommands().
#define QT_DELTAS 0x26 |
Referenced by Transmit_Delta().
#define QT_DUMMY 0x20 |
Referenced by Transmit_Dummy().
#define QT_GLOBAL_CONFIG 0x22 |
Referenced by Transmit_Global_Config().
#define QT_REFERENCES 0x25 |
Referenced by Transmit_Ref().
#define QT_SENSOR_CONFIG 0x23 |
Referenced by Transmit_Sensor_Config().
#define QT_SIGN_ON 0x21 |
Referenced by Transmit_Sign_On().
#define QT_SIGNALS 0x24 |
Referenced by Transmit_Signals().
#define QT_STATES 0x27 |
Referenced by Transmit_State().
#define SUBS_DELTA 5 |
Referenced by QDebug_SendData().
#define SUBS_GLOBAL_CONFIG 1 |
Referenced by QDebug_SendData().
#define SUBS_REF 4 |
Referenced by QDebug_SendData().
#define SUBS_SENSOR_CONFIG 2 |
Referenced by QDebug_SendData().
#define SUBS_SIGN_ON 0 |
Referenced by QDebug_SendData().
#define SUBS_SIGNALS 3 |
Referenced by QDebug_SendData().
#define SUBS_STATES 6 |
Referenced by QDebug_SendData().
void QDebug_Init | ( | void | ) |
This API initializes QDebug interface, including the low level hardware interface (SPI, TWI, USART etc).
This API initializes QDebug interface, including the low level hardware interface (SPI, TWI, USART etc).
References BitBangSPI_Master_Init(), Init_Buffers(), qt_lib_sig_info_t::library_version, qt_get_library_sig(), read_info_from_eeprom(), read_settings_from_eeprom(), write_burst_lenghts_to_eeprom(), write_global_settings_to_eeprom(), write_info_to_eeprom(), and write_sensor_settings_to_eeprom().
Referenced by main().
void QDebug_ProcessCommands | ( | void | ) |
Command handler for the data received from QTouch Studio.
References GetChar(), QT_CMD_DUMMY, QT_CMD_SET_CH_CONFIG, QT_CMD_SET_GLOBAL_CONFIG, QT_CMD_SET_QM_BURST_LENGTHS, QT_CMD_SET_SUBS, QT_CMD_SET_USER_DATA, Receive_Message(), RX_Buffer, RX_index, Set_Channel_Config(), Set_Global_Config(), Set_QM_Burst_Lengths(), Set_QT_User_Data(), and Set_Subscriptions().
Referenced by main().
void QDebug_SendData | ( | uint16_t | qt_lib_flags | ) |
Send data to QTouch Studio based on the subscription.
qt_lib_flags:Change | flag from measure_sensors. |
qt_lib_flags:Change | flag from measure_sensors. |
References delivery, qgLibraryChanges, qgSubsAllways, qgSubsChange, qgSubsOnce, QTLIB_CHANNEL_REF_CHANGE, QTLIB_ROTOR_SLIDER_POS_CHANGE, QTLIB_STATUS_CHANGE, SequenceH, SUBS_DELTA, SUBS_GLOBAL_CONFIG, SUBS_REF, SUBS_SENSOR_CONFIG, SUBS_SIGN_ON, SUBS_SIGNALS, SUBS_STATES, Transmit_Delta(), Transmit_Dummy(), Transmit_Global_Config(), Transmit_Ref(), Transmit_Sensor_Config(), Transmit_Sign_On(), Transmit_Signals(), and Transmit_State().
Referenced by main().
void QDebug_SetSubscriptions | ( | uint16_t | once, |
uint16_t | change, | ||
uint16_t | allways | ||
) |
Set subscription values.
References qgSubsAllways, qgSubsChange, and qgSubsOnce.
Referenced by Set_Subscriptions().
void Set_Channel_Config | ( | void | ) |
Extract the data packet from QTouch Studio and set channel config.
References GetChar(), sensors, tag_sensor_t::threshold, tag_sensor_t::type_aks_pos_hyst, and write_sensor_settings_to_eeprom().
Referenced by QDebug_ProcessCommands().
void Set_Global_Config | ( | void | ) |
Extract the data packet from QTouch Studio and set global config.
References GetChar(), qt_config_data, tag_qt_touch_lib_config_data_t::qt_di, tag_qt_touch_lib_config_data_t::qt_drift_hold_time, tag_qt_touch_lib_config_data_t::qt_max_on_duration, qt_measurement_period_msec, tag_qt_touch_lib_config_data_t::qt_neg_drift_rate, tag_qt_touch_lib_config_data_t::qt_pos_drift_rate, tag_qt_touch_lib_config_data_t::qt_pos_recal_delay, tag_qt_touch_lib_config_data_t::qt_recal_threshold, and write_global_settings_to_eeprom().
Referenced by QDebug_ProcessCommands().
void Set_Measurement_Period | ( | void | ) |
Extract the data packet from QTouch Studio and set measurement period.
void Set_QM_Burst_Lengths | ( | void | ) |
Extract the data packet from QTouch Studio and set QMatrix burst lengths.
Extract the data packet from QTouch Studio and set QMatrix burst lengths.
References GetChar(), qt_burst_lengths, QT_NUM_CHANNELS, and write_burst_lenghts_to_eeprom().
Referenced by QDebug_ProcessCommands().
void Set_QT_User_Data | ( | uint8_t * | pdata | ) |
Extracts user data from QTouch Studio to touch mcu memory.
pdata,: | data pointer. |
data | pointer |
References PutChar(), RX_Buffer, and Send_Message().
Referenced by QDebug_ProcessCommands().
void Set_Subscriptions | ( | void | ) |
Set Data Subscription values.
References GetChar(), and QDebug_SetSubscriptions().
Referenced by QDebug_ProcessCommands().
void Transmit_Delta | ( | void | ) |
Transmits the channel delta values to QTouch Studio.
References num_sensors, PutChar(), QT_DELTAS, qt_get_sensor_delta(), and Send_Message().
Referenced by QDebug_SendData().
void Transmit_Dummy | ( | void | ) |
Transmits a dummy packet if no other subscriptions are set.
References PutChar(), QT_DUMMY, and Send_Message().
Referenced by QDebug_SendData().
void Transmit_Global_Config | ( | void | ) |
Transmits the global config struct to QTouch Studio.
References PutChar(), PutInt(), qt_config_data, tag_qt_touch_lib_config_data_t::qt_di, tag_qt_touch_lib_config_data_t::qt_drift_hold_time, QT_GLOBAL_CONFIG, tag_qt_touch_lib_config_data_t::qt_max_on_duration, qt_measurement_period_msec, tag_qt_touch_lib_config_data_t::qt_neg_drift_rate, tag_qt_touch_lib_config_data_t::qt_pos_drift_rate, tag_qt_touch_lib_config_data_t::qt_pos_recal_delay, tag_qt_touch_lib_config_data_t::qt_recal_threshold, Send_Message(), and TICKS_PER_MS.
Referenced by QDebug_SendData().
void Transmit_QT_User_Data | ( | uint8_t * | pdata, |
uint16_t | c | ||
) |
Transmits user data to QTouch Studio.
pdata,: | data pointer. |
c,: | length of data in bytes. |
data | pointer, length of data in bytes |
References PutChar(), and Send_Message().
void Transmit_Ref | ( | void | ) |
Transmits the channel reference values to QTouch Studio.
References tag_qt_touch_lib_measure_data_t::channel_references, PutChar(), qt_measure_data, QT_NUM_CHANNELS, QT_REFERENCES, and Send_Message().
Referenced by QDebug_SendData().
void Transmit_Sensor_Config | ( | void | ) |
Transmits the channel config struct to QTouch Studio.
References PutChar(), QT_NUM_CHANNELS, QT_SENSOR_CONFIG, Send_Message(), and sensors.
Referenced by QDebug_SendData().
void Transmit_Sign_On | ( | void | ) |
Transmits the sign on packet to QTouch Studio.
References delivery, INTERFACE, qt_lib_sig_info_t::lib_sig_lword, qt_lib_sig_info_t::library_version, PROJECT_ID, PutChar(), PutInt(), QT_NUM_CHANNELS, QT_SIGN_ON, and Send_Message().
Referenced by QDebug_SendData().
void Transmit_Signals | ( | void | ) |
Transmits the measurement values for each channel to QTouch Studio.
References tag_qt_touch_lib_measure_data_t::channel_signals, PutChar(), qt_measure_data, QT_NUM_CHANNELS, QT_SIGNALS, and Send_Message().
Referenced by QDebug_SendData().
void Transmit_State | ( | void | ) |
Transmits the state values to QTouch Studio.
References PutChar(), QT_MAX_NUM_ROTORS_SLIDERS, qt_measure_data, QT_NUM_CHANNELS, QT_NUM_SENSOR_STATE_BYTES, QT_STATES, tag_qt_touch_lib_measure_data_t::qt_touch_status, tag_qt_touch_status_t::rotor_slider_values, Send_Message(), and tag_qt_touch_status_t::sensor_states.
Referenced by QDebug_SendData().
void Transmit_Time_Stamps | ( | void | ) |
Transmits the application execution timestamp values to QTouch Studio.
References PutInt(), Send_Message(), timestamp1_hword, timestamp1_lword, timestamp2_hword, timestamp2_lword, timestamp3_hword, and timestamp3_lword.