Microchip® Advanced Software Framework

QDebugTransport.h File Reference
#include <parts.h>
#include "touch_api.h"

Macros

#define DEF_TOUCH_QDEBUG_ENABLE   0
 
#define DEF_TOUCH_QDEBUG_ENABLE_AT   0
 
#define DEF_TOUCH_QDEBUG_ENABLE_QM   0
 
#define DEF_TOUCH_QDEBUG_ENABLE_QTA   0
 
#define DEF_TOUCH_QDEBUG_ENABLE_QTB   0
 
#define INT(a, b)   ((a << 8) | b)
 
#define MESSAGE_START   0x1B
 
#define RX_BUFFER_SIZE   (QT_NUM_CHANNELS*3)+10
 
#define STATE_DATA   3
 
#define STATE_IDLE   0
 
#define STATE_LENGTH1   1
 
#define STATE_LENGTH2   2
 
#define TX_BUFFER_SIZE   (QT_NUM_CHANNELS*3)+10
 

Functions

uint8_t GetChar (void)
 Get one byte from the Receive Buffer. More...
 
void Init_Buffers (void)
 Initialize the send and receive buffers. More...
 
void PutChar (uint8_t data)
 Puts one byte in the Transmit Buffer. More...
 
void PutInt (uint16_t data)
 Puts two bytes in the Transmit Buffer. More...
 
uint8_t Receive_Message (void)
 Executes a master read transmission if TWI is selected as interface. Checks if RX_Buffer has a valid frame. More...
 
uint8_t RxHandler (uint8_t c)
 Handles the incoming bytes from the interface selected in QDebugSettings.h and puts the bytes in the RX_Buffer data read by the selected interface. More...
 
void Send_Message (void)
 Send the content of the TX_Buffer to the USB Bridge using the interface selected in QDebugSettings.h. More...
 

Variables

uint8_t RX_Buffer [RX_BUFFER_SIZE]
 RX Buffer globals. More...
 
uint16_t RX_index
 
uint8_t SequenceH
 
uint8_t SequenceL
 
uint8_t TX_Buffer [TX_BUFFER_SIZE]
 TX Buffer globals. More...
 
uint16_t TX_index
 

#define DEF_TOUCH_QDEBUG_ENABLE   0
#define DEF_TOUCH_QDEBUG_ENABLE_AT   0
#define DEF_TOUCH_QDEBUG_ENABLE_QM   0
#define DEF_TOUCH_QDEBUG_ENABLE_QTA   0
#define DEF_TOUCH_QDEBUG_ENABLE_QTB   0
#define INT (   a,
 
)    ((a << 8) | b)
#define MESSAGE_START   0x1B
#define RX_BUFFER_SIZE   (QT_NUM_CHANNELS*3)+10
#define STATE_DATA   3
#define STATE_IDLE   0
#define STATE_LENGTH1   1
#define STATE_LENGTH2   2
#define TX_BUFFER_SIZE   (QT_NUM_CHANNELS*3)+10

void Init_Buffers ( void  )

Initialize the send and receive buffers.

Note
Called from QDebug_Init.

Initialize the send and receive buffers.

Initialize the send and receive buffers Called from QDebug_Init.

Called from QDebug_Init

Initialize the send and receive buffers Called from QDebug_Init.

Note
Called from QDebug_Init.

References MESSAGE_START, RX_Buffer, RX_index, TX_Buffer, and TX_index.

Referenced by QDebug_Init().

uint8_t Receive_Message ( void  )

Executes a master read transmission if TWI is selected as interface. Checks if RX_Buffer has a valid frame.

Returns
uint8_t: returns a true or false dependent on whether a valid frame is available or not
Note
Called from QDebug_ProcessCommands in QDebug.c.

Executes a master read transmission if TWI is selected as interface. Checks if RX_Buffer has a valid frame.

Parameters
mdatacontains merged touch data in RF4CE packet
Returns
returns a true or false depending on whether a valid frame is available or not

Executes a master read transmission if TWI is selected as interface

Checks if RX_Buffer has a valid frame Called from QDebug_ProcessCommands in QDebug.c.

Returns
uint8_t: returns a true or false Dependant on whether a valid frame is available or not
Note
Called from QDebug_ProcessCommands in QDebug.c.

References count, LED_ON, pal_led(), RF4CE_RX_Buffer, RX_Buffer, RX_index, and twi_retrieve_message().

Referenced by app_task(), and QDebug_ProcessCommands().

uint16_t RX_index
uint8_t SequenceH

Referenced by QDebug_SendData(), and Send_Message().

uint8_t SequenceL

Referenced by Send_Message().

uint8_t TX_Buffer[TX_BUFFER_SIZE]

TX Buffer globals.

compile qdebug files only when QDebug is enabled.

Referenced by BitBangSPI_Send_Message(), Init_Buffers(), PutChar(), PutInt(), Send_Message(), switch(), and twi_send_message().