|
typedef enum dev_type_tag | dev_type_t |
| Device types as defined by 094950r00ZB_RF4CE-Device-Type-List.pdf. More...
|
|
typedef void(* | gdp_data_indication_cb_t )(uint8_t PairingRef, uint8_t nsduLength, uint8_t *nsdu, uint8_t RxLinkQuality, uint8_t RxFlags) |
|
typedef enum nib_attribute_tag | nib_attribute_t |
| Network Information Base attributes as defined by 094945r00ZB_RF4CE-Specification.pdf. More...
|
|
typedef void(* | nlde_data_confirm_cb_t )(nwk_enum_t Status, uint8_t PairingRef, profile_id_t ProfileId, uint8_t Handle) |
| NLDE-DATA.confirm primitive API. More...
|
|
typedef void(* | nlde_data_indication_cb_t )(uint8_t PairingRef, profile_id_t ProfileId, uint16_t VendorId, uint8_t nsduLength, uint8_t *nsdu, uint8_t RxLinkQuality, uint8_t RxFlags) |
| NLDE-DATA.indication primitive API. More...
|
|
typedef void(* | nlme_auto_discovery_confirm_cb_t )(nwk_enum_t Status, uint64_t SrcIEEEAddr) |
| NLME-AUTO-DISCOVERY.confirm primitive API. More...
|
|
typedef void(* | nlme_comm_status_indication_cb_t )(nwk_enum_t Status, uint8_t PairingRef, uint16_t DstPANId, uint8_t DstAddrMode, uint64_t DstAddr) |
| NLME-COMM-STATUS.indication primitive API. More...
|
|
typedef void(* | nlme_discovery_confirm_cb_t )(nwk_enum_t Status, uint8_t NumNodes, node_desc_t *NodeDescList) |
|
typedef void(* | nlme_discovery_indication_cb_t )(nwk_enum_t Status, uint64_t SrcIEEEAddr, uint8_t OrgNodeCapabilities, uint16_t OrgVendorId, uint8_t OrgVendorString[7], uint8_t OrgAppCapabilities, uint8_t OrgUserString[15], dev_type_t OrgDevTypeList[3], profile_id_t OrgProfileIdList[7], dev_type_t SearchDevType, uint8_t RxLinkQuality) |
| NLME-DISCOVERY.indication primitive API. More...
|
|
typedef void(* | nlme_get_confirm_cb_t )(nwk_enum_t Status, nib_attribute_t NIBAttribute, uint8_t NIBAttributeIndex, void *NIBAttributeValue) |
| NLME-GET.confirm primitive API. More...
|
|
typedef void(* | nlme_pair_confirm_cb_t )(nwk_enum_t Status, uint8_t PairingRef, uint16_t RecVendorId, uint8_t RecVendorString[7], uint8_t RecAppCapabilities, uint8_t RecUserString[15], dev_type_t RecDevTypeList[3], profile_id_t RecProfileIdList[7]) |
| NLME-PAIR.confirm primitive API. More...
|
|
typedef void(* | nlme_pair_indication_cb_t )(nwk_enum_t Status, uint16_t SrcPANId, uint64_t SrcIEEEAddr, uint8_t OrgNodeCapabilities, uint16_t OrgVendorId, uint8_t OrgVendorString[7], uint8_t OrgAppCapabilities, uint8_t OrgUserString[15], dev_type_t OrgDevTypeList[3], profile_id_t OrgProfileIdList[7], uint8_t KeyExTransferCount, uint8_t ProvPairingRef) |
| NLME-PAIR.indication primitive API. More...
|
|
typedef void(* | nlme_reset_confirm_cb_t )(nwk_enum_t Status) |
| NLME-RESET.confirm primitive API. More...
|
|
typedef void(* | nlme_rx_enable_confirm_cb_t )(nwk_enum_t Status) |
| Confirmation callback pointer for NLME-RX-ENABLE request. More...
|
|
typedef void(* | nlme_set_confirm_cb_t )(nwk_enum_t Status, nib_attribute_t NIBAttribute, uint8_t NIBAttributeIndex) |
| NLME-SET.confirm primitive API. More...
|
|
typedef void(* | nlme_start_confirm_cb_t )(nwk_enum_t Status) |
| NLME-START.confirm primitive API. More...
|
|
typedef void(* | nlme_unpair_confirm_cb_t )(uint8_t Status, uint8_t PairingRef) |
| NLME-UNPAIR.confirm primitive API. More...
|
|
typedef void(* | nlme_unpair_indication_cb_t )(uint8_t PairingRef) |
| NLME-UNPAIR.indication primitive API. More...
|
|
typedef void(* | nlme_update_key_confirm_cb_t )(nwk_enum_t Status, uint8_t PairingRef) |
| NLME-UPDATE-KEY.confirm primitive API. More...
|
|
typedef struct NodeDesc_tag | node_desc_t |
| Elements of the NodeDesc type as defined by 094945r00ZB_RF4CE-Specification.pdf. More...
|
|
typedef enum nwk_addr_mode_tag | nwk_addr_mode_t |
| Enumeration identifiying the address mode as defined by 094945r00ZB_RF4CE-Specification.pdf. More...
|
|
typedef enum nwk_agility_mode_tag | nwk_agility_mode_t |
| Enumeration used for implementation-specific channel agility. More...
|
|
typedef void(* | nwk_ch_agility_indication_cb_t )(uint8_t LogicalChannel) |
| Indicates a channel agility event. More...
|
|
typedef __PACK__DATA__ enum
nwk_enum_tag | nwk_enum_t |
| NWK enumerations as defined by 094945r00ZB_RF4CE-Specification.pdf, Table 45 - NWK enumerations description. More...
|
|
typedef struct
nwk_indication_callback_tag | nwk_indication_callback_t |
| struct for network indication callback. More...
|
|
typedef struct pairing_table_tag | pairing_table_t |
| Structure implementing the pairing table entry as defined by 094945r00ZB_RF4CE-Specification.pdf. More...
|
|
typedef enum profile_id_tag | profile_id_t |
| Profile IDs as defined by 094951r00ZB_RF4CE-Profile-ID-List.pdf. More...
|
|
typedef void(* | zid_data_indication_cb_t )(uint8_t PairingRef, uint16_t VendorId, uint8_t nsduLength, uint8_t *nsdu, uint8_t RxLinkQuality, uint8_t RxFlags) |
|
typedef void(* | zrc_data_indication_cb_t )(uint8_t PairingRef, uint16_t VendorId, uint8_t nsduLength, uint8_t *nsdu, uint8_t RxLinkQuality, uint8_t RxFlags) |
|
|
enum | dev_type_tag {
DEV_TYPE_RESERVED = 0x00,
DEV_TYPE_REMOTE_CONTROL = 0x01,
DEV_TYPE_TELEVISION = 0x02,
DEV_TYPE_PROJECTON = 0x03,
DEV_TYPE_PLAYER = 0x04,
DEV_TYPE_RECORDER = 0x05,
DEV_TYPE_VIDEO = 0x06,
DEV_TYPE_AUDIO = 0x07,
DEV_TYPE_AV_RECORDER = 0x08,
DEV_TYPE_SET_TOP_BOX = 0x09,
DEV_TYPE_HOME_THEATER = 0x0A,
DEV_TYPE_MEDIA_CENTER = 0x0B,
DEV_TYPE_GAME_CONSOLE = 0x0C,
DEV_TYPE_SAT_RADIO = 0x0D,
DEV_TYPE_IR_EXTENDER = 0x0E,
DEV_TYPE_MONITOR = 0x0F,
DEV_TYPE_GENERIC = 0xFE,
DEV_TYPE_WILDCARD = 0xFF,
DEV_TYPE_RESERVED = 0x00,
DEV_TYPE_REMOTE_CONTROL = 0x01,
DEV_TYPE_TELEVISION = 0x02,
DEV_TYPE_PROJECTON = 0x03,
DEV_TYPE_PLAYER = 0x04,
DEV_TYPE_RECORDER = 0x05,
DEV_TYPE_VIDEO = 0x06,
DEV_TYPE_AUDIO = 0x07,
DEV_TYPE_AV_RECORDER = 0x08,
DEV_TYPE_SET_TOP_BOX = 0x09,
DEV_TYPE_HOME_THEATER = 0x0A,
DEV_TYPE_MEDIA_CENTER = 0x0B,
DEV_TYPE_GAME_CONSOLE = 0x0C,
DEV_TYPE_SAT_RADIO = 0x0D,
DEV_TYPE_IR_EXTENDER = 0x0E,
DEV_TYPE_MONITOR = 0x0F,
DEV_TYPE_GENERIC = 0xFE,
DEV_TYPE_WILDCARD = 0xFF
} |
| Device types as defined by 094950r00ZB_RF4CE-Device-Type-List.pdf. More...
|
|
enum | nib_attribute_tag {
nwkActivePeriod = 0x60,
nwkBaseChannel = 0x61,
nwkDiscoveryLQIThreshold = 0x62,
nwkDiscoveryRepetitionInterval = 0x63,
nwkDutyCycle = 0x64,
nwkFrameCounter = 0x65,
nwkIndicateDiscoveryRequests = 0x66,
nwkInPowerSave = 0x67,
nwkPairingTable = 0x68,
nwkMaxDiscoveryRepetitions = 0x69,
nwkMaxFirstAttemptCSMABackoffs = 0x6a,
nwkMaxFirstAttemptFrameRetries = 0x6b,
nwkMaxReportedNodeDescriptors = 0x6c,
nwkResponseWaitTime = 0x6d,
nwkScanDuration = 0x6e,
nwkUserString = 0x6f,
nwkPrivateIeeeAddr = 0x70,
nwkPrivateVendorIdentifier = 0x71,
nwkPrivateVendorString = 0x72,
nwkPrivateNodeCapabilities = 0x73,
nwkPrivatePanIdentifier = 0x74,
nwkPrivateShortAddress = 0x75,
nwkPrivateMaxPairingTableEntries = 0x76,
nwkPrivateChAgEnabled = 0x77,
nwkPrivateChAgScanInterval = 0x78,
nwkPrivateChAgEdThreshold = 0x79,
aplKeyRepeatInterval = 0x80,
aplKeyRepeatWaitTime = 0x81,
aplKeyExchangeTransferCount = 0x82,
nwkActivePeriod = 0x60,
nwkBaseChannel = 0x61,
nwkDiscoveryLQIThreshold = 0x62,
nwkDiscoveryRepetitionInterval = 0x63,
nwkDutyCycle = 0x64,
nwkFrameCounter = 0x65,
nwkIndicateDiscoveryRequests = 0x66,
nwkInPowerSave = 0x67,
nwkPairingTable = 0x68,
nwkMaxDiscoveryRepetitions = 0x69,
nwkMaxFirstAttemptCSMABackoffs = 0x6a,
nwkMaxFirstAttemptFrameRetries = 0x6b,
nwkMaxReportedNodeDescriptors = 0x6c,
nwkResponseWaitTime = 0x6d,
nwkScanDuration = 0x6e,
nwkUserString = 0x6f,
nwkPrivateIeeeAddr = 0x70,
nwkPrivateVendorIdentifier = 0x71,
nwkPrivateVendorString = 0x72,
nwkPrivateNodeCapabilities = 0x73,
nwkPrivatePanIdentifier = 0x74,
nwkPrivateShortAddress = 0x75,
nwkPrivateMaxPairingTableEntries = 0x76,
nwkPrivateChAgEnabled = 0x77,
nwkPrivateChAgScanInterval = 0x78,
nwkPrivateChAgEdThreshold = 0x79,
aplKeyRepeatInterval = 0x80,
aplKeyRepeatWaitTime = 0x81,
aplKeyExchangeTransferCount = 0x82
} |
| Network Information Base attributes as defined by 094945r00ZB_RF4CE-Specification.pdf. More...
|
|
enum | nwk_addr_mode_tag {
NWK_ADDR_MODE_16 = 0,
NWK_ADDR_MODE_64 = 1,
NWK_ADDR_MODE_16 = 0,
NWK_ADDR_MODE_64 = 1
} |
| Enumeration identifiying the address mode as defined by 094945r00ZB_RF4CE-Specification.pdf. More...
|
|
enum | nwk_agility_mode_tag {
AG_ONE_SHOT = 0,
AG_PERIODIC = 1,
AG_STOP = 2,
AG_ONE_SHOT = 0,
AG_PERIODIC = 1,
AG_STOP = 2
} |
| Enumeration used for implementation-specific channel agility. More...
|
|
enum | nwk_enum_tag {
NWK_SUCCESS = 0x00,
NWK_NO_ORG_CAPACITY = 0xb0,
NWK_NO_REC_CAPACITY = 0xb1,
NWK_NO_PAIRING = 0xb2,
NWK_NO_RESPONSE = 0xb3,
NWK_NOT_PERMITTED = 0xb4,
NWK_DUPLICATE_PAIRING = 0xb5,
NWK_FRAME_COUNTER_EXPIRED = 0xb6,
NWK_DISCOVERY_ERROR = 0xb7,
NWK_DISCOVERY_TIMEOUT = 0xb8,
NWK_SECURITY_TIMEOUT = 0xb9,
NWK_SECURITY_FAILURE = 0xba,
NWK_INVALID_PARAMETER = 0xe8,
NWK_UNSUPPORTED_ATTRIBUTE = 0xf4,
NWK_INVALID_INDEX = 0xf9,
NWK_MAC_CHANNEL_ACCESS_FAILURE = 0xE1,
NWK_MAC_DISABLE_TRX_FAILURE = 0xE3,
NWK_MAC_FRAME_TOO_LONG = 0xE5,
NWK_MAC_INVALID_GTS = 0xE6,
NWK_MAC_INVALID_HANDLE = 0xE7,
NWK_MAC_NO_ACK = 0xE9,
NWK_MAC_NO_BEACON = 0xEA,
NWK_MAC_NO_DATA = 0xEB,
NWK_MAC_NO_SHORT_ADDRESS = 0xEC,
NWK_MAC_OUT_OF_CAP = 0xED,
NWK_MAC_PAN_ID_CONFLICT = 0xEE,
NWK_MAC_REALIGNMENT = 0xEF,
NWK_MAC_TRANSACTION_EXPIRED = 0xF0,
NWK_MAC_TRANSACTION_OVERFLOW = 0xF1,
NWK_MAC_TX_ACTIVE = 0xF2,
NWK_MAC_INVALID_ADDRESS = 0xF5,
NWK_SUCCESS = 0x00,
NWK_NO_ORG_CAPACITY = 0xb0,
NWK_NO_REC_CAPACITY = 0xb1,
NWK_NO_PAIRING = 0xb2,
NWK_NO_RESPONSE = 0xb3,
NWK_NOT_PERMITTED = 0xb4,
NWK_DUPLICATE_PAIRING = 0xb5,
NWK_FRAME_COUNTER_EXPIRED = 0xb6,
NWK_DISCOVERY_ERROR = 0xb7,
NWK_DISCOVERY_TIMEOUT = 0xb8,
NWK_SECURITY_TIMEOUT = 0xb9,
NWK_SECURITY_FAILURE = 0xba,
NWK_INVALID_PARAMETER = 0xe8,
NWK_UNSUPPORTED_ATTRIBUTE = 0xf4,
NWK_INVALID_INDEX = 0xf9,
NWK_MAC_CHANNEL_ACCESS_FAILURE = 0xE1,
NWK_MAC_DISABLE_TRX_FAILURE = 0xE3,
NWK_MAC_FRAME_TOO_LONG = 0xE5,
NWK_MAC_INVALID_GTS = 0xE6,
NWK_MAC_INVALID_HANDLE = 0xE7,
NWK_MAC_NO_ACK = 0xE9,
NWK_MAC_NO_BEACON = 0xEA,
NWK_MAC_NO_DATA = 0xEB,
NWK_MAC_NO_SHORT_ADDRESS = 0xEC,
NWK_MAC_OUT_OF_CAP = 0xED,
NWK_MAC_PAN_ID_CONFLICT = 0xEE,
NWK_MAC_REALIGNMENT = 0xEF,
NWK_MAC_TRANSACTION_EXPIRED = 0xF0,
NWK_MAC_TRANSACTION_OVERFLOW = 0xF1,
NWK_MAC_TX_ACTIVE = 0xF2,
NWK_MAC_INVALID_ADDRESS = 0xF5
} |
| NWK enumerations as defined by 094945r00ZB_RF4CE-Specification.pdf, Table 45 - NWK enumerations description. More...
|
|
enum | profile_id_tag {
PROFILE_ID_RESERVED_00 = 0x00,
PROFILE_ID_ZRC = 0x01,
PROFILE_ID_VENDOR_DATA = 0xFE,
PROFILE_ID_WILDCARD = 0xFF,
PROFILE_ID_RESERVED_00 = 0x00,
PROFILE_ID_ZRC = 0x01,
PROFILE_ID_ZID = 0x02,
PROFILE_ID_VENDOR_DATA = 0xFE,
PROFILE_ID_WILDCARD = 0xFF
} |
| Profile IDs as defined by 094951r00ZB_RF4CE-Profile-ID-List.pdf. More...
|
|
|
void | clear_pairing_ref (uint8_t first_ref, uint8_t length) |
| Clears pairing references within EEPROM. More...
|
|
bool | nlde_data_request (uint8_t PairingRef, profile_id_t ProfileId, uint16_t VendorId, uint8_t nsduLength, uint8_t *nsdu, uint8_t TxOptions, uint8_t Handle, FUNC_PTR confirm_cb) |
| NLDE-DATA.request primitive API. More...
|
|
bool | nlme_auto_discovery_request (uint8_t RecAppCapabilities, dev_type_t RecDevTypeList[3], profile_id_t RecProfileIdList[7], uint32_t AutoDiscDuration, FUNC_PTR confirm_cb) |
| NLME-AUTO-DISCOVERY.request primitive API. More...
|
|
bool | nlme_discovery_request (uint16_t DstPANId, uint16_t DstNwkAddr, uint8_t OrgAppCapabilities, dev_type_t OrgDevTypeList[3], profile_id_t OrgProfileIdList[7], dev_type_t SearchDevType, uint8_t DiscProfileIdListSize, profile_id_t DiscProfileIdList[7], uint32_t DiscDuration, FUNC_PTR confirm_cb) |
| NLME-DISCOVERY.request primitive API. More...
|
|
bool | nlme_discovery_response (nwk_enum_t Status, uint64_t DstIEEEAddr, uint8_t RecAppCapabilities, dev_type_t RecDevTypeList[3], profile_id_t RecProfileIdList[7], uint8_t DiscReqLQI) |
| NLME-DISCOVERY.response primitive API. More...
|
|
bool | nlme_get_request (nib_attribute_t NIBAttribute, uint8_t NIBAttributeIndex, FUNC_PTR confirm_cb) |
| NLME-GET.request primitive API. More...
|
|
bool | nlme_pair_request (uint8_t LogicalChannel, uint16_t DstPANId, uint64_t DstIEEEAddr, uint8_t OrgAppCapabilities, dev_type_t OrgDevTypeList[3], profile_id_t OrgProfileIdList[7], uint8_t KeyExTransferCount, FUNC_PTR confirm_cb) |
| NLME-PAIR.request primitive API. More...
|
|
bool | nlme_pair_response (nwk_enum_t Status, uint16_t DstPANId, uint64_t DstIEEEAddr, uint8_t RecAppCapabilities, dev_type_t RecDevTypeList[3], profile_id_t RecProfileIdList[7], uint8_t ProvPairingRef) |
| NLME-PAIR.response primitive API. More...
|
|
bool | nlme_reset_request (bool SetDefaultNIB, FUNC_PTR confirm_cb) |
| NLME-RESET.request primitive API. More...
|
|
bool | nlme_rx_enable_request (uint32_t RxOnDuration, FUNC_PTR confirm_cb) |
| NLME-RX-ENABLE.request primitive API. More...
|
|
bool | nlme_set_request (nib_attribute_t NIBAttribute, uint8_t NIBAttributeIndex, uint8_t *NIBAttributeValue, FUNC_PTR confirm_cb) |
| NLME-SET.request primitive API. More...
|
|
bool | nlme_start_request (FUNC_PTR confirm_cb) |
| NLME-START.request primitive API. More...
|
|
bool | nlme_unpair_request (uint8_t PairingRef, FUNC_PTR confirm_cb) |
| NLME-UNPAIR.request primitive API. More...
|
|
bool | nlme_unpair_response (uint8_t PairingRef) |
| NLME-UNPAIR.response primitive API. More...
|
|
bool | nlme_update_key_request (uint8_t PairingRef, uint8_t NewLinkKey[16], FUNC_PTR confirm_cb) |
| NLME-UPDATE-KEY.request primitive API. More...
|
|
bool | nwk_ch_agility_request (nwk_agility_mode_t AgilityMode, FUNC_PTR confirm_cb) |
| Sets channel agility mode. More...
|
|
uint8_t | nwk_get_nib_attribute_size (uint8_t nib_attribute_id) |
| Gets the NIB attribute value size. More...
|
|
nwk_enum_t | nwk_init (void) |
| Initialization of RF4CE network layer. More...
|
|
bool | nwk_ready_to_sleep (void) |
| Checks if the entire stack is idle. More...
|
|
bool | nwk_stack_idle (void) |
| Checks if the network stack is idle. More...
|
|
bool | nwk_task (void) |
| Task handling of RF4CE network layer. More...
|
|
void | read_pairing_ref (uint8_t *pairing_ref, uint8_t length) |
| Reads pairing reference from EEPROM. More...
|
|
void | register_nwk_indication_callback (nwk_indication_callback_t *nwk_indication_cb) |
| Registering network indication callback. More...
|
|
void | store_pairing_ref (uint8_t *pairing_ref, uint8_t length) |
| Stores pairing references to EEPROM. More...
|
|