Main functions for USB composite example.
Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
int | main (void) |
Main function. Execution starts here. More... | |
void | main_mouse_disable (void) |
Called by HID interface Callback running when USB Host disable mouse interface. More... | |
bool | main_mouse_enable (void) |
Called by HID interface Callback running when USB Host enable mouse interface. More... | |
void | main_msc_disable (void) |
Called by MSC interface Callback running when USB Host disable MSC interface. More... | |
bool | main_msc_enable (void) |
Called by MSC interface Callback running when USB Host enable MSC interface. More... | |
void | main_remotewakeup_disable (void) |
Called by UDC when USB Host request to disable remote wakeup. More... | |
void | main_remotewakeup_enable (void) |
Called by UDC when USB Host request to enable remote wakeup. More... | |
void | main_resume_action (void) |
Turn on a led to notify active mode Called when the USB line is resumed from the suspend state. More... | |
void | main_sof_action (void) |
Manages the leds behaviors Called when a start of frame is received on USB line each 1ms. More... | |
void | main_suspend_action (void) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More... | |
Variables | |
static volatile bool | main_b_mouse_enable = false |
static volatile bool | main_b_msc_enable = false |
int main | ( | void | ) |
Main function. Execution starts here.
References board_init(), cpu_irq_enable(), irq_initialize_vectors, main_b_msc_enable, memories_initialization(), sleepmgr_enter_sleep(), sleepmgr_init(), sysclk_init(), udc_start(), udi_msc_process_trans(), ui_init(), and ui_powerdown().
void main_mouse_disable | ( | void | ) |
Called by HID interface Callback running when USB Host disable mouse interface.
bool main_mouse_enable | ( | void | ) |
Called by HID interface Callback running when USB Host enable mouse interface.
true | if mouse startup is ok |
void main_msc_disable | ( | void | ) |
Called by MSC interface Callback running when USB Host disable MSC interface.
References main_b_msc_enable.
bool main_msc_enable | ( | void | ) |
Called by MSC interface Callback running when USB Host enable MSC interface.
true | if MSC startup is ok |
References main_b_msc_enable.
void main_remotewakeup_disable | ( | void | ) |
Called by UDC when USB Host request to disable remote wakeup.
References ui_wakeup_disable().
void main_remotewakeup_enable | ( | void | ) |
Called by UDC when USB Host request to enable remote wakeup.
References ui_wakeup_enable().
void main_resume_action | ( | void | ) |
Turn on a led to notify active mode Called when the USB line is resumed from the suspend state.
Called by UDD when the USB line exit of suspend state.
References ui_wakeup().
void main_sof_action | ( | void | ) |
Manages the leds behaviors Called when a start of frame is received on USB line each 1ms.
Called when a start of frame is received on USB line.
References main_b_mouse_enable, main_b_msc_enable, udd_get_frame_number(), and ui_process().
void main_suspend_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state.
Turn off all leds Callback running when USB Host set USB line in suspend state.
Called by UDD when a suspend is received Callback running when USB Host set USB line in suspend state.
References ui_powerdown().
Referenced by main_mouse_disable(), main_mouse_enable(), and main_sof_action().
Referenced by main(), main_msc_disable(), main_msc_enable(), and main_sof_action().