Microchip® Advanced Software Framework

at86rf212/src/tfa.c File Reference
#include <stdint.h>
#include <string.h>
#include <stdbool.h>
#include <stdlib.h>
#include "pal.h"
#include "return_val.h"
#include "tal.h"
#include "tal_constants.h"
#include "tal_internal.h"
#include "ieee_const.h"
#include "at86rf212.h"
#include "tfa.h"

Macros

#define CLIP_VALUE_REG   (62)
 

Functions

static void init_tfa_pib (void)
 
phy_enum_t tfa_cca_perform (void)
 
void tfa_continuous_tx_start (continuous_tx_mode_t tx_mode, bool random_content)
 
void tfa_continuous_tx_stop (void)
 
uint8_t tfa_ed_sample (void)
 
uint16_t tfa_get_batmon_voltage (void)
 Gets the transceiver's supply voltage. More...
 
retval_t tfa_init (void)
 Initializes the TFA. More...
 
retval_t tfa_pib_get (tfa_pib_t tfa_pib_attribute, void *value)
 Gets a TFA PIB attribute. More...
 
retval_t tfa_pib_set (tfa_pib_t tfa_pib_attribute, void *value)
 Sets a TFA PIB attribute. More...
 
void tfa_reset (bool set_default_pib)
 Reset the TFA. More...
 
static void write_all_tfa_pibs_to_trx (void)
 Write all shadow PIB variables to the transceiver. More...
 

Variables

static int8_t tfa_pib_rx_sens
 TFA PIB attribute to reduce the Rx sensitivity. More...
 

#define CLIP_VALUE_REG   (62)

Referenced by tfa_ed_sample().

static void init_tfa_pib ( void  )
static

References tfa_pib_rx_sens, and TFA_PIB_RX_SENS_DEF.

Referenced by tfa_init(), and tfa_reset().

void tfa_continuous_tx_stop ( void  )

References tal_reset().

static void write_all_tfa_pibs_to_trx ( void  )
static

Write all shadow PIB variables to the transceiver.

This function writes all shadow PIB variables to the transceiver. It is assumed that the radio does not sleep.

References TFA_PIB_RX_SENS, tfa_pib_rx_sens, and tfa_pib_set().

Referenced by tfa_init(), and tfa_reset().

int8_t tfa_pib_rx_sens
static

TFA PIB attribute to reduce the Rx sensitivity.

Represents the Rx sensitivity value in dBm; example: -52

Referenced by init_tfa_pib(), tfa_pib_get(), tfa_pib_set(), and write_all_tfa_pibs_to_trx().