In this section you can find all the projects related to the FLASHCALW - FLASH Controller Double-Word.
FLASHCALW example1 for SAM4L Xplained Pro | |
Use the FLASHCALW, read and write data to the internal flash, using a flash block as an NVRAM, located either in the flash array or in the user page. Use the last page as the locked page, check the lock status and finally unlock it. | |
FLASHCALW example1 for SAM4L8 Xplained Pro | |
Use the FLASHCALW, read and write data to the internal flash, using a flash block as an NVRAM, located either in the flash array or in the user page. Use the last page as the locked page, check the lock status and finally unlock it. | |
FLASHCALW example1 for SAM4L_EK | |
Use the FLASHCALW, read and write data to the internal flash, using a flash block as an NVRAM, located either in the flash array or in the user page. Use the last page as the locked page, check the lock status and finally unlock it. | |
FLASHCALW example2 for SAM4L Xplained Pro | |
Read the unique ID of the device. | |
FLASHCALW example2 for SAM4L8 Xplained Pro | |
Read the unique ID of the device. | |
FLASHCALW example2 for SAM4L_EK | |
Read the unique ID of the device. | |
FLASHCALW PicoCache example for SAM4L Xplained Pro | |
PicoCache example for flashcalw driver. | |
FLASHCALW PicoCache example for SAM4L8 Xplained Pro | |
PicoCache example for flashcalw driver. | |
FLASHCALW PicoCache example for SAM4L_EK | |
PicoCache example for flashcalw driver. |
FLASHCALW unit tests for SAM4L Xplained Pro | |
Unit test application for the flashcalw driver. | |
FLASHCALW unit tests for SAM4L8 Xplained Pro | |
Unit test application for the flashcalw driver. | |
FLASHCALW unit tests for SAM4L_EK | |
Unit test application for the flashcalw driver. |