Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Serial Interface Module

This module is responsible for encoding and decoding the serial bytes to/from Host into corresponding MAC APIs .

Macros

#define EOT   (4)
 The end of transmission delimiter. More...
 
#define MAC_PID   (1)
 
#define MAC_PID_LEN   (1)
 
#define SIO_BUF_COUNT   (5)
 
#define SIO_RX_BUF_SIZE   (156)
 
#define SIO_TX_BUF_SIZE   SIO_RX_BUF_SIZE
 
#define SOT   (1)
 The start of transmission delimiter. More...
 
#define UART_RX_STATE_DATA   (3)
 A UART state that expects the next data character to be received. More...
 
#define UART_RX_STATE_EOT   (4)
 A UART state that expects a EOT to be received as the next character. More...
 
#define UART_RX_STATE_LENGTH   (2)
 A UART state that expects the length to be received as the next character. More...
 
#define UART_RX_STATE_SOT   (1)
 A UART state that expects a SOT to be received as the next character. More...
 

Functions

void serial_data_handler (void)
 Function to handle the state machine serial data exchange. More...
 
void serial_interface_init (void)
 This function does the initialization of the Serial handler state Machine. More...
 

#define EOT   (4)

The end of transmission delimiter.

#define SIO_BUF_COUNT   (5)
#define SIO_RX_BUF_SIZE   (156)
#define SIO_TX_BUF_SIZE   SIO_RX_BUF_SIZE
#define SOT   (1)

The start of transmission delimiter.

#define UART_RX_STATE_DATA   (3)

A UART state that expects the next data character to be received.

#define UART_RX_STATE_EOT   (4)

A UART state that expects a EOT to be received as the next character.

#define UART_RX_STATE_LENGTH   (2)

A UART state that expects the length to be received as the next character.

#define UART_RX_STATE_SOT   (1)

A UART state that expects a SOT to be received as the next character.

void serial_interface_init ( void  )

This function does the initialization of the Serial handler state Machine.

This function does the initialization of the Serial handler state Machine.

References sio2host_init(), sio_rx_state, and UART_RX_STATE_SOT.

Referenced by main().