Microchip® Advanced Software Framework

slipif.h File Reference
#include "lwip/opt.h"
#include "lwip/netif.h"

Macros

#define SLIP_RX_FROM_ISR   0
 Set this to 1 to enable functions to pass in RX bytes from ISR context. More...
 
#define SLIP_RX_QUEUE   SLIP_RX_FROM_ISR
 Set this to 1 (default for SLIP_RX_FROM_ISR) to queue incoming packets received by slipif_received_byte[s]() as long as PBUF_POOL pbufs are available. More...
 
#define SLIP_USE_RX_THREAD   !NO_SYS
 Set this to 1 to start a thread that blocks reading on the serial line (using sio_read()). More...
 

Functions

err_t slipif_init (struct netif *netif)
 
void slipif_poll (struct netif *netif)
 

#define SLIP_RX_FROM_ISR   0

Set this to 1 to enable functions to pass in RX bytes from ISR context.

If enabled, slipif_received_byte[s]() process incoming bytes and put assembled packets on a queue, which is fed into lwIP from slipif_poll(). If disabled, slipif_poll() polls the serial line (using sio_tryread()).

#define SLIP_RX_QUEUE   SLIP_RX_FROM_ISR

Set this to 1 (default for SLIP_RX_FROM_ISR) to queue incoming packets received by slipif_received_byte[s]() as long as PBUF_POOL pbufs are available.

If disabled, packets will be dropped if more than one packet is received.

#define SLIP_USE_RX_THREAD   !NO_SYS

Set this to 1 to start a thread that blocks reading on the serial line (using sio_read()).

err_t slipif_init ( struct netif netif)
void slipif_poll ( struct netif netif)